Other Parts Discussed in Thread: Z-STACK, CC2650, CC2630, CC2650STK
Hi,
I am very pleased to announce the release of a new TI Z-Stack (TM) Home 1.2.2a, which includes several important updates on top of the previous release. It is recommended for anyone currently using any previous z-stack release to update to this latest release.
The detailed change list is included in the release notes, which are part of the installed package.
This latest release also includes all the features that were previously introduced in 1.2.2, as listed below, including support for our best-in class low power Wireless MCU device family, CC2630/CC2650.
For more information about the SimpleLink UltraLowPower family, please visit www.ti.com/simplelinkulp
Applications on CC2630/CC2650 are implemented on top of TI-RTOS, TI real-time operating system for multi-threaded operation.
TI-RTOS package includes additional middleware components and device drivers and it is integrated in the Z-Stack (TM) SDK. For more information on TI-RTOS, please visit www.ti.com/tool/ti-rtos
Z-Stack (TM) SDK also features support for the sensor tag platform.
For more information on on the Sensor Tag based on the SimpleLink Ultra Low Power, please visit www.ti.com/tool/cc2650stk
Also included are enhanced ZDO features that will be part of the r21 ZigBee (R) specification, added and improved documentation and bug fixes.
To download the latest Z-Stack (TM) Home release, please visit www.ti.com/tool/z-stack
Thanks,
OD