Other Parts Discussed in Thread: CC2650, CC2650EMK, Z-STACK
Hi,
I try to use CC2650 as coordinator by using CC2650EM+SmartRF06. I put the znp_coordinator_pro_secure_linkkeyjoin.hex to CC2650 and tried it with Z-tool. It successfully iniatiate the network with my ZHA 1.2 compliant third party endpoint. CC2650 replied its beacon requests, sets network and starts communication by using z-tool.
Then I jump up the Sample Light-ZAP Coordinator application at the "zstack_home_1_02_02a_44539\Projects\zstack\ZAP\HA-SampleLight\EXP5438" folder. Since I dont have 5438 I changed the codes for my 5419A board. I see something is coming from UART channel's RX,TX pins. It seems there is a two way communication occuring after the app starts and periodically when the software hits zap_app.c/zapMonInfo() function.
My problem is, my endpoint is broadcasting beacon requests but nothing happens on my SampleLight-ZAP Coordinator application side. I am waiting my application to setup the network as a coordinator but it seems nothing happens. How can I debug at this point? Do you have any feedback or documents that I can refer for further digging?
Note: I dont have Packet Sniffer yet. I have second CC2650+SmarfRf06 board and using it with SmartRF Studio software. I can see my endpoint's beacon requests on Channel 11 with this setup.
Thanks.