Other Parts Discussed in Thread: Z-STACK
hi all
there are one ZED and two ZR
ZED was the child node of the ZR1 at frist。
i take ZED and ZR2 far from the ZC, and make sure they could not link with ZC any more。
sometime later ZED change parents with ZR2。 and then take them back to ZC。
after doing above Testing step (to simulate ZC had not notificed ZED changing parents) several cycle 。
i found sometimes ZC could send the msg to ZED via ZR2(the right one)
sometimes it could not send the msg via ZR2 ,although using the wrong way via ZR1 forever~~~~
then it could control ZED anymore。。。
when it could send the msg via ZR2, i saw something strange in the log ,which shows :“Reversed”:
i saw there is a MAC address in the APS payload, but i don't know what does it mean
and there is nothing like that while ZC choosing the wrong way to sending the msg ~~~~~~
so does anybody knows what will caused the ZC had not updating the routing path ?
is that related with this “Reversed” msg !!!!