Hi everyone. Im using ZStack 1.2.1 HA on a CC2530 which acts as the coordinator of the network.
I made a network consisting of a coordinator, 20 routers, and 5 end devices. If I check the AssociatedDevList, I only see 16 devices. I assume 9 of the devices have joined the network through some routers. (Is that assumption correct?). Now I power off all the routers and try to join a new one to the network. The beacons sent by the coordinator say it has no more capacity (neither routers nor end devices)., and it cant join the network. I cant understand why it says it has no more capacity when there is still place to 4 more devices in the AssociatedDevList.
Thanks!