Other Parts Discussed in Thread: CC1120, CC1310,
Hi,about 2 years ago we went through a a painful implementation of Contiki/Thingsquare (CC1120 & MSP430; Sub-GHz is a must for us).
Painful because it took some time to get it up and running, without having a decent support,
We also don't manage to get moving nodes in production, because rebuilding routing when moving between motes took up to 30s - so e.g. a fork lift can't stop for 30s. until it has reconnected...
As we are not familiar enough with the fundamentals of Contiki, we couldn't change the code accordingly - if we changed something, we got side effects on other places.
And we are not trustful enough to put such a system into production - being dependent on a system without industrial quaility grade behind.
With CC13xx I have some hope that there is a TI supported framework to adopt a TI supported Mesh-OS without the need to care about the underlaying stuff - like RTOS.
Change some parameters and you are done, being sure TI has verified the rest :-)
Back to reality: I learned from the experts that Contiki has never been designed for moving motes, so is there an alternative you can recommend?
What about THREAD (sub-GHz...)?
thx. in advance!