Other Parts Discussed in Thread: CC2650, SEGGER, Z-STACK, CC2538,
I have been looking for ZIgBee modules from TI and have only found one, the CC2650MODAMOHx. Since this module can handle ZigBee (as well as other protocols) it should work for my project. Since it is based on a Cortex-M core I'm liking it even more.
The only thing missing is a USB port so it looks like I have to create a dongle myself using a UART-to-USB solution. It just seems odd that there are no solutions already created that have a CC2650MODAMOHx in a "dongle on a stick" configuration. Have I missed a part or am I correct that I'll need to design a dongle myself?
Any suggestions as to what software libraries/stacks I should look into would be appreciated. I apparently cannot use Zstack 3.0 since it does not support the CC2650.
While I would prefer to use Eclipse/GCC I do have IAR's EWARM available. I also have a Segger J-Link available for use as a programming/debug interface although I might make the UART-to-USB interface similar enough to an ST-LINK that I can use the open source BlackMagic software as a GDBserver using JTAG for the hardware connection.
I would normally go to my local distributors for advice but since TI seems to have dropped distributors there is a bit of an information vacuum where TI's wireless parts are concerned.