Other Parts Discussed in Thread: CC2531
Good afternoon everyone
I am a beginner in this zigbee wireless transmission area. I have an application question I don't know how to solve, hope someone can help me, thank you very much.
I designed a chip that output 2 frequency signals they are all at a range of 10k to 50kHz. We want to use the CC2531 to transmit these two frequency signal wireless. I notice that the CC2531 USB dongle has 8 pins (user interface IO connector) that can be customized. If I connect my two signals to two of those IO connector, would it be OK? I think I also need software code to do such application, if so where can I find some open source code? I don't understand coding very much. Finally we want to display the two frequency signal, maybe on a computer screen. I don't know how to do this, do I need to download specific software for display?
I appreciate any suggestion and advise, have a great day.
Ran
Best