This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650DK: How CC2650 work as a coordinator

Part Number: CC2650DK
Other Parts Discussed in Thread: Z-STACK

Hello All,

I am trying to learn Zigbee HA applications with the help of CC2650.

I would like to communicate between two CC2650(One as End device other one as Coordinator(ZNP+Ztool))

With the help of Zstack documents and some answers from this forum I am able to set up below test environment.

1. Sample Switch (CC2650 End Device) :

I have flashed "Sample Switch" application in this device in LCD screen able to see below lines

"Up : ToggleLight"

"Rt : EZ-Mode"

"Select: Main"

2.  Sample Light (Ztool+ZNP) :

- I have flashed "znp_coordinator_pro.hex" 

- In Ztool script window executed "znp-bringup.zjs" with proper COM port changes.

- in Ztool, I have given ZB_PERMIT_JOINING_REQUEST with time-out value as 0xFF(Allow always for joining)

- in Ztool , I have given UTIL_GET_DEVICE_INFO and the response was

<TX>07:30:03.86 COM35 UTIL_GET_DEVICE_INFO (0x2700)

<RX>07:30:03.88 COM35 UTIL_GET_DEVICE_INFO_RESPONSE (0x6700)
    Status: SUCCESS (0x0)
    IEEEAddr: 0x00124B0007BAC004
    ShortAddress: 0x0000
    DeviceType: COORDINATOR (0x1)
    DeviceState: DEV_ZB_COORD (0x9)
    NumAssocDevices: 0x00
    AssocDevicesList

Could I assume that Zigbee Coordinator is successfully started?

Can anyone help me to make communication between end device and Coordinator?