Dear Support:
I have used zStack package of OTA_boot.ewm (boot-image boot manager) and download to the demo board of cc2538 & smatRF06 EB,
and I can't go into the main function.
and if I use the sampleswitch-enddevice-otaclient-imageA-withbootloader and do the OTA process communicate with OTA_DONGLE project, the OTA process is successful, but the device after the OTA the normal function is not ok, I should
re-download the firmware and it will ok.
Can you do the same thing for me to check the issue?
thank you very much.
BR,