I doing tests on rc2400hp module cc2350 znp processor
the following are the issues I am facing this. I am using api mode for data transfer
1. Failed to get expected routing table response (ZDO_MGMT_RTG_RSP) from the coordinator for ZDO_MGMT_RTG_REQ.
2. While transmitting 6 different broadcast packets (with packet size 94 bytes) at a time, unknown response from the coordinator (Status return value : 0x1A).
3. While transmitting more than 1 packet in unicast (with packet size 94 byte) at a time, SRSP and ZB_SEND_DATA_CONFIRM are received unevenly, which are not equal to the no.of packets being transmitted.
4.how to disable the nwk layer security key so that I can send 99 bytes payload