This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TA,
Thanks for the link. We do have the tools to tune the trace impedance. Since our board thickness is different, the helical antenna may not be properly centered for 868MHz operation and the matching network and/or the physical properties of antenna might need to be modified. Original design has a board thickness of 0.8mm while our board is 2.2mm thick. Can you offer some guidance on how to go about it? If there are any formulas that we can use to fine tune the design or any electromagnetic simulations that you can help us with then that would be great.
For cross reference, there is a similar thread
but we would like to have first pass success rather than trial and error.
Regards,
- Pushkar