I am searching ZIGBEE module which has support of different OS's like Contiki,Linux,Zephyr and RIOT for iotivity frame work. please suggest any Zigbee module with above specs.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi YK Chen,
Can u please tell me, from above mention OS's which OS supports this CC2650MODA Module?
Hi YK Chen,
Thanks for ur reply.
I want to implement Z-Stack in Contiki OS, for that i have downloaded Z-stack and Zigbee 3.0 SDK from TI, so now how to move forward, do u have any documents or blocks related to the same,if yes please provide me.
Hope u will give some idea...!!!!!!
Thanks & Regards,
Akshay YAdawar
sorry for the last mail,
I have one doubt every time ur mentioning zigbee in OS list......
Actually i want a zigbee module with zigbee stack and my requirement is to run the stack in my PC using any one OS(Contiki,Linux,Zephyr and RIOT).
For that the zigbee module should support any one OS than only i can use and zigbee is in application level.
akshay
Contiki and Zigbee are two different SW stack. You can either run Contiki or Zigbee on CC2538 but not both concurrently on it.
Hi YK Chen,
Now I am trying to Build TI Z-Stack Linux Home Gateway for x64 Linux(64-bit ubuntu).
Can u please tell me the procedure for building the stack,
I am following this link: sunmaysky.blogspot.in/.../build-ti-z-stack-linux-home-gateway.html
Getting some issues in above link can u please share steps or any other link...
Akshay Yadawar
Hi,
Z-STACK-HOME (Zigbee Home Automation Solution) and Z-STACK-3.0.0 both stacks are different ???
1. As you told Z-STACK-3.0.0 will not work on ubuntu 32-bit machine,
2. Z-STACK-HOME which has support of LINUX platform? If YES, on which ubuntu machine it will work 64-bit OR 32-bit?
3. Z-STACK-HOME has latest version of zigbee 3.0 and HA profile ?
please reply me..
aksahy
Hie YK Chen,
1. Is there any zigbee module without controller, i need only radio module which supports TI Z-stack 3.0 and Z-Stack Linux gateway.
2. Want to build a Z-stack in Host machine and through any serial interface, i will connect zigbee radio module for sending the data on-air.
akshay