Other Parts Discussed in Thread: CC2650
Tool/software: TI-RTOS
I have a perfectly functioning build in the IAR IDE, but I need to automate builds for testing and with the following command line:
C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.2\common\bin\IarBuild.exe" msa_cc2650.ewp MyDebugConfig
from the location:
C:\MeRepo\MyProject\CC26xx
I'm getting the following error message (added CRs to help with readability):
Building configuration: msa_cc2650 - MyDebugConfig
Updating build tree...
Variable expansion failed for Pre-Build command line.
Offending text:
"
"$PROJ_DIR$\version.bat"
"$PROJ_DIR$" & "$XDCROOT$/xs"
--xdcpath="$XDCPATH$" iar.tools.configuro
-c "$TOOLKIT_DIR$"
--cc "$COMPILER_PATH$"
--device "$DEVICE$"
--compileOptions $COMPILER_ARGS_ROOT_QUOTED$
--linkOptions $LINKER_ARGS_QUOTED$
--profile release
--projFile "$PROJ_PATH$"
"
My project directory looks like
C:\MeRepo\MyProject\
--source <<<sub directory>>>
--CC26xx <<<sub directory>>>
msa_cc2650.eww
msa_cc2650.ewp
version.bat
----MyDebugConfig <<<This sub directory gets created under --CC26xx when I build configuration in the IDE>>>
I've also tried executing:
"C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.2\common\bin\IarBuild.exe" CC26xx\msa_cc2650.ewp MyDebugConfig
from
C:\MeRepo\MyProject\
and I get the same results. The error message is a bit thin. Is there a way to get more details? My pre build BAT file works just fine in the IDE so I'm not clear on the next steps?
thanks