Other Parts Discussed in Thread: CC2530, CC3200, , Z-STACK
Hi,
I have setup as below,
- CC2530 on Smartrf05 hardware, Home automation sample switch is downloaded on it.
- It will act as coordinator.
- On the other side I have, ZNP(cc2650 on smartrf06) + ZAP (cc3200 LaunchPad).
- ZNP code is standard code from TI given in ha1.2 folder. It will work as router.
- ZAP code is non profile generic code for metering cluster as per SWRA444 doc from TI.
- ZNP used is from HA1.2 folder.
- This code works well with metering as well as HA clusters as coordinator and router with same znp stacks on both side.
- Now I have connected 2 bulbs via GPIO to CC3200 ZAP .
I have following queries ,
- I want to connect my above router setup(point no 3) to coordinator (above point no 1). It is not connecting.
- My router gets stuck at , as per TI swra444 doc,
- What changes should I make in my code. Since I have different TC link Key in my generic code.
- Secondly is it possible to get commands from coordinator to control individual bulb separately from multiple bulbs connected via gpio(non zigbee bulbs).
- If yes please tell me the registration method and ZAP commands and their sequence to ZNP.