This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2530: little help with AF_DataRequest in zigbee

Part Number: CC2530
Other Parts Discussed in Thread: CC2531

hi

till now i have a coordinator that it is znp 

and a router that i use inner 8051 and run samplelight project on it

i wrote these lines

  bdb_setChannelAttribute(true,0x2000);
  bdb_setChannelAttribute(false,0x0000);

  bdb_initialize ();
  afRegister(&DoorSensorEndPoint);
  
  
  bdb_StartCommissioning(BDB_COMMISSIONING_MODE_NWK_STEERING);

when this event is occured 

DEV_ROUTER Device joined, authenticated and is a router

i rcieved this line in coordinator in znp

FEh 0Ch 45h CAh 62h 0Fh 94h 60h 6Bh 0Fh 00h 4Bh 12h 00h 00h 00h 27h 


im just recieving ZDO_TC_DEV_IND but never recieved ZDO_END_DEVICE_ANNCE_IND

why is that?

what should i do?