Other Parts Discussed in Thread: Z-STACK, CC2538, , CC2530
Hello friends,
I am trying to configure a simple ZigBee network using ZNP method.
I have done the following.
1 - Build and Flash the unmodified ZNP program from Z-stack 3.1 with the following DEFINED SYMBOLS:
HAL_UART_USB USB_SETUP_MAX_NUMBER_OF_INTERFACES=5 xHAL_SPI=TRUE xHAL_UART=TRUE BDB_FINDING_BINDING_CAPABILITY_ENABLED=0 TC_LINKKEY_JOIN ewarm CC2538_USE_ALTERNATE_INTERRUPT_MAP=1 CC2538ZNP ZNP_ALT xPOWER_SAVING FEATURE_SYSTEM_STATS FEATURE_RESET_MACRO ZDNWKMGR_MIN_TRANSMISSIONS=0 MT_UART_DEFAULT_OVERFLOW=FALSE ASSERT_RESET FAKE_CRC_SHDW ZCL_READ ZCL_DISCOVER ZCL_WRITE ZCL_BASIC
2 - Using Z-Tool and following the tutorial in I also refer to the post and
3 - This is the screen shoot of my Z-Tool Commands.
As you can see, I cannot establish the network on my Coordinator (COM12) thus, Router (COM8) cannot join. I can't quite identify where is the problem despite trying many times. I am using Windows 10 FYI.
It would be very great if someone can help pointing me into the right direction.
Thank you very much,
Alex