Other Parts Discussed in Thread: CC2650, Z-STACK
ZigBee H/W :
Chip Sets
Coordinator CC2538 1
Router CC2538 1
End Device CC2650 400
SDK : Z-Stack Home 1.2.2a.44539
Situation :
1. Router , Coordinator power on.
2. After Router join to Coordinator network, then the coordinator can’t be joined any other device.
3. MCU ( Linux Base )use Uart communication with CC2538 ( USB Uart – TI ZNP Protocol )
4. 400 set of End device power on at the same time, and start join to Router.
5. If end Device Join network already, then send information to Router and Router report information thought USB Uart to MCU.
We find out two issue as below :
Question 1 :
400 End Device's power on, and start join network. But almost end device's join to network over 30 min.
When power on the 400 sets of device at the same time, it seems stock by an un-certain situation, takes over 30 min to finish most device to join the router, some devices else still can’t join to the router.
Status:
Keep waiting, the router still can’t be joined by any end device it these device did not join in, and cmd no any respond.
Question 2 :
400 end device's can’t join to network totally ( test for 5 times, every time, approx 40 sets of device can’t join to the network )
Status :
1. during the joining period, some end device’s will be crashed.
2. After Joining to network, End device’s RF Tx/Rx is OK, but using the ICall ZStack feedback the Device State, the Device State got abnormal status.