Other Parts Discussed in Thread: CC2530, CC2531
Hi,
I'm doing some TX/RX tests between CC2538 and CC2530.
I've noticed that transmitting with CC2538 is much slower compared to transmitting with CC2530. CC2538 seems to deliver packets with a frequency of ~1 second.
Receiving is not a problem with both CC2538 and CC2530 as if I transmit from CC2530, CC2538 seems to receive packets at the same frequency CC2530 deliver them.
Why CC2538 is slower in TX? That is a huge problem for my application as I'm using CC2538 as coordinator which will also be responsible for upgrading devices via OTA and that will take ages.
Any help would be very much appreciated.
Thanks,
John