Other Parts Discussed in Thread: Z-STACK, CC-DEVPACK-DEBUG, CC2650, Z-STACK-ARCHIVE, CC2630
Tool/software: Code Composer Studio
Hello everyone,
I tried to read on this forum and on the DIGI International forum but it is not clear how to solve the problem.
I bought some CC2650STK cards and the CC-DEVPACK-DEBUG; the idea is to use CC2650STK as END-DEVICE (ZED) in a Zigbee network.
The network topology that I intend to use is simple:
- The DIGI CPX4 gateway is configured as a coordinator of the Zigbee network.
- CC2650STK modules as END-DEVICE Zigbee.
The CPX4 Gateway must be able to see the sensor nodes (CC2650STK) and receive the following information from them:
- Battery level
- Temperature value
- Humidity value
- Acceleration value *
* The idea is to read the acceleration values for tot seconds (for example 5 seconds) and send: average, min and max.
I saw that from the Android application (or OS) there is the possibility to download the Zigbee firmware to be uploaded to CC2650STK; this is not enough (at least in the initial phase) to be able to read from the gateway (coordinator) CPX4?
After implementing this (when the previous steps have been implemented) I need to:
- Change the configuration of the CC2650STK on the fly (OTA) via the CPX4 (for example, simply change the "reading range" from the modules).
Thanks to everyone!