Other Parts Discussed in Thread: Z-STACK, ,
Hello
I'm trying to talk to a CC2530 using the ZNP Stack and uart.
To do this, I flashed CC2530ZNP-with-SBL.hex from C:\Texas Instruments\Z-Stack 3.0.1\Projects\zstack\ZNP\CC253x\dev
I found two documents about ZNP usage.
Version 1.0 (02/2015): e2echina.ti.com/.../3731.Z_2D00_Stack-ZNP-Interface-Specification.pdf
version 1.1 (11/2016): from my ZStak 3.0.1 installation
Version 1.1 difference is (from document history) : "Update ZNP usage and definitions to Z3.0 stack. Removed support for SPI."
I wired it as stated in 2.2.1.1.4 (page 13) of the second document. CTS is grounded. CFG0 to gnd. CFG1 usage is not discussed in this doc but I connected it to ground too (based on the other 1.0 document)
I apply a low level on reset for one second and... nothing happens. I should receive SYS_RESET_IND
So my questions are :
- Did I flash the right hex file?
- Did I use the right array for wiring ( 2.2.1.1.4 )?
- what about CFG1 which is still described as an input in the documentation?
- Anything else I could have forgoten?
Thanks
Julien