Part Number: CC2538
Other Parts Discussed in Thread: Z-STACK
Tool/software: TI-RTOS
Hi,
We are trying to do OTA upgrade in cc2538 between Coordinator and router. Its happening but very slowly. 0.02% per sec it's transferring. The total size of .zigbee file is 145kb.
It's happening till 0.30% to 0.80% only, after that we are getting the below error (Attached Image).
Error: OtaServer Firmware Timeout
if this message appears just after program start
please confirm that the port settings are correct
the com port has been automatically closed
how to solve this problem?
Thanks in advance,
shiva