Other Parts Discussed in Thread: Z-STACK
Do we need to revise ZDSECMGR_TC_DEVICE_MAX if we want to add more than 40 ZHA 1.2 devices into Z-Stack 3.0.1 coordinator (CC2530)? Let's say we use default ZDSECMGR_TC_DEVICE_MAX which is 40 on ZC of Z-Stack 3.0 and I have 20 ZHA 1.2 ZRs and 140 ZHA 1.2 ZEds to join this Zigbee 3.0 ZC. Do I have to increase ZDSECMGR_TC_DEVICE_MAX to 160 or there is no need to do such revision. Besides, if all those 20 ZRs and 140 ZEDs run Zigbee 3.0 instead of ZHA 1.2, I think we have to revise ZDSECMGR_TC_DEVICE_MAX to 160, right?