Looking for better solution which help to create a bridge which create understanding between mesh network IEEE standards and WIFI network IEEE standards so that it will help me to connect the sensor SHT31 connected with mesh transmitter which transmit the readings of sensor and should be receive by some device which help to send and store it to internet cloud database
Major Problem Right now I am facing is connecting a mesh module with sensor at one end (as router) to transmit the readings and connecting one more mesh module with raspberry pi at another end (as coordinator)to receive the readings and then create the path which help the readings to send it to cloud
Is there any better and cheaper suggestions which help me to connect to internet cloud much more easily ?
Will be looking for you helpful leads.