This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630: When Vin 3.3V, No RF signal and Vin 3V is OK

Part Number: CC2630

Hi,

We used CC2630F128RGZR(7X7) for Zigbee node. We met a issue when debug.

When Vin=3.3V, there is no RF singal and can't networking. But when hand touch the PCB trace antenna, The RF is OK.

When Vin=3V, The RF is OK.

We tested CC2630EVM and it is OK.

PS: The PCB is smaller than CC2630EVM and two layers.

Could you kindly help to check the issue and give some suggestions. Thanks.

Schematic

Thanks

Walsh