Other Parts Discussed in Thread: , TIMAC
HI,guys
I am using CC2530 to send packet,point to point communication
Working with IAR workbench 8051
Packet testing with TI packet sniffer
The function(basicRfPacketIsReady) could work when i without config SECURITY_CCM(Test with breakpoint)
Unfortunately,it does not work when i config it
My sniffing result display:
Sequence number:increasing when i send packet
FCS:Both(TX/RX) are OK
ACK:Got it
So i have no idea why basicRfPacketIsReady() function return false continuously
Sequence numbers error?I can'y find any parameter to defind or change it
Does anyone solve the problem?Thanks