Browse By Tags

  • OPA859: NC pin

    Other Parts Discussed in Thread: OPA859

    Hello,

    I have questions about NC pin of OPA859. OPA859 pin2 is NC, means not connect,  datasheet explain user not connect this pin to any circuit. But nc has a little ambiguous meaning for user, is nc means opa859…

  • OPA857-DIE: Transimpedance amplifier

    Part Number: OPA857-DIE
    Other Parts Discussed in Thread: OPA857, , OPA855, LMH32401, OPA858, OPA859, OPA856

    Hello,

    I was wondering if there are any experimental/test data about this device?

    I would expect the input capacitance to be affected by the packaging…

  • OPA356: Amplification for Ultrasonic NDT Signal

    Part Number: OPA356
    Other Parts Discussed in Thread: LMP7718, THS4551, OPA838, OPA365, LMH6703, OPA859, OPA858

    Hello,

    I am developing an ultrasonic sensor for NDT testing, specifically with the goal of measuring the thickness of metal.  I am using a 5MHz…

  • RE: OPA859: FB pin of OPA859

    Hello Ikuo-san,

    I am glad my explanation was able to assist you.  If you ever have any additional questions regarding high-speed parts, please know you can always ask here.

    Best Regards,

    Alec  

  • RE: OPA859: FB pin of OPA859

    Hello Alec-san,

    Thank you for your reply.

    I failed to attach the figure, however I am very satisfied with your answer.

    The detailed explanation of 1) was very helpful.
    Also, thank you for agreeing to 2).

    Best Regards,

    Ikuo

  • RE: OPA859: FB pin of OPA859

    Hello,

    The questions you asked are good ones to discuss, I will do my best to help below.  I have a shorter section at the bottom with less explanation.  Also, your images you attached did not post/are not visible.  If you would like, you could repost/edit…

  • OPA859: FB pin of OPA859

    Part Number: OPA859

    Hello,

    I have two questions FB pin of OPA859.

    1) At "6 Pin Configuration and Functions" of datasheet,

        FB pin is I (input).

       However, in Figure 50, the FB pin is connected to the output of the amplifier, so it looks like…

  • RE: WEBENCH® Tools/OPA859: PSPICE model for OPA859

    Hello Sima,

    Thank you for your reply. I could simulate of OPA859.

    Your answers and training videos were very helpful.

    Thank you very much,

    Ikuo

  • RE: WEBENCH® Tools/OPA859: PSPICE model for OPA859

    Hello Ikuo,

       It looks like the OPA859 is one of TI devices that has not yet been loaded into Pspice for TI. I believe they are working on importing all TI models into this software. In the meantime you can import the OPA859 .lib file into Pspice for TI…

  • WEBENCH® Tools/OPA859: PSPICE model for OPA859

    Part Number: OPA859
    Other Parts Discussed in Thread: TINA-TI

    Tool/software: WEBENCH® Design Tools

    Hi, 

    I would like to simulate OPA859 with PSPICE for TI. I searched for PSPICE for TI but couldn't find OPA859. Is there a PSPICE model?

    ikuo

  • [FAQ] Transimpedance Amplifier Calculator

    Use the following link to access the calculator: 

    TIA Calculator

  • RE: OPA857EVM-978: OPA857EVM

    Hello Andrea,

    Kai's simulations should give you an idea of what to expect for transient simulations. I don't think the OPA857 is the correct device to use here as an integrator since the feedback is limited to either 20kohms or 5k-ohms. You can use the…

  • 高速アンプを用いた設計によくある3つの疑問

    高速アンプを使って設計する際には、共通の仕様に精通し、考え方をある程度理解しておくことが重要です。この技術記事では、ゲイン帯域幅積(GBW)が50MHz以上を高速オペアンプとしますが、それ以下の速度のデバイスにもここで紹介する考え方が当てはまる場合もあります。高速アンプを用いる場合に設計者がよく抱く疑問をいくつか紹介していきます。

    Q:一部の高速オペアンプの仕様に最小ゲインが規定されているのはなぜですか?

    A不完全補償型オペアンプには閉ループの最小ゲイン安定仕様がありますが、ユニティ・ゲイン安定アンプと比べて不完全補償型オペアンプは…

  • 고속 증폭기를 사용해서 설계할 때 흔히 하는 3가지 질문

    Other Parts Discussed in Post: OPA858, THS3491

    모든 증폭기 디자인이 동일하게 설계되지 않으므로, 고속 증폭기를 사용해서 설계할 때는 주요 사양과 특정한 측면들을 이해하는 것이 중요하다. 이 글에서 고속 증폭기는 이득-대역폭 곱(GBW)이 50MHz 이상인 연산 증폭기를 말한다. 여기서 설명하는 내용은 저속 증폭기에도 마찬가지로 적용할 수 있다. 그러면 고속 증폭기를 사용해서 설계할 때 디자이너들이 흔히 하는 질문…

  • 3 common questions when designing with high-speed amplifiers

    Other Parts Discussed in Post: OPA858, OPA859, THS3491

    Not all amplifier designs are created equal, and it’s important to be familiar with common specifications and understand certain concepts when designing with high-speed amplifiers. In the context of…

  • RE: OPA659: Question about current noise

    Hello George,

    Please use the 1.8fA/rtHz of the OPA659 as an initial flatband number of the current noise that will rise over frequency. Current noise at 10MHz will be closer to the magnitude of the OPA859 rather than 1.8fA/rthz.

    Best,

    Hasan Babiker

  • RE: OPA659: Question about current noise

    If that is the case, the OPA659 data sheet is way off because it shows a current noise of 1.8fA/rtHz at 10MHz whereas the OPA859 has ~0.8pA/rtHz at 10MHz.  Which one am I supposed to believe?  Or are they both wrong?

  • RE: OPA659: Question about current noise

    Hello George,

    The plot on the OPA859 datasheet is a more accurate representation of how the current-noise will behave on the OPA659.

    Best,

    Hasan Babiker

  • RE: OPA659: Question about current noise

    The plot in the OPA859 data sheet is what prompted me to ask the question.  It is not clear to me if it applies to CMOS transistors only or if it applies to JFETs as well.  Figure 22 in the OPA659 data sheet shows the current noise constant up to 10MHz…

  • RE: LM7171: High gain bandwidth product OP Amp

    Incidentally, the OPA859 is one option - 

  • RE: OPA659: Question about current noise

    I see this plot in the OPA859, certainly a designer sim and not likely in the TINA model,

    TheOPA659 might be similar but only a designer sim would tell, 

      

  • RE: OPA659: Question about current noise

    That is right if the current noise remains close to 1.8fA/rtHz.  For the OPA859, the current noise is <1fA/rtHz at low frequency but it increases to ~4pA/rtHz at 100MHz.  That much current noise is unacceptable for my application, so I need to know how…
  • THS4631: What is the capacitance to "ground" on the Vp and Vn pins of the opamp from the datasheet spec of 3.9pF

    Part Number: THS4631
    Other Parts Discussed in Thread: OPA1652, OPA859, OPA350, OPA656, OPA810, OPA832, OPA659, OPA695

    What is correct interpretation of Common Mode Input Resistance in datasheet 10^9 || 3.9 Ohms || pF in the THS4631 opamp datasheet.

    What…

  • RE: WEBENCH® Tools/OPA859: Why is the Gain Bandwidth required in the Filter Design Tool Always so high?

    Hi kai, 

    any Idea why I'm seeing clipping at the output when I increase the amplitude of the signal? With a signal of amplitude 20m, I'm seeing clipping at 2.4V. I would have expected a peak of 2.65V.