Other Parts Discussed in Thread: TCAN1043-Q1
Hi,
Since these parts are p2p, no issues on the hardware side. From the software perspective, what are the differences? Anything particular that would require additional attention…
Hi,
Since these parts are p2p, no issues on the hardware side. From the software perspective, what are the differences? Anything particular that would require additional attention…
Hello,
Please check if the below my understanding about wake-up request is correct:
In stand-by state, when wake-up request is made, nFAULT pin goes Low but no state transition occurs.
In go-to-sleep state, when wake-up request…
Hello Team,
I have a query form my customer on TCAN1043-Q1
Can you please confirm the expected behavior for TCAN1043 during STG and STB for individual lines – CANH / CANL
Hi Team,
i have several questions about our TCAN devices, please kindly help to answer. Thanks.
Hi Experts,
What's the maximum Ground shif voltage that TCAN1043 can support? Can we pass +/-7V GND shift test? Thank you.
Arie
Hi Team,
There is a good new that we could DIN TI product!
Could TCAN1043-Q1 support 5M ? THX
Hi Team,
Now customer use TJA1043T/1J !!!
I currently want to recommend TCAN1043A-Q1 & TCAN1043-Q1 to customers!
Can you provide the comparison table and advantages and disadvantages…
Hi,
We are using TCAN1043-Q1 in the design. In the datasheet, for the local faults it is provided that the nFault pin will be low only when IC is transitioned from Normal mode to silent mode. Which means, the processor/microcontroller…
I am using TCAN1043-Q1 with TMS570LS1224PGE device.
Can I please get a CAN communication code example for TMS570/ any MCU device with the TCAN1043 ?
As I am a beginner , please tell…
Hi Team,
Now customer need TI solution to replace UJA1164 !
Do we have a solution to replace UJA1164 ? THX
Below is UJA1164 datasheet
Hi Team,
The customer has drawn up a schematic for EN control.
I connected TCAN1043 INH pin and LM5160 EN pin directly, is there any problem?
TCAN1043-Q1 INH pin spec

Delete…
Hi team,
Could you tell how to deal with WAKE-pin when it is not used?
Regards,
Noriyuki Takahashi
Hello,
What's the max voltage ripple of a 5V power supply that the TCAN1043 can operate without issues?
Is 100mVpp (1KHz) acceptable?
Any rough estimate on a max value & also advice to minimize that ripple would be appreciated…
Hi Teams
Customer is using TCAN1043-Q1 in their new project and have few questions about SLEEP mode control.
The power supply connection is the same like below diagram in datasheet.
When we enter the SLEEP mode through MCU output…
Hi,
I want to use TCAN1043DQ1 to replace TJA1043T. Could you provide a comparison table between the two? THX
Hello,
My customer is looking for alternative device of NXP TJA1043TK.
PKG is VSON.
I have TI TCAN1043XXX-Q1 device inventory having device top marking as follows.
Is this device P2P compatible with NXP TJA1043TK?
TJA1043TK…
Hi Srivatsan,
1. You understanding of the Vsup is correct in that it allows the device to operate and keep a low-power receiver active while Vcc is unavailable. However, the Vsup supply is critical to device operation and will be deactivated (or in a…
Hi,
1. This CAN transceiver "TCAN1043-Q1" has VBAT pin for battery supply that is powering an internal LDO.I assume that this supply acts as a backup when VCC is cut off. Is it possible to use this IC without providing…
Monisha,
1. Do you mean SIL certification for the transceiver itself? No, this won't be possible. But if you mean the end product, then yes some of our CAN transceivers can aid in ASIL ratings with the right documentation. For the SN65HVD257 device I…
Diamond,
If you email me directly I can share more information about this particular topic. You can find my email by clicking my username. For now, I will close this thread.
Regards,
Eric Hackett
Hi
In the ground shift test, we found that bus diagnosis function in a ground shifting situation, CAN transceiver error pin may be triggered which is a misdiagnosis.
We also do the same test on CAN transceivers from other supplier…
Hi Fujiwara-san,
1. Low-side switch configuration(Figure 23 in TCAN1043-Q1 datasheet p30) is for falling edge detection, right?
The WAKE pin is sensitive to both rising and falling edges, so both configurations depicted will work. In the case of the low…
Hi Eric-san,
I have more question.
1. Low-side switch configuration(Figure 23 in TCAN1043-Q1 datasheet p30) is for falling edge detection, right?
2. Regarding equation 3 for Rbias (TCAN1143-Q1 datasheet p30), would you please tell about Iih?
3. TCAN1145-Q1EVM…
Hi Aki,
Our equivalent device would be TCAN1145. There are two other variants, TCAN1144 and TCAN1146, which offer different feature sets. See page 3 on the datasheet for a feature table of these three devices.
Note that while these are all pin-to-pin…
Customer is looking for the replacement for TJA1145T, but TCAN1043 does not have the SPI feature. Could you please help further check it? Thank you.