U-Boot SPL 2013.04-dirty (Jul 10 2013 - 14:02:53) musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Peripheral mode controller at 47401000 using PIO, IRQ 0 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Host mode controller at 47401800 using PIO, IRQ 0 OMAP SD/MMC: 0 mmc_send_cmd : timeout: No status update reading u-boot.img reading u-boot.img U-Boot 2013.04-dirty (Jul 10 2013 - 14:02:53) I2C: ready DRAM: 512 MiB WARNING: Caches not enabled NAND: No NAND device found!!! 0 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - readenv() failed, using default environment musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Peripheral mode controller at 47401000 using PIO, IRQ 0 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Host mode controller at 47401800 using PIO, IRQ 0 Net: not set. Validating first E-fuse MAC cpsw, usb_ether Hit any key to stop autoboot: 0 gpio: pin 53 (gpio 53) value is 1 mmc0 is current device micro SD card found mmc0 is current device gpio: pin 54 (gpio 54) value is 1 SD/MMC found on device 0 reading uEnv.txt 788 bytes read in 7 ms (109.4 KiB/s) Loaded environment from uEnv.txt Importing environment from mmc ... Running uenvcmd ... mmc_send_cmd : timeout: No status update mmc1(part 0) is current device mmc_send_cmd : timeout: No status update mmc0 is current device 4134232 bytes read in 716 ms (5.5 MiB/s) Booting from external microSD... 28978 bytes read in 81 ms (348.6 KiB/s) ## Flattened Device Tree blob at 80f80000 Booting using the fdt blob at 0x80f80000 Using Device Tree in place at 80f80000, end 80f8a131 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Initializing cgroup subsys cpu [ 0.000000] Initializing cgroup subsys cpuacct [ 0.000000] Linux version 3.16.0-rc6-00141-g361f018-dirty (laurens@laurens) (gcc version 4.9.2 20140904 (prerelease) (crosstool-NG linaro-1.13.1-4.9-2014.09 - Linaro GCC 4.9-2014.09) ) #19 SMP Tue Nov 25 10:36:43 CET 2014 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=50c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine model: TI AM335x BeagleBone [ 0.000000] Memory policy: Data cache writeback [ 0.000000] HighMem zone: 1048574 pages exceeds freesize 0 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (sgx neon ) [ 0.000000] PERCPU: Embedded 8 pages/cpu @dfabd000 s8448 r8192 d16128 u32768 [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129792 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] allocated 1046528 bytes of page_cgroup [ 0.000000] please try 'cgroup_disable=memory' option if you don't want memory cgroups [ 0.000000] Memory: 510680K/523264K available (3581K kernel code, 426K rwdata, 2160K rodata, 220K init, 356K bss, 12584K reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xffe00000 (2048 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf800000 - 0xbfe00000 ( 6 MB) [ 0.000000] .text : 0xc0008000 - 0xc05a3914 (5743 kB) [ 0.000000] .init : 0xc05a4000 - 0xc05db100 ( 221 kB) [ 0.000000] .data : 0xc05dc000 - 0xc0646bc0 ( 427 kB) [ 0.000000] .bss : 0xc0646bc8 - 0xc069fe58 ( 357 kB) [ 0.000000] Hierarchical RCU implementation. [ 0.000000] RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1. [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1 [ 0.000000] NR_IRQS:16 nr_irqs:16 16 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000014] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956969942ns [ 0.000042] OMAP clocksource: timer1 at 24000000 Hz [ 0.000404] Console: colour dummy device 80x30 [ 0.000441] Calibrating delay loop... 548.86 BogoMIPS (lpj=2744320) [ 0.049076] pid_max: default: 32768 minimum: 301 [ 0.049288] Security Framework initialized [ 0.049377] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.049396] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.050591] Initializing cgroup subsys memory [ 0.050768] Initializing cgroup subsys net_cls [ 0.050818] Initializing cgroup subsys blkio [ 0.050915] CPU: Testing write buffer coherency: ok [ 0.051372] CPU0: thread -1, cpu 0, socket -1, mpidr 0 [ 0.051484] Setting up static identity map for 0x80359060 - 0x803590ac [ 0.053402] Brought up 1 CPUs [ 0.053420] SMP: Total of 1 processors activated. [ 0.053434] CPU: All CPU(s) started in SVC mode. [ 0.054384] devtmpfs: initialized [ 0.061648] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.082665] omap_hwmod: tptc0 using broken dt data from edma [ 0.082893] omap_hwmod: tptc1 using broken dt data from edma [ 0.083107] omap_hwmod: tptc2 using broken dt data from edma [ 0.089199] omap_hwmod: debugss: _wait_target_disable failed [ 0.147467] pinctrl core: initialized pinctrl subsystem [ 0.148164] regulator-dummy: no parameters [ 0.166558] NET: Registered protocol family 16 [ 0.167385] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.168979] cpuidle: using governor ladder [ 0.169090] cpuidle: using governor menu [ 0.179583] platform 49000000.edma: alias fck already exists [ 0.179618] platform 49000000.edma: alias fck already exists [ 0.179645] platform 49000000.edma: alias fck already exists [ 0.180974] OMAP GPIO hardware version 0.1 [ 0.193787] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.228066] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver [ 0.228704] vmmcsd_fixed: 3300 mV [ 0.231605] SCSI subsystem initialized [ 0.232213] usbcore: registered new interface driver usbfs [ 0.232377] usbcore: registered new interface driver hub [ 0.232704] usbcore: registered new device driver usb [ 0.233360] omap_i2c 44e0b000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2c0_pins, deferring probe [ 0.233400] platform 44e0b000.i2c: Driver omap_i2c requests probe deferral [ 0.233590] media: Linux media interface: v0.10 [ 0.233723] Linux video capture interface: v2.00 [ 0.233911] pps_core: LinuxPPS API ver. 1 registered [ 0.233927] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.234726] Advanced Linux Sound Architecture Driver Initialized. [ 0.236142] lo:Netpoll enabled. [ 0.236162] lo: Called set_rx_mode... [ 0.236174] Called set_rx_mode...success [ 0.236721] Switched to clocksource timer1 [ 0.257828] Protocol ipv4 registered (layer: 3). [ 0.257855] Protocol ipv6 registered (layer: 3). [ 0.257870] Protocol icmp4 registered (layer: 4). [ 0.257884] Protocol udp registered (layer: 4). [ 0.257899] Protocol tcp registered (layer: 4). [ 0.258189] PicoTCP created. [ 0.258245] NET: Registered protocol family 2 [ 0.258285] picoTCP: Created /proc/net/route. [ 0.258306] picoTCP: Created /proc/net/stack. [ 0.258352] NET: Registered protocol family 1 [ 0.259256] hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters available [ 0.262803] futex hash table entries: 256 (order: 2, 16384 bytes) [ 0.265305] VFS: Disk quotas dquot_6.5.2 [ 0.265418] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.266058] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. [ 0.266489] msgmni has been set to 997 [ 0.266911] Device lo created. [ 0.270388] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 249) [ 0.270423] io scheduler noop registered [ 0.270447] io scheduler deadline registered [ 0.270495] io scheduler cfq registered (default) [ 0.271874] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568 [ 0.274332] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.277482] omap_uart 44e09000.serial: no wakeirq for uart0 [ 0.277773] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 88, base_baud = 3000000) is a OMAP UART0 [ 0.951542] console [ttyO0] enabled [ 0.957212] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20 [ 0.964548] [drm] Initialized drm 1.1.0 20060810 [ 0.984737] brd: module loaded [ 0.995756] loop: module loaded [ 1.003364] usbcore: registered new interface driver asix [ 1.009301] usbcore: registered new interface driver ax88179_178a [ 1.015834] usbcore: registered new interface driver cdc_ether [ 1.022180] usbcore: registered new interface driver smsc95xx [ 1.028387] usbcore: registered new interface driver net1080 [ 1.034485] usbcore: registered new interface driver cdc_subset [ 1.040873] usbcore: registered new interface driver zaurus [ 1.047205] usbcore: registered new interface driver cdc_ncm [ 1.054027] usbcore: registered new interface driver cdc_acm [ 1.060058] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters [ 1.068697] usbcore: registered new interface driver usb-storage [ 1.077937] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517 [ 1.086166] platform musb-hdrc.0.auto: Driver musb-hdrc requests probe deferral [ 1.095531] musb-hdrc musb-hdrc.1.auto: musb_init_controller failed with status -517 [ 1.103797] platform musb-hdrc.1.auto: Driver musb-hdrc requests probe deferral [ 1.113048] mousedev: PS/2 mouse device common for all mice [ 1.121690] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0 [ 1.129804] i2c /dev entries driver [ 1.134368] IR Sharp protocol handler initialized [ 1.139750] pps_ldisc: PPS line discipline registered [ 1.145285] Driver for 1-wire Dallas network protocol. [ 1.152544] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.249033] ledtrig-cpu: registered to indicate activity on CPUs [ 1.255752] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2 [ 1.263458] omap-sham 53100000.sham: hw accel on OMAP rev 4.3 [ 1.271729] hidraw: raw HID events driver (C) Jiri Kosina [ 1.283232] mmc0: host does not support reading read-only switch. assuming write-enable. [ 1.292891] usbcore: registered new interface driver usbhid [ 1.298896] usbhid: USB HID core driver [ 1.305018] NET: Registered protocol family 17 [ 1.310112] mmc0: new high speed SDHC card at address 0001 [ 1.316917] NET: Registered protocol family 15 [ 1.321693] Key type dns_resolver registered [ 1.326474] omap_voltage_late_init: Voltage driver support not added [ 1.333371] mmcblk0: mmc0:0001 ASTC 7.38 GiB [ 1.339609] cpu cpu0: cpu0 regulator not ready, retry [ 1.345140] mmcblk0: p1 p2 [ 1.348317] platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral [ 1.356419] ThumbEE CPU extension supported. [ 1.362645] Registering SWP/SWPB emulation handler [ 1.372200] registered taskstats version 1 [ 1.378660] slave hdmi: could not get i2c [ 1.383034] platform hdmi: Driver slave requests probe deferral [ 1.393140] platform 4830e000.lcdc: Driver tilcdc requests probe deferral [ 1.404566] DCDC1: at 1500 mV [ 1.409207] vdd_mpu: 925 <--> 1325 mV at 1100 mV [ 1.415370] vdd_core: 925 <--> 1150 mV at 1100 mV [ 1.421882] LDO1: at 1800 mV [ 1.426363] LDO2: at 3300 mV [ 1.430865] LDO3: 1800 mV [ 1.434893] LDO4: at 3300 mV [ 1.438135] mmc1: BKOPS_EN bit is not set [ 1.443550] tps65217 0-0024: TPS65217 ID 0xe version 1.2 [ 1.449388] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 1.456153] mmc1: new high speed MMC card at address 0001 [ 1.462111] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517 [ 1.471186] mmcblk1: mmc1:0001 MMC02G 1.78 GiB [ 1.476249] platform musb-hdrc.0.auto: Driver musb-hdrc requests probe deferral [ 1.484123] mmcblk1boot0: mmc1:0001 MMC02G partition 1 1.00 MiB [ 1.491250] musb-hdrc musb-hdrc.1.auto: musb_init_controller failed with status -517 [ 1.499593] mmcblk1boot1: mmc1:0001 MMC02G partition 2 1.00 MiB [ 1.507138] platform musb-hdrc.1.auto: Driver musb-hdrc requests probe deferral [ 1.515024] mmcblk1: p1 p2 [ 1.520621] cpufreq: __cpufreq_add_dev: CPU0: Running at unlisted freq: 550000 KHz [ 1.530176] mmcblk1boot1: unknown partition table [ 1.537481] cpufreq: __cpufreq_add_dev: CPU0: Unlisted initial frequency changed to: 600000 KHz [ 1.547772] mmcblk1boot0: unknown partition table [ 1.679496] tda998x 0-0070: found TDA19988 [ 1.684931] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 1.691914] [drm] No driver support for vblank timestamp query. [ 1.698534] tilcdc 4830e000.lcdc: No connectors reported connected with modes [ 1.706023] [drm] Cannot find any crtc or sizes - going 1024x768 [ 1.724266] Console: switching to colour frame buffer device 128x48 [ 1.738859] tilcdc 4830e000.lcdc: fb0: frame buffer device [ 1.744703] tilcdc 4830e000.lcdc: registered panic notifier [ 1.750612] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0 [ 1.757232] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517 [ 1.765399] platform musb-hdrc.0.auto: Driver musb-hdrc requests probe deferral [ 1.773596] musb-hdrc musb-hdrc.1.auto: musb_init_controller failed with status -517 [ 1.781834] platform musb-hdrc.1.auto: Driver musb-hdrc requests probe deferral [ 1.846765] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6 [ 1.853165] davinci_mdio 4a101000.mdio: detected phy mask fffffffe [ 1.860662] libphy: 4a101000.mdio: probed [ 1.864882] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720 [ 1.874910] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517 [ 1.883182] platform musb-hdrc.0.auto: Driver musb-hdrc requests probe deferral [ 1.891569] cpsw 4a100000.ethernet: Detected MACID = 1c:ba:8c:a1:e9:dc [ 1.899029] musb-hdrc musb-hdrc.1.auto: musb_init_controller failed with status -517 [ 1.908297] Assigned ipv6 fe80:0000:0000:0000:1eba:8cff:fea1:e9dc to device eth0 [ 1.916068] Device eth0 created. [ 1.919678] platform musb-hdrc.1.auto: Driver musb-hdrc requests probe deferral [ 1.927892] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517 [ 1.936047] platform musb-hdrc.0.auto: Driver musb-hdrc requests probe deferral [ 1.943814] net eth0: initializing cpsw version 1.12 (0) [ 2.027468] net eth0: phy found : id is : 0x7c0f1 [ 2.032471] libphy: PHY 4a101000.mdio:01 not found [ 2.037523] net eth0: phy 4a101000.mdio:01 not found on slave 1 [ 2.045042] eth0:Netpoll enabled. [ 2.048572] eth0: Called set_rx_mode... [ 2.053444] Called set_rx_mode...success [ 2.058299] musb-hdrc musb-hdrc.1.auto: musb_init_controller failed with status -517 [ 2.066463] platform musb-hdrc.1.auto: Driver musb-hdrc requests probe deferral [ 2.074660] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01 00:00:01 UTC (946684801) [ 2.090469] ALSA device list: [ 2.093595] No soundcards found. [ 2.098021] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517 [ 2.106187] platform musb-hdrc.0.auto: Driver musb-hdrc requests probe deferral [ 2.133260] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 2.141975] VFS: Mounted root (ext4 filesystem) readonly on device 179:2. [ 2.150826] devtmpfs: mounted [ 2.154347] Freeing unused kernel memory: 220K (c05a4000 - c05db000) Mount failed for selinuxfs on /sys/fs/selinux: No such file or directory [ 2.573991] random: init urandom read with 53 bits of entropy available [ 2.841318] init: plymouth-upstart-bridge main process (76) terminated with status 1 [ 2.850972] init: plymouth-upstart-bridge main process ended, respawning [ 2.981219] init: ureadahead main process (79) terminated with status 5 [ 2.992229] init: plymouth-upstart-bridge main process (86) terminated with status 1 [ 3.001436] init: plymouth-upstart-bridge main process ended, respawning [ 5.046919] Unable to handle kernel paging request at virtual address e02f8fe0 [ 5.054509] pgd = df3d8000 [ 5.057345] [e02f8fe0] *pgd=00000000 [ 5.061102] Internal error: Oops: 5 [#1] SMP THUMB2 [ 5.066212] Modules linked in: [ 5.069423] CPU: 0 PID: 70 Comm: kworker/0:2 Not tainted 3.16.0-rc6-00141-g361f018-dirty #19 [ 5.078285] Workqueue: events cache_reap [ 5.082402] task: df2ab980 ti: df3d0000 task.ti: df3d0000 [ 5.088062] PC is at free_block+0x32/0xd8 [ 5.092264] LR is at drain_array+0x59/0x80 [ 5.096559] pc : [] lr : [] psr: 000f01b3 [ 5.096559] sp : df3d1e78 ip : 0000001c fp : c0687cc0 [ 5.108589] r10: df5f8c20 r9 : 00000000 r8 : 2c9a4447 [ 5.114065] r7 : b269111c r6 : df5f8c20 r5 : 00000000 r4 : df27ba40 [ 5.120906] r3 : 007fffe0 r2 : dfaf9000 r1 : df5f8c20 r0 : fffffffe [ 5.127748] Flags: nzcv IRQs off FIQs on Mode SVC_32 ISA Thumb Segment kernel [ 5.135680] Control: 50c5387d Table: 9f3d8019 DAC: 00000015 [ 5.141701] Process kworker/0:2 (pid: 70, stack limit = 0xdf3d0248) [ 5.148269] Stack: (0xdf3d1e78 to 0xdf3d2000) [ 5.152834] 1e60: 00000000 df5f8c00 [ 5.161410] 1e80: 2c9a4447 df5f8c20 b269111c df5ccbc0 df27ba40 00000000 00000000 c009c8a5 [ 5.169984] 1ea0: df27ba40 df5ccbc0 00000000 c06108c0 df3d0000 c05de0c0 dfabdd50 c009c917 [ 5.178559] 1ec0: 00000000 00000000 df3a00c0 dfabdd50 dfabe400 00000000 dfac1600 dfabe420 [ 5.187134] 1ee0: df3d0008 c0038e4d c002dfb7 c05da900 df030b00 00000000 00000000 df3a00c0 [ 5.195709] 1f00: dfabe400 dfabe400 df3d0000 df3a00d8 dfabe420 00000000 00000008 c0039677 [ 5.204284] 1f20: df3a00c0 df3d0000 00000000 df5f4a00 00000000 df3a00c0 c0039459 00000000 [ 5.212859] 1f40: 00000000 00000000 00000000 c003c8e9 df3d1f70 00000000 df2abc8c df3a00c0 [ 5.221434] 1f60: 00000000 00000000 dead4ead ffffffff ffffffff df3d1f74 df3d1f74 00000000 [ 5.230010] 1f80: 00000000 dead4ead ffffffff ffffffff df3d1f90 df3d1f90 00000000 df5f4a00 [ 5.238585] 1fa0: c003c865 00000000 00000000 c000c3b9 00000000 00000000 00000000 00000000 [ 5.247158] 1fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 [ 5.255732] 1fe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000 [ 5.264323] [] (free_block) from [] (drain_array+0x59/0x80) [ 5.271989] [] (drain_array) from [] (cache_reap+0x4b/0xcc) [ 5.279664] [] (cache_reap) from [] (process_one_work+0x15b/0x21a) [ 5.287975] [] (process_one_work) from [] (worker_thread+0x21f/0x2f4) [ 5.296555] [] (worker_thread) from [] (kthread+0x85/0x98) [ 5.304139] [] (kthread) from [] (ret_from_fork+0x11/0x38) [ 5.311715] Code: 0b1b f8db 2000 015b (58d6) 18d1 [ 5.316741] ---[ end trace ceaadc3e59ee68a1 ]--- [ 6.184007] Unable to handle kernel paging request at virtual address ffffffe0 [ 6.191593] pgd = c0004000 [ 6.194428] [ffffffe0] *pgd=9fefd821, *pte=00000000, *ppte=00000000 [ 6.201021] Internal error: Oops: 17 [#2] SMP THUMB2 [ 6.206222] Modules linked in: [ 6.209435] CPU: 0 PID: 70 Comm: kworker/0:2 Tainted: G D 3.16.0-rc6-00141-g361f018-dirty #19 [ 6.219383] task: df2ab980 ti: df3d0000 task.ti: df3d0000 [ 6.225052] PC is at kthread_data+0x4/0xa [ 6.229266] LR is at wq_worker_sleeping+0x9/0x8c [ 6.234106] pc : [] lr : [] psr: a00f00b3 [ 6.234106] sp : df3d1c00 ip : 00000000 fp : df2abc8c [ 6.246135] r10: df2abd10 r9 : 00000000 r8 : dfabe900 [ 6.251612] r7 : df3d1c20 r6 : df3d0010 r5 : df2ab980 r4 : 00000000 [ 6.258451] r3 : 00000000 r2 : 7b000000 r1 : 00000000 r0 : df2ab980 [ 6.265293] Flags: NzCv IRQs off FIQs on Mode SVC_32 ISA Thumb Segment user [ 6.273045] Control: 50c5387d Table: 9f684019 DAC: 00000015 [ 6.279067] Process kworker/0:2 (pid: 70, stack limit = 0xdf3d0248) [ 6.285636] Stack: (0xdf3d1c00 to 0xdf3d2000) [ 6.290208] 1c00: b0000000 dfabe900 df2ab980 c035657b 00000046 00000000 0000001a 00000013 [ 6.298785] 1c20: c002dfb7 c05da900 df030b00 00000000 00000000 600f0093 df030b1c c0358d5f [ 6.307360] 1c40: 00000001 c003aac7 00000000 df2ab980 df2ab980 00000000 00000000 c05d9350 [ 6.315934] 1c60: 00000001 c002ce75 df2ab980 000f0093 00000000 df2ab980 00000001 df04b940 [ 6.324511] 1c80: 00000001 df3d0000 df3d1ca8 df2ab978 df2abc8c c002dfb7 df2abc8c c05e7cec [ 6.333086] 1ca0: c009c4f6 df2abcd4 df3d1ca8 df3d1ca8 59ee68a1 c0646ec4 df3d0000 0000000b [ 6.341661] 1cc0: c009c4fa 00000020 df3d1d13 c05e7cec c009c4f6 c000e87f df3d0248 0000000b [ 6.350238] 1ce0: 00000000 00000004 200f0193 00000000 30000000 20623162 62643866 30303220 [ 6.358812] 1d00: 31302030 28206235 36643835 38312029 00203164 df3d1e30 00000000 df5f8c20 [ 6.367387] 1d20: c0687cc0 c0353d67 c0526663 e02f8fe0 df3d1e30 00000005 df5c3e40 df3d1e30 [ 6.375962] 1d40: 00000000 df5f8c20 c0687cc0 c035388b df5c3e40 c00144e3 e02f8fe0 00000005 [ 6.384537] 1d60: df3d1e30 00003808 e02f8fe0 df3d1e30 c0007808 c0014561 c00144f7 00000050 [ 6.393111] 1d80: 00000005 c05e8b7c e02f8fe0 c00083d7 00000000 800f0093 00000000 c0358d5f [ 6.401687] 1da0: 00000001 c00441e1 00000000 800f0093 00000000 df599bbc df599bc8 00000001 [ 6.410262] 1dc0: 00000001 00000003 00000000 df59e200 0000003d c004dbe3 00000000 df599b80 [ 6.418838] 1de0: df5806c0 400f0093 00000000 00000001 df599be0 400f0093 00000000 c0358d5f [ 6.427413] 1e00: df599b80 df2ab9c8 df2ab9c8 dfabe958 00000001 00000356 c009c4f6 000f01b3 [ 6.435989] 1e20: ffffffff df3d1e64 2c9a4447 c000edb5 fffffffe df5f8c20 dfaf9000 007fffe0 [ 6.444564] 1e40: df27ba40 00000000 df5f8c20 b269111c 2c9a4447 00000000 df5f8c20 c0687cc0 [ 6.453141] 1e60: 0000001c df3d1e78 c009c8a5 c009c4f6 000f01b3 ffffffff 00000000 df5f8c00 [ 6.461718] 1e80: 2c9a4447 df5f8c20 b269111c df5ccbc0 df27ba40 00000000 00000000 c009c8a5 [ 6.470293] 1ea0: df27ba40 df5ccbc0 00000000 c06108c0 df3d0000 c05de0c0 dfabdd50 c009c917 [ 6.478867] 1ec0: 00000000 00000000 df3a00c0 dfabdd50 dfabe400 00000000 dfac1600 dfabe420 [ 6.487444] 1ee0: df3d0008 c0038e4d c002dfb7 c05da900 df030b00 00000000 00000000 df3a00c0 [ 6.496019] 1f00: dfabe400 dfabe400 df3d0000 df3a00d8 dfabe420 00000000 00000008 c0039677 [ 6.504595] 1f20: df3a00c0 df3d0000 00000000 df5f4a00 00000000 df3a00c0 c0039459 00000000 [ 6.513172] 1f40: 00000000 00000000 00000000 c003c8e9 df3d1f70 00000000 df2abc8c df3a00c0 [ 6.521746] 1f60: 00000000 00000000 dead4ead ffffffff ffffffff df3d1f74 df3d1f74 00000001 [ 6.530322] 1f80: 00010001 dead4ead ffffffff ffffffff df3d1f90 df3d1f90 00000000 df5f4a00 [ 6.538896] 1fa0: c003c865 00000000 00000000 c000c3b9 00000000 00000000 00000000 00000000 [ 6.547471] 1fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 [ 6.556043] 1fe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000 [ 6.564631] [] (kthread_data) from [] (wq_worker_sleeping+0x9/0x8c) [ 6.573034] [] (wq_worker_sleeping) from [] (__schedule+0xdb/0x448) [ 6.581430] Code: 0080 4770 f8d0 3364 (f853) 0c20 [ 6.586455] ---[ end trace ceaadc3e59ee68a2 ]--- [ 6.591293] Fixing recursive fault but reboot is needed! [ 20.567945] BUG: spinlock lockup suspected on CPU#0, kworker/0:2/70 [ 20.574520] lock: 0xdfabe900, .magic: dead4ead, .owner: kworker/0:2/70, .owner_cpu: 0 [ 20.582821] CPU: 0 PID: 70 Comm: kworker/0:2 Tainted: G D 3.16.0-rc6-00141-g361f018-dirty #19 [ 20.592792] [] (unwind_backtrace) from [] (show_stack+0xb/0xc) [ 20.600749] [] (show_stack) from [] (dump_stack+0x51/0x64) [ 20.608331] [] (dump_stack) from [] (do_raw_spin_lock+0xd1/0x114) [ 20.616546] [] (do_raw_spin_lock) from [] (__schedule+0x91/0x448) [ 20.624769] [] (__schedule) from [] (do_exit+0x9d/0x61c) [ 20.632166] [] (do_exit) from [] (die+0x19f/0x27c) [ 20.639019] [] (die) from [] (__do_kernel_fault.part.11+0x37/0x54) [ 20.647328] [] (__do_kernel_fault.part.11) from [] (do_page_fault+0x1f1/0x230) [ 20.656724] [] (do_page_fault) from [] (do_DataAbort+0x27/0x64) [ 20.664755] [] (do_DataAbort) from [] (__dabt_svc+0x35/0x60) [ 20.672507] Exception stack(0xdf3d1bb8 to 0xdf3d1c00) [ 20.677801] 1ba0: df2ab980 00000000 [ 20.686375] 1bc0: 7b000000 00000000 00000000 df2ab980 df3d0010 df3d1c20 dfabe900 00000000 [ 20.694949] 1be0: df2abd10 df2abc8c 00000000 df3d1c00 c00397ad c003cc6a a00f00b3 ffffffff [ 20.703527] [] (__dabt_svc) from [] (kthread_data+0x4/0xa) [ 20.711103] [] (kthread_data) from [] (wq_worker_sleeping+0x9/0x8c) [ 20.719499] [] (wq_worker_sleeping) from [] (__schedule+0xdb/0x448) [ 20.727895] [] (__schedule) from [] (do_exit+0x603/0x61c) [ 20.735382] [] (do_exit) from [] (die+0x19f/0x27c) [ 20.742234] [] (die) from [] (__do_kernel_fault.part.11+0x37/0x54) [ 20.750539] [] (__do_kernel_fault.part.11) from [] (do_bad_area+0x43/0x4c) [ 20.759570] [] (do_bad_area) from [] (do_translation_fault+0x6b/0x76) [ 20.768145] [] (do_translation_fault) from [] (do_DataAbort+0x27/0x64) [ 20.776813] [] (do_DataAbort) from [] (__dabt_svc+0x35/0x60) [ 20.784564] Exception stack(0xdf3d1e30 to 0xdf3d1e78) [ 20.789859] 1e20: fffffffe df5f8c20 dfaf9000 007fffe0 [ 20.798434] 1e40: df27ba40 00000000 df5f8c20 b269111c 2c9a4447 00000000 df5f8c20 c0687cc0 [ 20.807008] 1e60: 0000001c df3d1e78 c009c8a5 c009c4f6 000f01b3 ffffffff [ 20.813953] [] (__dabt_svc) from [] (free_block+0x32/0xd8) [ 20.821532] [] (free_block) from [] (drain_array+0x59/0x80) [ 20.829200] [] (drain_array) from [] (cache_reap+0x4b/0xcc) [ 20.836868] [] (cache_reap) from [] (process_one_work+0x15b/0x21a) [ 20.845173] [] (process_one_work) from [] (worker_thread+0x21f/0x2f4) [ 20.853751] [] (worker_thread) from [] (kthread+0x85/0x98) [ 20.861328] [] (kthread) from [] (ret_from_fork+0x11/0x38)