# # Refer Developer's User Guide document for usage details # ##### CAUTION: Don't change any variable name in this file. ##### # #mmWave Device Variant #AWR1443, AWR1642, AWR1843, AWR6843, AWR1243, AWR2243 #IWR1443, IWR1642, IWR1843, IWR6843 #For AWR1243 and AWR2243 device This tool uses SPI interface and uses JSON # file for configuration input #For other devices it uses UART COM port and can use CFG or JSON input file. # #@Note: For AWR1243/AWR2243 # a. If FW_DOWNLOAD_ENABLE=1 & FLASH_CONNECTED_TO_SENSOR=1 # then: Flash matching MetaImage binary file to device first. # b. Set LVDS Lanes (DCA_LVDS_LANE_MODE=4) # MMWAVE_DEVICE_VARIANT=IWR6843 # #COM port number (@921600 baud rate) #Same COM port is being used for sending CLI commands #And after sensorStart same COM port is used to read monitoring data. # COM_PORT_NUM=10 # #Global configuration: these define the task to be done # #To configure the mmWave RF Front End: [ENABLE_CONFIG_MMWAVE] 1- Yes, 0-No #To capture Monitoring report to JSON file: [ENABLE_MONITOR_CAPTURE] 1- Yes, 0-No #To capture Raw ADC data using DCA1000: [ENABLE_DCA_CAPTURE] 1- Yes, 0-No #To post process the captured ADC data: [ENABLE_POSTPROC] 1- Yes, 0-No # (assuming postproc.exe is available at same path of this tool) #mmWave Config file can be *.cfg or JSON format: [CONFIG_FILE_FORMAT] 1-cfg, 0-json # ENABLE_CONFIG_MMWAVE=1 ENABLE_MONITOR_CAPTURE=0 ENABLE_DCA_CAPTURE=1 ENABLE_POSTPROC=0 #CONFIG_FILE_FORMAT=0 CONFIG_FILE_FORMAT=1 # #Path for mmWave Config JSON or .cfg file (including file name). #JSON file must be generated by SensingEstimator or mmWave Studio # Set CONFIG_FILE_FORMAT accordingly. # CONFIG_JSON_CFG_PATH=..\..\src\profiles\profile_monitor_xwr68xx_cont.cfg #CONFIG_JSON_CFG_PATH=..\..\src\profiles\profile_monitor_xwr68xx.cfg #CONFIG_JSON_CFG_PATH=..\..\src\profiles\profile_monitor_xwr18xx.cfg #CONFIG_JSON_CFG_PATH=..\..\src\profiles\22xx_monitor.mmwave.json # #Path to store the monitoring report in JSON format #Each report in seperate JSON file #Note: make sure this path and directory exist # MONITORING_JSON_PATH=..\monitor_report_dir # #Number of monitoring report to store in JSON file #Set to zero for infinite time till terminated (CLI CMD: "quit") #or CLI CMD : "monCaptureStop" # NUMBER_OF_MONITOR_REPORT_STORE=10000 # #Path to store Captured ADC data binary file # CAPTURED_ADC_DATA_PATH=..\captured_adc_IWR6843 #CAPTURED_ADC_DATA_PATH=..\captured_adc_AWR1843 # #DCA1000 Configurations #It captures the num. of frames worth data which is given in JSON or CFG file #DCA_FILE_PREFIX: File prefix for each ADC data DCA1000 captures. # e.g. with ‘adc_data’ prefix, file name would be adc_data_Raw_0.bin #DCA_MAX_REC_FILE_SIZE_MB:Max size of each ADC data file DCA1000 captures, at # this size limit it splits captured data into next binary file. #DCA_DATA_FORMAT_MODE: 1: 12Bit, 2: 14Bit, 3: 16Bit mode #@Note make sure this format matches with data-format in CFG or JSON config parameters. #DCA_LVDS_LANE_MODE : 2 or 4 LVDS lanes (AR1243/2243 - 4 lane, AR1642/1843/6843 - 2 lane) # DCA_FILE_PREFIX=adc_data DCA_MAX_REC_FILE_SIZE_MB=1000 #DCA_MAX_REC_FILE_SIZE_MB=100 DCA_DATA_FORMAT_MODE=3 DCA_LVDS_LANE_MODE=2 # #PostProc exe utility path #This tool is provided along with CLI tool, so you may not touch this input text # POST_PROC_EXE_PATH=..\mmw_post_proc\mmwave_postproc.exe # #Set this parameter when you need to run this CLI tool with CCS image running # i.e. Not running from Flashed App-Image but loading application from CCS. # In that case application sometime responses slowely for CLI CMD so in the # tool we will add delay for each CLI CMD so it doesn't get expire with error. # 0: Running from Flash, 1: running from CCS # CCS_DEBUG=0 # #Below Configuration is mainly used for AWR1243/AWR2243 device #When Communication happens over SPI interface using mmwavelink library # # #If Firmware Download is disabled with AWR1243/AWR2243 device #0: Yes, 1: No firmware download #For this tool, it is recommended to flash the firmware and set this option to '1' # As this tool doesn't contains all version of FW for AWR1243/AWR2243. # FW_DOWNLOAD_DISABLE=1 # #If sFlash is connected with AWR1243/AWR2243 device #1: Yes, 0: nosFlash is connected with sensor # # FLASH_CONNECTED_TO_SENSOR=1 # #power on master arguments, please modify if needed (for AWR1243/AWR2243) #rlClientCbs_t: CRC_TYPE 0:16Bit/1:32Bit/2:64Bit, #ACK_TIMEOUT : ACK Timeout for mmWaveLink # CRC_TYPE=1; ACK_TIMEOUT=5000; #END # #End of Config File #