# # Refer Developer's User Guide document for usage details # ########## CAUTION: Don't change any variable name in this file. ########## # ------------------------------------------------------------------------- # mmWave Device Variant # AWR1443, AWR1642, AWR1843, AWR6843, AWR1243, AWR2243 # IWR1443, IWR1642, IWR1843, IWR6843 # For AWR1243 and AWR2243 device This tool uses SPI interface and uses JSON file for configuration input # For other devices it uses UART COM port and can use CFG or JSON input file. # # @Note: For AWR1243/AWR2243 # a. If FW_DOWNLOAD_ENABLE=1 & FLASH_CONNECTED_TO_SENSOR=1 # then: Flash matching MetaImage binary file to device first. # b. Set LVDS Lanes (DCA_LVDS_LANE_MODE=4) # ------------------------------------------------------------------------- MMWAVE_DEVICE_VARIANT=AWR1642 # ------------------------------------------------------------------------- # COM port number (@921600 baud rate) # Same COM port is being used for sending CLI commands # And after sensorStart same COM port is used to read monitoring data. # ------------------------------------------------------------------------- COM_PORT_NUM=13 # ------------------------------------------------------------------------- # Global configuration: these define the task to be done # # To configure the mmWave RF Front End : [ENABLE_CONFIG_MMWAVE] 1-Yes, 0-No # To capture Monitoring report to JSON file : [ENABLE_MONITOR_CAPTURE] 1-Yes, 0-No # To capture Raw ADC data using DCA1000 : [ENABLE_DCA_CAPTURE] 1-Yes, 0-No # To post process the captured ADC data : [ENABLE_POSTPROC] 1-Yes, 0-No, assuming postproc.exe is at same path of this tool # mmWave Config file can be *.cfg or JSON format : [CONFIG_FILE_FORMAT] 1-cfg, 0-json # ------------------------------------------------------------------------- ENABLE_CONFIG_MMWAVE=1 ENABLE_MONITOR_CAPTURE=0 ENABLE_DCA_CAPTURE=1 ENABLE_POSTPROC=0 CONFIG_FILE_FORMAT=1 # ------------------------------------------------------------------------- # Path for mmWave Config JSON or .cfg file (including file name). # JSON file must be generated by SensingEstimator or mmWave Studio # Set CONFIG_FILE_FORMAT accordingly. # ------------------------------------------------------------------------- CONFIG_JSON_CFG_PATH=..\cfg_xWR1642\profile_monitor_xwr16xx.cfg #CONFIG_JSON_CFG_PATH=..\cfg_xWR1642\profile_2_4.cfg # ------------------------------------------------------------------------- # Path to store the monitoring report in JSON format # Each report in seperate JSON file # Note: make sure this path and directory exist # ------------------------------------------------------------------------- MONITORING_JSON_PATH=..\monitor_report_dir # ------------------------------------------------------------------------- # Number of monitoring report to store in JSON file # Set to zero for infinite time till terminated (CLI CMD: "quit") or CLI CMD : "monCaptureStop" # ------------------------------------------------------------------------- NUMBER_OF_MONITOR_REPORT_STORE=10000 # ------------------------------------------------------------------------- # Path to store Captured ADC data binary file # ------------------------------------------------------------------------- CAPTURED_ADC_DATA_PATH=..\captured_adc_xWR1642 # ------------------------------------------------------------------------- # DCA1000 Configurations # It captures the number of frames worth data which is given in JSON or CFG file # # DCA_FILE_PREFIX: File prefix for each ADC data DCA1000 captures. # e.g. with ‘adc_data’ prefix, file name would be adc_data_Raw_0.bin # # DCA_MAX_REC_FILE_SIZE_MB: Max size of each ADC data file DCA1000 captures, at this size limit it splits captured data into next binary file. # # DCA_DATA_FORMAT_MODE: 1: 12Bit, 2: 14Bit, 3: 16Bit mode # # @Note make sure this format matches with data-format in CFG or JSON config parameters. # DCA_LVDS_LANE_MODE: 2 or 4 LVDS lanes (AR1243/2243 - 4 lane, AR1642/1843/6843 - 2 lane) # ------------------------------------------------------------------------- DCA_FILE_PREFIX=adc_data DCA_MAX_REC_FILE_SIZE_MB=100 DCA_DATA_FORMAT_MODE=3 DCA_LVDS_LANE_MODE=2 # ------------------------------------------------------------------------- # PostProc exe utility path # This tool is provided along with CLI tool, so you may not touch this input text # ------------------------------------------------------------------------- POST_PROC_EXE_PATH=..\mmw_post_proc\mmwave_postproc.exe # ------------------------------------------------------------------------- # Set this parameter when you need to run this CLI tool with CCS image running # i.e. Not running from Flashed App-Image but loading application from CCS. # In that case application sometime responses slowely for CLI CMD so in the # tool we will add delay for each CLI CMD so it doesn't get expire with error. # 0: Running from Flash, 1: running from CCS # ------------------------------------------------------------------------- CCS_DEBUG=0 # ------------------------------------------------------------------------- # Below Configuration is mainly used for AWR1243/AWR2243 device # When Communication happens over SPI interface using mmwavelink library # ------------------------------------------------------------------------- # ------------------------------------------------------------------------- # If Firmware Download is disabled with AWR1243/AWR2243 device # 0: Yes, 1: No firmware download # For this tool, it is recommended to flash the firmware and set this option to '1' # As this tool doesn't contains all version of FW for AWR1243/AWR2243. # ------------------------------------------------------------------------- FW_DOWNLOAD_DISABLE=1 # ------------------------------------------------------------------------- # If sFlash is connected with AWR1243/AWR2243 device # 1: Yes, 0: nosFlash is connected with sensor # ------------------------------------------------------------------------- FLASH_CONNECTED_TO_SENSOR=1 # ------------------------------------------------------------------------- # power on master arguments, please modify if needed (for AWR1243/AWR2243) # rlClientCbs_t: CRC_TYPE 0: 16Bit, 1: 32Bit, 2: 64Bit # ACK_TIMEOUT : ACK Timeout for mmWaveLink # ------------------------------------------------------------------------- CRC_TYPE=1; ACK_TIMEOUT=5000; # # End of Config File #