[00:28:10.390] 954-:DEVICE_STS [0x04]=0xDF [00:28:10.390] 954-:PAR_ERR_THOLD_HI [0x05]=0x01 [00:28:10.390] 954-:RX_PORT_STS1 [0x4D]=0x43 [00:28:10.391] 954-:RX_PORT_STS2 [0x4E]=0x14 [00:28:10.392] 954-:LINK_ERROR_COUNT [0xB9]=0x33 [00:28:10.392] 954-:CSI_STS [0x35]=0x01 [00:28:10.393] 954-:CSI_TX_ISR [0x37]=0x03 [00:28:10.394] 953-:DEVICE_ID [0x00]=0x32:0x32 [00:28:10.395] 953-:GENERAL_STATUS [0x52]=0x45:0x45