Pixium specific setup ------------------------- BCC error status 0x00 SER General status 0x52 (Should be 0x45) 0x45 ------------------------- bist error count before bist on SER 0x00 ------------------------- read bist enable should be 0x0 or 0x8 0x00 read bist enable should be 0x1 0x01 ------------------------- Read bist lock status (0x4D RX_PORT_STS1) 0x33 forcing errors Post bist Lock status (0x4D RX_PORT_STS1) should read 0x03 if OK. 0x13 if lock status change during bist 0x03 RX_PORT_STS2 0xfd ------------------------- general SER status 0x52 (should be 0x4d) 0x4d general DES status 0x04 (should be 0xCF) 0xdf ------------------------- BIST CRC Error Count on SER 0x54 0x06 Parity Error count MSB on DES 0x56 0x00 Parity Error count LSB on DES 0x55 0x00 ------------------------- SER Device ID (should be 0x30) 0x30