Wed Jan 15 17:28:23 2020: * -----/|-------------------------------------------------------------------- * Wed Jan 15 17:28:23 2020: * / |__ * Wed Jan 15 17:28:23 2020: * /_ / MSP Flasher v1.3.20 * Wed Jan 15 17:28:23 2020: * | / * Wed Jan 15 17:28:23 2020: * -----|/-------------------------------------------------------------------- * Wed Jan 15 17:28:23 2020: * Wed Jan 15 17:28:23 2020: * Evaluating triggers...done Wed Jan 15 17:28:23 2020: No arguments. Aborting. Wed Jan 15 17:28:23 2020: ******************************************************************************* Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: Usage: MSP430Flasher [OPTIONS] Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -h / -? Displays usage information (displays this table Wed Jan 15 17:28:23 2020: of command line switches) Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -x Displays available exit specifications Wed Jan 15 17:28:23 2020: (see tigger -z) Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -i (TI)USB | DETECT | Communication port for the FET debugger. TIUSB Wed Jan 15 17:28:23 2020: COMn (Win) | (or USB) is the default. Use COMn (for example, Wed Jan 15 17:28:23 2020: ttyACMn (Linux) | COM15) on Windows or ttyACMn(for example, Wed Jan 15 17:28:23 2020: usbmodem* (OSX) | ttyACM15) on Linux or usbmodemn (for example, Wed Jan 15 17:28:23 2020: HIDn:COMn usbmodem1421) on OS X to choose a debugger Wed Jan 15 17:28:23 2020: connected to COM port n. Use HIDn:COMn for Wed Jan 15 17:28:23 2020: specific eZ430 tools on Windows. Use -i DETECT to Wed Jan 15 17:28:23 2020: execute a FET detection sweep, to display Wed Jan 15 17:28:23 2020: detailed information about all connected debug Wed Jan 15 17:28:23 2020: tools, and to prompt to select a FET. Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -j fast | medium | slow Configures the MSP Debug Stack to increase or Wed Jan 15 17:28:23 2020: decrease the JTAG or SBW frequency of the FET. Wed Jan 15 17:28:23 2020: Default = medium Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -n DEVICE_NAME | NO_TARGET (optional for MSP430, required for MSP432) Wed Jan 15 17:28:23 2020: The name of the device being accessed (prompt Wed Jan 15 17:28:23 2020: if mismatch between found and selected device). Wed Jan 15 17:28:23 2020: -n NO_TARGET executes MSP Flasher without Wed Jan 15 17:28:23 2020: attempting to connect to a target device Wed Jan 15 17:28:23 2020: Choose this option to detect if a certain FET Wed Jan 15 17:28:23 2020: is connected or when the FET firmware should be Wed Jan 15 17:28:23 2020: updated only. Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -r [filenname,mem_sect] Triggers a read operation in target device Wed Jan 15 17:28:23 2020: memory section specified by mem_section. The Wed Jan 15 17:28:23 2020: memory content is written to a file specified Wed Jan 15 17:28:23 2020: by Filename. Available memory sections are: Wed Jan 15 17:28:23 2020: - MAIN = the main memory of the device Wed Jan 15 17:28:23 2020: - INFO = info memory (see trigger –u) Wed Jan 15 17:28:23 2020: - BSL = bootloader memory (see trigger –b) Wed Jan 15 17:28:23 2020: - RAM = random access memory Wed Jan 15 17:28:23 2020: - 0x****-0x**** = custom memory section Wed Jan 15 17:28:23 2020: Specify .txt as the extension for Filename to Wed Jan 15 17:28:23 2020: write data in TI-TXT format, or specify .a43 Wed Jan 15 17:28:23 2020: (or .hex) to write data in Intel-Hex format. Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -w filenname Triggers a memory write operation. The accepted Wed Jan 15 17:28:23 2020: formats are txt (TI-txt) or a43/hex (Intel-hex). Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -v filename (optional) Triggers verification of the target memory against Wed Jan 15 17:28:23 2020: a target code file. If -w is used, no argument is Wed Jan 15 17:28:23 2020: required. For a stand-alone verify, provide the Wed Jan 15 17:28:23 2020: path to a target code file as an argument. Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -u Unlocks protected InfoA memory for writing Wed Jan 15 17:28:23 2020: (use only with -w switch) Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -b Unlocks protected BSL memory for writing Wed Jan 15 17:28:23 2020: (use only with -w switch) Wed Jan 15 17:28:23 2020: -e ERASE_ALL | Erase memory. Default: ERASE_ALL (INFO & MAIN) Wed Jan 15 17:28:23 2020: ERASE_MAIN | ERASE_MAIN: erase MAIN memory only Wed Jan 15 17:28:23 2020: ERASE_SEGMENT | ERASE_SEGMENT: erase segment to be programmed only Wed Jan 15 17:28:23 2020: ERASE_TOTAL | ERASE_TOTAL: applicable for FR5xx/FR6xx only! Wed Jan 15 17:28:23 2020: ERASE_USER_CODE | ERASE_USER_CODE: applicable for FR4xx only! Wed Jan 15 17:28:23 2020: NO_ERASE NO_ERASE: use only with -w switch Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -p JTAG PASSWORD Specifies the JTAG password that should be used Wed Jan 15 17:28:23 2020: to open a password protected target device Wed Jan 15 17:28:23 2020: (supported on FRAM devices only). The user is Wed Jan 15 17:28:23 2020: prompted if the password is incompatible with Wed Jan 15 17:28:23 2020: the password length deteced by MSP Flasher. Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -o L | C Operating mode for L092 and RF430FR152H family Wed Jan 15 17:28:23 2020: devices. L = L092 mode (normal mode) Wed Jan 15 17:28:23 2020: C = C092 mode (ROM development mode) Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -f Permanently secures JTAG access to the target MSP. Wed Jan 15 17:28:23 2020: Caution: The device will no longer be accessible Wed Jan 15 17:28:23 2020: through JTAG or Spy-Bi-Wire. This action Wed Jan 15 17:28:23 2020: is irreversible. Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -g Disables the logging mechanism. Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -a Causes a nonintrusive target connection: use Wed Jan 15 17:28:23 2020: this switch if no reset should be applied to Wed Jan 15 17:28:23 2020: the target device on start up. Correct target Wed Jan 15 17:28:23 2020: device name must be specified using the -n switch. Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -s Suppresses the FET firmware update prompt. Wed Jan 15 17:28:23 2020: In case of a mismatch between MSP Debug Stack Wed Jan 15 17:28:23 2020: and FET firmware, an update is forced. Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -q QUIET mode: No system messages will be displayed Wed Jan 15 17:28:23 2020: (except for errors and user prompts) Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: -z [exit_spec,...] Specifies the state of the device after Wed Jan 15 17:28:23 2020: programming. View available 'exit_spec's using Wed Jan 15 17:28:23 2020: -x switch). Use ", " as a delimiter. Wed Jan 15 17:28:23 2020: Wed Jan 15 17:28:23 2020: For a GUI-based alternative, check out UniFlash: http://ti.com/tool/uniflash Wed Jan 15 17:28:23 2020: ******************************************************************************* Wed Jan 15 17:28:23 2020: Press ENTER to continue. Wed Jan 15 17:28:37 2020: * -----/|-------------------------------------------------------------------- * Wed Jan 15 17:28:37 2020: * / |__ * Wed Jan 15 17:28:37 2020: * /_ / MSP Flasher v1.3.20 * Wed Jan 15 17:28:37 2020: * | / * Wed Jan 15 17:28:37 2020: * -----|/-------------------------------------------------------------------- * Wed Jan 15 17:28:37 2020: * Wed Jan 15 17:28:37 2020: * Evaluating triggers...done Wed Jan 15 17:28:37 2020: * Checking for available FET debuggers: Wed Jan 15 17:28:37 2020: * Found USB FET @ COM21 <- Selected Wed Jan 15 17:28:37 2020: * Initializing interface @ COM21...done Wed Jan 15 17:28:37 2020: * Checking firmware compatibility: Wed Jan 15 17:28:37 2020: * FET firmware is up to date. Wed Jan 15 17:28:37 2020: * Reading FW version...done Wed Jan 15 17:28:37 2020: * Setting VCC to 3000 mV...done Wed Jan 15 17:28:43 2020: * Accessing device...done Wed Jan 15 17:28:43 2020: * Reading device information...done Wed Jan 15 17:28:47 2020: * Wed Jan 15 17:28:47 2020: * ---------------------------------------------------------------------------- Wed Jan 15 17:28:47 2020: * Arguments : DETECT Wed Jan 15 17:28:47 2020: * ---------------------------------------------------------------------------- Wed Jan 15 17:28:47 2020: * Driver : loaded Wed Jan 15 17:28:47 2020: * Dll Version : 31400000 Wed Jan 15 17:28:47 2020: * FwVersion : 31200000 Wed Jan 15 17:28:47 2020: * Interface : TIUSB Wed Jan 15 17:28:47 2020: * HwVersion : U 3.0 Wed Jan 15 17:28:47 2020: * JTAG Mode : AUTO Wed Jan 15 17:28:47 2020: * Device : MSP430F5659 Wed Jan 15 17:28:47 2020: * EEM : Level 7, ClockCntrl 2 Wed Jan 15 17:28:47 2020: * VCC OFF Wed Jan 15 17:28:47 2020: * ---------------------------------------------------------------------------- Wed Jan 15 17:28:47 2020: * Powering down...done Wed Jan 15 17:28:48 2020: * Disconnecting from device...done Wed Jan 15 17:28:48 2020: * Wed Jan 15 17:28:48 2020: * ---------------------------------------------------------------------------- Wed Jan 15 17:28:48 2020: * Driver : closed (No error) Wed Jan 15 17:28:48 2020: * ---------------------------------------------------------------------------- Wed Jan 15 17:28:48 2020: */ Wed Jan 15 17:31:01 2020: * -----/|-------------------------------------------------------------------- * Wed Jan 15 17:31:01 2020: * / |__ * Wed Jan 15 17:31:01 2020: * /_ / MSP Flasher v1.3.20 * Wed Jan 15 17:31:01 2020: * | / * Wed Jan 15 17:31:01 2020: * -----|/-------------------------------------------------------------------- * Wed Jan 15 17:31:01 2020: * Wed Jan 15 17:31:01 2020: * Evaluating triggers...done Wed Jan 15 17:31:01 2020: * Checking for available FET debuggers: Wed Jan 15 17:31:01 2020: * Found USB FET @ COM21 <- Selected Wed Jan 15 17:31:01 2020: * Initializing interface @ COM21...done Wed Jan 15 17:31:02 2020: * Checking firmware compatibility: Wed Jan 15 17:31:02 2020: * FET firmware is up to date. Wed Jan 15 17:31:02 2020: * Reading FW version...done Wed Jan 15 17:31:02 2020: * Setting VCC to 3000 mV...done Wed Jan 15 17:31:02 2020: * Accessing device...done Wed Jan 15 17:31:02 2020: * Reading device information...done Wed Jan 15 17:31:02 2020: * Loading file into device... Wed Jan 15 17:31:09 2020: # Exit: 59 Wed Jan 15 17:31:09 2020: # ERROR: Could not write device memory Wed Jan 15 17:31:09 2020: * Powering down...done Wed Jan 15 17:31:09 2020: * Disconnecting from device...done Wed Jan 15 17:31:09 2020: * Wed Jan 15 17:31:09 2020: * ---------------------------------------------------------------------------- Wed Jan 15 17:31:09 2020: * Driver : closed (No error) Wed Jan 15 17:31:09 2020: * ---------------------------------------------------------------------------- Wed Jan 15 17:31:09 2020: */ Wed Jan 22 16:18:58 2020: * -----/|-------------------------------------------------------------------- * Wed Jan 22 16:18:58 2020: * / |__ * Wed Jan 22 16:18:58 2020: * /_ / MSP Flasher v1.3.20 * Wed Jan 22 16:18:58 2020: * | / * Wed Jan 22 16:18:58 2020: * -----|/-------------------------------------------------------------------- * Wed Jan 22 16:18:58 2020: * Wed Jan 22 16:18:58 2020: * Evaluating triggers...done Wed Jan 22 16:18:58 2020: No arguments. Aborting. Wed Jan 22 16:18:58 2020: ******************************************************************************* Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: Usage: MSP430Flasher [OPTIONS] Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -h / -? Displays usage information (displays this table Wed Jan 22 16:18:58 2020: of command line switches) Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -x Displays available exit specifications Wed Jan 22 16:18:58 2020: (see tigger -z) Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -i (TI)USB | DETECT | Communication port for the FET debugger. TIUSB Wed Jan 22 16:18:58 2020: COMn (Win) | (or USB) is the default. Use COMn (for example, Wed Jan 22 16:18:58 2020: ttyACMn (Linux) | COM15) on Windows or ttyACMn(for example, Wed Jan 22 16:18:58 2020: usbmodem* (OSX) | ttyACM15) on Linux or usbmodemn (for example, Wed Jan 22 16:18:58 2020: HIDn:COMn usbmodem1421) on OS X to choose a debugger Wed Jan 22 16:18:58 2020: connected to COM port n. Use HIDn:COMn for Wed Jan 22 16:18:58 2020: specific eZ430 tools on Windows. Use -i DETECT to Wed Jan 22 16:18:58 2020: execute a FET detection sweep, to display Wed Jan 22 16:18:58 2020: detailed information about all connected debug Wed Jan 22 16:18:58 2020: tools, and to prompt to select a FET. Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -j fast | medium | slow Configures the MSP Debug Stack to increase or Wed Jan 22 16:18:58 2020: decrease the JTAG or SBW frequency of the FET. Wed Jan 22 16:18:58 2020: Default = medium Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -n DEVICE_NAME | NO_TARGET (optional for MSP430, required for MSP432) Wed Jan 22 16:18:58 2020: The name of the device being accessed (prompt Wed Jan 22 16:18:58 2020: if mismatch between found and selected device). Wed Jan 22 16:18:58 2020: -n NO_TARGET executes MSP Flasher without Wed Jan 22 16:18:58 2020: attempting to connect to a target device Wed Jan 22 16:18:58 2020: Choose this option to detect if a certain FET Wed Jan 22 16:18:58 2020: is connected or when the FET firmware should be Wed Jan 22 16:18:58 2020: updated only. Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -r [filenname,mem_sect] Triggers a read operation in target device Wed Jan 22 16:18:58 2020: memory section specified by mem_section. The Wed Jan 22 16:18:58 2020: memory content is written to a file specified Wed Jan 22 16:18:58 2020: by Filename. Available memory sections are: Wed Jan 22 16:18:58 2020: - MAIN = the main memory of the device Wed Jan 22 16:18:58 2020: - INFO = info memory (see trigger –u) Wed Jan 22 16:18:58 2020: - BSL = bootloader memory (see trigger –b) Wed Jan 22 16:18:58 2020: - RAM = random access memory Wed Jan 22 16:18:58 2020: - 0x****-0x**** = custom memory section Wed Jan 22 16:18:58 2020: Specify .txt as the extension for Filename to Wed Jan 22 16:18:58 2020: write data in TI-TXT format, or specify .a43 Wed Jan 22 16:18:58 2020: (or .hex) to write data in Intel-Hex format. Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -w filenname Triggers a memory write operation. The accepted Wed Jan 22 16:18:58 2020: formats are txt (TI-txt) or a43/hex (Intel-hex). Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -v filename (optional) Triggers verification of the target memory against Wed Jan 22 16:18:58 2020: a target code file. If -w is used, no argument is Wed Jan 22 16:18:58 2020: required. For a stand-alone verify, provide the Wed Jan 22 16:18:58 2020: path to a target code file as an argument. Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -u Unlocks protected InfoA memory for writing Wed Jan 22 16:18:58 2020: (use only with -w switch) Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -b Unlocks protected BSL memory for writing Wed Jan 22 16:18:58 2020: (use only with -w switch) Wed Jan 22 16:18:58 2020: -e ERASE_ALL | Erase memory. Default: ERASE_ALL (INFO & MAIN) Wed Jan 22 16:18:58 2020: ERASE_MAIN | ERASE_MAIN: erase MAIN memory only Wed Jan 22 16:18:58 2020: ERASE_SEGMENT | ERASE_SEGMENT: erase segment to be programmed only Wed Jan 22 16:18:58 2020: ERASE_TOTAL | ERASE_TOTAL: applicable for FR5xx/FR6xx only! Wed Jan 22 16:18:58 2020: ERASE_USER_CODE | ERASE_USER_CODE: applicable for FR4xx only! Wed Jan 22 16:18:58 2020: NO_ERASE NO_ERASE: use only with -w switch Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -p JTAG PASSWORD Specifies the JTAG password that should be used Wed Jan 22 16:18:58 2020: to open a password protected target device Wed Jan 22 16:18:58 2020: (supported on FRAM devices only). The user is Wed Jan 22 16:18:58 2020: prompted if the password is incompatible with Wed Jan 22 16:18:58 2020: the password length deteced by MSP Flasher. Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -o L | C Operating mode for L092 and RF430FR152H family Wed Jan 22 16:18:58 2020: devices. L = L092 mode (normal mode) Wed Jan 22 16:18:58 2020: C = C092 mode (ROM development mode) Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -f Permanently secures JTAG access to the target MSP. Wed Jan 22 16:18:58 2020: Caution: The device will no longer be accessible Wed Jan 22 16:18:58 2020: through JTAG or Spy-Bi-Wire. This action Wed Jan 22 16:18:58 2020: is irreversible. Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -g Disables the logging mechanism. Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -a Causes a nonintrusive target connection: use Wed Jan 22 16:18:58 2020: this switch if no reset should be applied to Wed Jan 22 16:18:58 2020: the target device on start up. Correct target Wed Jan 22 16:18:58 2020: device name must be specified using the -n switch. Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -s Suppresses the FET firmware update prompt. Wed Jan 22 16:18:58 2020: In case of a mismatch between MSP Debug Stack Wed Jan 22 16:18:58 2020: and FET firmware, an update is forced. Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -q QUIET mode: No system messages will be displayed Wed Jan 22 16:18:58 2020: (except for errors and user prompts) Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: -z [exit_spec,...] Specifies the state of the device after Wed Jan 22 16:18:58 2020: programming. View available 'exit_spec's using Wed Jan 22 16:18:58 2020: -x switch). Use ", " as a delimiter. Wed Jan 22 16:18:58 2020: Wed Jan 22 16:18:58 2020: For a GUI-based alternative, check out UniFlash: http://ti.com/tool/uniflash Wed Jan 22 16:18:58 2020: ******************************************************************************* Wed Jan 22 16:18:58 2020: Press ENTER to continue. Wed Jan 22 16:38:31 2020: * -----/|-------------------------------------------------------------------- * Wed Jan 22 16:38:31 2020: * / |__ * Wed Jan 22 16:38:31 2020: * /_ / MSP Flasher v1.3.20 * Wed Jan 22 16:38:31 2020: * | / * Wed Jan 22 16:38:31 2020: * -----|/-------------------------------------------------------------------- * Wed Jan 22 16:38:31 2020: * Wed Jan 22 16:38:31 2020: * Evaluating triggers...done Wed Jan 22 16:38:31 2020: No arguments. Aborting. Wed Jan 22 16:38:31 2020: ******************************************************************************* Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: Usage: MSP430Flasher [OPTIONS] Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -h / -? Displays usage information (displays this table Wed Jan 22 16:38:31 2020: of command line switches) Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -x Displays available exit specifications Wed Jan 22 16:38:31 2020: (see tigger -z) Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -i (TI)USB | DETECT | Communication port for the FET debugger. TIUSB Wed Jan 22 16:38:31 2020: COMn (Win) | (or USB) is the default. Use COMn (for example, Wed Jan 22 16:38:31 2020: ttyACMn (Linux) | COM15) on Windows or ttyACMn(for example, Wed Jan 22 16:38:31 2020: usbmodem* (OSX) | ttyACM15) on Linux or usbmodemn (for example, Wed Jan 22 16:38:31 2020: HIDn:COMn usbmodem1421) on OS X to choose a debugger Wed Jan 22 16:38:31 2020: connected to COM port n. Use HIDn:COMn for Wed Jan 22 16:38:31 2020: specific eZ430 tools on Windows. Use -i DETECT to Wed Jan 22 16:38:31 2020: execute a FET detection sweep, to display Wed Jan 22 16:38:31 2020: detailed information about all connected debug Wed Jan 22 16:38:31 2020: tools, and to prompt to select a FET. Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -j fast | medium | slow Configures the MSP Debug Stack to increase or Wed Jan 22 16:38:31 2020: decrease the JTAG or SBW frequency of the FET. Wed Jan 22 16:38:31 2020: Default = medium Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -n DEVICE_NAME | NO_TARGET (optional for MSP430, required for MSP432) Wed Jan 22 16:38:31 2020: The name of the device being accessed (prompt Wed Jan 22 16:38:31 2020: if mismatch between found and selected device). Wed Jan 22 16:38:31 2020: -n NO_TARGET executes MSP Flasher without Wed Jan 22 16:38:31 2020: attempting to connect to a target device Wed Jan 22 16:38:31 2020: Choose this option to detect if a certain FET Wed Jan 22 16:38:31 2020: is connected or when the FET firmware should be Wed Jan 22 16:38:31 2020: updated only. Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -r [filenname,mem_sect] Triggers a read operation in target device Wed Jan 22 16:38:31 2020: memory section specified by mem_section. The Wed Jan 22 16:38:31 2020: memory content is written to a file specified Wed Jan 22 16:38:31 2020: by Filename. Available memory sections are: Wed Jan 22 16:38:31 2020: - MAIN = the main memory of the device Wed Jan 22 16:38:31 2020: - INFO = info memory (see trigger –u) Wed Jan 22 16:38:31 2020: - BSL = bootloader memory (see trigger –b) Wed Jan 22 16:38:31 2020: - RAM = random access memory Wed Jan 22 16:38:31 2020: - 0x****-0x**** = custom memory section Wed Jan 22 16:38:31 2020: Specify .txt as the extension for Filename to Wed Jan 22 16:38:31 2020: write data in TI-TXT format, or specify .a43 Wed Jan 22 16:38:31 2020: (or .hex) to write data in Intel-Hex format. Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -w filenname Triggers a memory write operation. The accepted Wed Jan 22 16:38:31 2020: formats are txt (TI-txt) or a43/hex (Intel-hex). Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -v filename (optional) Triggers verification of the target memory against Wed Jan 22 16:38:31 2020: a target code file. If -w is used, no argument is Wed Jan 22 16:38:31 2020: required. For a stand-alone verify, provide the Wed Jan 22 16:38:31 2020: path to a target code file as an argument. Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -u Unlocks protected InfoA memory for writing Wed Jan 22 16:38:31 2020: (use only with -w switch) Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -b Unlocks protected BSL memory for writing Wed Jan 22 16:38:31 2020: (use only with -w switch) Wed Jan 22 16:38:31 2020: -e ERASE_ALL | Erase memory. Default: ERASE_ALL (INFO & MAIN) Wed Jan 22 16:38:31 2020: ERASE_MAIN | ERASE_MAIN: erase MAIN memory only Wed Jan 22 16:38:31 2020: ERASE_SEGMENT | ERASE_SEGMENT: erase segment to be programmed only Wed Jan 22 16:38:31 2020: ERASE_TOTAL | ERASE_TOTAL: applicable for FR5xx/FR6xx only! Wed Jan 22 16:38:31 2020: ERASE_USER_CODE | ERASE_USER_CODE: applicable for FR4xx only! Wed Jan 22 16:38:31 2020: NO_ERASE NO_ERASE: use only with -w switch Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -p JTAG PASSWORD Specifies the JTAG password that should be used Wed Jan 22 16:38:31 2020: to open a password protected target device Wed Jan 22 16:38:31 2020: (supported on FRAM devices only). The user is Wed Jan 22 16:38:31 2020: prompted if the password is incompatible with Wed Jan 22 16:38:31 2020: the password length deteced by MSP Flasher. Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -o L | C Operating mode for L092 and RF430FR152H family Wed Jan 22 16:38:31 2020: devices. L = L092 mode (normal mode) Wed Jan 22 16:38:31 2020: C = C092 mode (ROM development mode) Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -f Permanently secures JTAG access to the target MSP. Wed Jan 22 16:38:31 2020: Caution: The device will no longer be accessible Wed Jan 22 16:38:31 2020: through JTAG or Spy-Bi-Wire. This action Wed Jan 22 16:38:31 2020: is irreversible. Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -g Disables the logging mechanism. Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -a Causes a nonintrusive target connection: use Wed Jan 22 16:38:31 2020: this switch if no reset should be applied to Wed Jan 22 16:38:31 2020: the target device on start up. Correct target Wed Jan 22 16:38:31 2020: device name must be specified using the -n switch. Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -s Suppresses the FET firmware update prompt. Wed Jan 22 16:38:31 2020: In case of a mismatch between MSP Debug Stack Wed Jan 22 16:38:31 2020: and FET firmware, an update is forced. Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -q QUIET mode: No system messages will be displayed Wed Jan 22 16:38:31 2020: (except for errors and user prompts) Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: -z [exit_spec,...] Specifies the state of the device after Wed Jan 22 16:38:31 2020: programming. View available 'exit_spec's using Wed Jan 22 16:38:31 2020: -x switch). Use ", " as a delimiter. Wed Jan 22 16:38:31 2020: Wed Jan 22 16:38:31 2020: For a GUI-based alternative, check out UniFlash: http://ti.com/tool/uniflash Wed Jan 22 16:38:31 2020: ******************************************************************************* Wed Jan 22 16:38:31 2020: Press ENTER to continue. Wed Jan 22 16:38:47 2020: * -----/|-------------------------------------------------------------------- * Wed Jan 22 16:38:47 2020: * / |__ * Wed Jan 22 16:38:47 2020: * /_ / MSP Flasher v1.3.20 * Wed Jan 22 16:38:47 2020: * | / * Wed Jan 22 16:38:47 2020: * -----|/-------------------------------------------------------------------- * Wed Jan 22 16:38:47 2020: * Wed Jan 22 16:38:47 2020: * Evaluating triggers...done Wed Jan 22 16:38:47 2020: * Executing FET detection sweep: Wed Jan 22 16:38:47 2020: - 1: MSP-FET @ COM6 Wed Jan 22 16:38:47 2020: - Select FET number: Wed Jan 22 16:38:51 2020: 1 Wed Jan 22 16:38:51 2020: * Initializing interface @ COM6...done Wed Jan 22 16:38:51 2020: * Checking firmware compatibility: Wed Jan 22 16:38:51 2020: * FET firmware is up to date. Wed Jan 22 16:38:51 2020: * Reading FW version...done Wed Jan 22 16:38:51 2020: * Setting VCC to 3000 mV...done Wed Jan 22 16:38:57 2020: * Accessing device...done Wed Jan 22 16:38:57 2020: * Reading device information...done Wed Jan 22 16:38:58 2020: * Wed Jan 22 16:38:58 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:38:58 2020: * Arguments : -i DETECT Wed Jan 22 16:38:58 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:38:58 2020: * Driver : loaded Wed Jan 22 16:38:58 2020: * Dll Version : 31400000 Wed Jan 22 16:38:58 2020: * FwVersion : 31200000 Wed Jan 22 16:38:58 2020: * Interface : DETECT Wed Jan 22 16:38:58 2020: * HwVersion : U 3.0 Wed Jan 22 16:38:58 2020: * JTAG Mode : AUTO Wed Jan 22 16:38:58 2020: * Device : MSP430F5659 Wed Jan 22 16:38:58 2020: * EEM : Level 7, ClockCntrl 2 Wed Jan 22 16:38:58 2020: * VCC OFF Wed Jan 22 16:38:58 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:38:58 2020: * Powering down...done Wed Jan 22 16:38:58 2020: * Disconnecting from device...done Wed Jan 22 16:38:58 2020: * Wed Jan 22 16:38:58 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:38:58 2020: * Driver : closed (No error) Wed Jan 22 16:38:58 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:38:58 2020: */ Wed Jan 22 16:42:32 2020: * -----/|-------------------------------------------------------------------- * Wed Jan 22 16:42:32 2020: * / |__ * Wed Jan 22 16:42:32 2020: * /_ / MSP Flasher v1.3.20 * Wed Jan 22 16:42:32 2020: * | / * Wed Jan 22 16:42:32 2020: * -----|/-------------------------------------------------------------------- * Wed Jan 22 16:42:32 2020: * Wed Jan 22 16:42:32 2020: * Evaluating triggers...done Wed Jan 22 16:42:32 2020: * Checking for available FET debuggers: Wed Jan 22 16:42:32 2020: * Found USB FET @ COM6 <- Selected Wed Jan 22 16:42:32 2020: * Initializing interface @ COM6...done Wed Jan 22 16:42:33 2020: * Checking firmware compatibility: Wed Jan 22 16:42:33 2020: * FET firmware is up to date. Wed Jan 22 16:42:33 2020: * Reading FW version...done Wed Jan 22 16:42:33 2020: * Setting VCC to 3000 mV...done Wed Jan 22 16:42:33 2020: * Accessing device...done Wed Jan 22 16:42:33 2020: * Reading device information...done Wed Jan 22 16:42:33 2020: * Loading file into device... Wed Jan 22 16:42:40 2020: # Exit: 59 Wed Jan 22 16:42:40 2020: # ERROR: Could not erase device memory Wed Jan 22 16:42:40 2020: * Powering down...done Wed Jan 22 16:42:40 2020: * Disconnecting from device...done Wed Jan 22 16:42:40 2020: * Wed Jan 22 16:42:40 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:42:40 2020: * Driver : closed (No error) Wed Jan 22 16:42:40 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:42:40 2020: */ Wed Jan 22 16:42:58 2020: * -----/|-------------------------------------------------------------------- * Wed Jan 22 16:42:58 2020: * / |__ * Wed Jan 22 16:42:58 2020: * /_ / MSP Flasher v1.3.20 * Wed Jan 22 16:42:58 2020: * | / * Wed Jan 22 16:42:58 2020: * -----|/-------------------------------------------------------------------- * Wed Jan 22 16:42:58 2020: * Wed Jan 22 16:42:58 2020: * Evaluating triggers...done Wed Jan 22 16:42:58 2020: * Checking for available FET debuggers: Wed Jan 22 16:42:58 2020: * Found USB FET @ COM6 <- Selected Wed Jan 22 16:42:58 2020: * Initializing interface @ COM6...done Wed Jan 22 16:42:59 2020: * Checking firmware compatibility: Wed Jan 22 16:42:59 2020: * FET firmware is up to date. Wed Jan 22 16:42:59 2020: * Reading FW version...done Wed Jan 22 16:42:59 2020: * Setting VCC to 3000 mV...done Wed Jan 22 16:42:59 2020: * Accessing device...done Wed Jan 22 16:42:59 2020: * Reading device information...done Wed Jan 22 16:42:59 2020: * Erasing device memory...done Wed Jan 22 16:43:01 2020: * Wed Jan 22 16:43:01 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:43:01 2020: * Arguments : -e ERASE_ALL Wed Jan 22 16:43:01 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:43:01 2020: * Driver : loaded Wed Jan 22 16:43:01 2020: * Dll Version : 31400000 Wed Jan 22 16:43:01 2020: * FwVersion : 31200000 Wed Jan 22 16:43:01 2020: * Interface : TIUSB Wed Jan 22 16:43:01 2020: * HwVersion : U 3.0 Wed Jan 22 16:43:01 2020: * JTAG Mode : AUTO Wed Jan 22 16:43:01 2020: * Device : MSP430F5659 Wed Jan 22 16:43:01 2020: * EEM : Level 7, ClockCntrl 2 Wed Jan 22 16:43:01 2020: * Erase Mode : ERASE_ALL Wed Jan 22 16:43:01 2020: * VCC OFF Wed Jan 22 16:43:01 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:43:01 2020: * Powering down...done Wed Jan 22 16:43:01 2020: * Disconnecting from device...done Wed Jan 22 16:43:01 2020: * Wed Jan 22 16:43:01 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:43:01 2020: * Driver : closed (No error) Wed Jan 22 16:43:01 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:43:01 2020: */ Wed Jan 22 16:43:05 2020: * -----/|-------------------------------------------------------------------- * Wed Jan 22 16:43:05 2020: * / |__ * Wed Jan 22 16:43:05 2020: * /_ / MSP Flasher v1.3.20 * Wed Jan 22 16:43:05 2020: * | / * Wed Jan 22 16:43:05 2020: * -----|/-------------------------------------------------------------------- * Wed Jan 22 16:43:05 2020: * Wed Jan 22 16:43:05 2020: * Evaluating triggers...done Wed Jan 22 16:43:05 2020: * Checking for available FET debuggers: Wed Jan 22 16:43:06 2020: * Found USB FET @ COM6 <- Selected Wed Jan 22 16:43:06 2020: * Initializing interface @ COM6...done Wed Jan 22 16:43:06 2020: * Checking firmware compatibility: Wed Jan 22 16:43:06 2020: * FET firmware is up to date. Wed Jan 22 16:43:06 2020: * Reading FW version...done Wed Jan 22 16:43:06 2020: * Setting VCC to 3000 mV...done Wed Jan 22 16:43:06 2020: * Accessing device...done Wed Jan 22 16:43:07 2020: * Reading device information...done Wed Jan 22 16:43:07 2020: * Loading file into device... Wed Jan 22 16:43:10 2020: # Exit: 59 Wed Jan 22 16:43:10 2020: # ERROR: Could not write device memory Wed Jan 22 16:43:10 2020: * Powering down...done Wed Jan 22 16:43:15 2020: * Disconnecting from device...done Wed Jan 22 16:43:15 2020: * Wed Jan 22 16:43:15 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:43:15 2020: * Driver : closed (No error) Wed Jan 22 16:43:15 2020: * ---------------------------------------------------------------------------- Wed Jan 22 16:43:15 2020: */