// //Script example MSP432 UART BSL //Device : MSP432P401R //Comm Bridge: XDS110 - MSP432LP BackChannelUART // for this setting, the parity need to be // set from Scripter side // When MSP-BSL Rocket is used, parity will be // generated by the Rocket // //Download blink application to //MSP432 device through UART BSL // LOG MODE P4xx UART 9600 COM71 PARITY RX_PASSWORD_32 pass256_wrong.txt RX_PASSWORD_32 pass256_default.txt MASS_ERASE RX_DATA_BLOCK_32 Datenlogger.txt //RX_DATA_BLOCK_32 BSL_TEST.txt //RX_DATA_BLOCK_32 Blink_LED.hex TX_BSL_VERSION_32 TX_DATA_BLOCK_32 0x0000 0x4000 ReadBlock_cleanDevice.txt //TX_DATA_BLOCK_32 0x0000 0x4000 ReadBlock_MSP432P401R.hex REBOOT_RESET