// Define a size for the CLA scratchpad area that will be used // by the CLA compiler for local symbols and temps // Also force references to the special symbols that mark the // scratchpad are. CLA_SCRATCHPAD_SIZE = 0x100; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x080000, length = 0x000002 RAMM0 : origin = 0x0000F3, length = 0x00030D RAMLS0 : origin = 0x008000, length = 0x000800 RAMLS3 : origin = 0x009800, length = 0x000800 RAMLS4 : origin = 0x00A000, length = 0x000800 RESET : origin = 0x3FFFC0, length = 0x000002 /* Flash sectors */ /* BANK 0 */ FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE /* on-chip Flash */ FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x00F80 /* on-chip Flash */ CSM_RSVD : origin = 0x08FF82, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ CSM_PWL_P0 : origin = 0x08FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ /* BANK 1 */ FLASH_BANK1_SEC0 : origin = 0x090000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC1 : origin = 0x091000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC2 : origin = 0x092000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC3 : origin = 0x093000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC4 : origin = 0x094000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC5 : origin = 0x095000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC6 : origin = 0x096000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC7 : origin = 0x097000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC8 : origin = 0x098000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC9 : origin = 0x099000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x000FF0 /* on-chip Flash */ FPUTABLES : origin = 0x3F9200, length = 0x001800 /* FPU Tables in Boot ROM */ // IQTABLES : origin = 0x3F0800, length = 0x000F00 /* IQ Math Tables in Boot ROM */ // IQTABLES2 : origin = 0x3F1700, length = 0x000100 /* IQ Math Tables in Boot ROM */ // IQTABLES3 : origin = 0x3F1800, length = 0x000100 /* IQ Math Tables in Boot ROM */ ROM : origin = 0x3FEB22, length = 0x000B13 /* Boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ PAGE 1 : BOOT_RSVD : origin = 0x000002, length = 0x0000F1 /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */ // RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ RAMLS1 : origin = 0x008800, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x000800 RAMLS5 : origin = 0x00A800, length = 0x000800 RAMLS6 : origin = 0x00B000, length = 0x000800 RAMLS7 : origin = 0x00B800, length = 0x000800 RAMGS0 : origin = 0x00C000, length = 0x002000 RAMGS1 : origin = 0x00E000, length = 0x002000 RAMGS2 : origin = 0x010000, length = 0x002000 RAMGS3 : origin = 0x012000, length = 0x001FF8 // RAMGS3_RSVD : origin = 0x013FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 // CLA_CPU_MSGRAM : origin = 0x001480, length = 0x000080 /* CLA-R/W, CPU-R message RAM */ // CPU_CLA_MSGRAM : origin = 0x001500, length = 0x000080 /* CPU-R/W, CLA-R message RAM */ } SECTIONS { .cinit : > FLASH_BANK0_SEC0, PAGE = 0, ALIGN(4) .text : >>FLASH_BANK0_SEC1 | FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3 | FLASH_BANK0_SEC4 | FLASH_BANK0_SEC5 | FLASH_BANK0_SEC6 | FLASH_BANK0_SEC7 | FLASH_BANK0_SEC8 | FLASH_BANK0_SEC9 | FLASH_BANK0_SEC10 | FLASH_BANK0_SEC11 | FLASH_BANK0_SEC12 , PAGE = 0, ALIGN(4) codestart : > BEGIN PAGE = 0, ALIGN(4) .stack : > RAMM1 PAGE = 1 .switch : > FLASH_BANK0_SEC0, PAGE = 0, ALIGN(4) #if defined(__TI_EABI__) .init_array : > FLASH_BANK0_SEC0, PAGE = 0, ALIGN(4) .bss : > RAMLS5, PAGE = 1 .bss:output : > RAMLS5, PAGE = 1 .bss:cio : > RAMLS5, PAGE = 1 .data : > RAMLS6, PAGE = 1 .sysmem : > RAMLS6, PAGE = 1 .const : >> FLASH_BANK0_SEC14 | FLASH_BANK0_SEC15, PAGE = 0, ALIGN(4) #else .pinit : > FLASH_BANK0_SEC0, PAGE = 0, ALIGN(4) .ebss : >>RAMLS5 | RAMLS6 | RAMLS7 | RAMGS0 , PAGE = 1 .esysmem : > RAMLS6, PAGE = 1 .cio : > RAMLS5, PAGE = 1 .econst : >>FLASH_BANK0_SEC14 | FLASH_BANK0_SEC15, PAGE = 0, ALIGN(4) #endif ramgs0 : > RAMGS0, PAGE = 1 ramgs1 : > RAMGS1, PAGE = 1 .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ csmpasswds : > CSM_PWL_P0, PAGE = 0 csm_rsvd : > CSM_RSVD, PAGE = 0 /* Allocate IQ math areas: */ // IQmath : > FLASH_BANK0_SEC13, PAGE = 0 /* Math Code */ // IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD /* Allocate IQ math areas: */ IQmath : > FLASH_BANK1_SEC2, PAGE = 0, ALIGN(8) /* Math Code */ IQmathTables : > FLASH_BANK1_SEC3, PAGE = 0, ALIGN(8) /* Allocate FPU math areas: */ FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD debug_buffer : > RAMGS3, PAGE = 1 vectors : > VECTORS, PAGE = 0, TYPE = DSECT #if defined(__TI_EABI__) /* CLA specific sections */ Cla1Prog : LOAD = FLASH_BANK1_SEC0, RUN = RAMLS0, LOAD_START(Cla1ProgLoadStart), RUN_START(Cla1ProgRunStart), LOAD_SIZE(Cla1ProgLoadSize), PAGE = 0, ALIGN(4) #else /* CLA specific sections */ Cla1Prog : LOAD = FLASH_BANK1_SEC0, RUN = RAMLS0, LOAD_START(_Cla1ProgLoadStart), RUN_START(_Cla1ProgRunStart), LOAD_SIZE(_Cla1ProgLoadSize), PAGE = 0, ALIGN(4) #endif Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1 #if defined(__TI_EABI__) .TI.ramfunc : LOAD = FLASH_BANK0_SEC0, RUN = RAMLS4 LOAD_START(RamfuncsLoadStart), LOAD_SIZE(RamfuncsLoadSize), LOAD_END(RamfuncsLoadEnd), RUN_START(RamfuncsRunStart), RUN_SIZE(RamfuncsRunSize), RUN_END(RamfuncsRunEnd), PAGE = 0, ALIGN(4) #else .TI.ramfunc : LOAD = FLASH_BANK0_SEC0, RUN = RAMLS4 LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(4) #endif .scratchpad : >> RAMGS1 | RAMGS2 | RAMGS3 , PAGE = 1 // .scratchpad : > RAMGS1, PAGE = 1 .bss_cla : > RAMLS1, PAGE = 1 Cla1DataRam : > RAMLS2, PAGE = 1 cla_shared : > RAMLS1, PAGE = 1 CLAmathTables : > RAMLS1, PAGE = 1 CLA1mathTables : > RAMLS1, PAGE = 1 #if defined(__TI_EABI__) .const_cla : LOAD = FLASH_BANK1_SEC2, RUN = RAMLS3, RUN_START(Cla1ConstRunStart), LOAD_START(Cla1ConstLoadStart), LOAD_SIZE(Cla1ConstLoadSize), PAGE = 0, ALIGN(4) #else .const_cla : LOAD = FLASH_BANK1_SEC2, RUN = RAMLS3, RUN_START(_Cla1ConstRunStart), LOAD_START(_Cla1ConstLoadStart), LOAD_SIZE(_Cla1ConstLoadSize), PAGE = 0, ALIGN(4) #endif CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > RAMGS3, PAGE = 1, ALIGN=2 } /* //=========================================================================== // End of file. //=========================================================================== */