/* //########################################################################### // // FILE: 28069_RAM_CLA_C_lnk.cmd // // TITLE: Linker Command File For F28069 examples that run out of RAM // // This ONLY includes all SARAM blocks on the F28069 device. // This does not include flash or OTP. // // Keep in mind that L0,L1,L2,L3 and L4 are protected by the code // security module. // // What this means is in most cases you will want to move to // another memory map file which has more memory defined. // //########################################################################### // $TI Release: F2806x C/C++ Header Files and Peripheral Examples V150 $ // $Release Date: June 16, 2015 $ // $Copyright: Copyright (C) 2011-2015 Texas Instruments Incorporated - // http://www.ti.com/ ALL RIGHTS RESERVED $ //########################################################################### */ /* ====================================================== // For Code Composer Studio V2.2 and later // --------------------------------------- // In addition to this memory linker command file, // add the header linker command file directly to the project. // The header linker command file is required to link the // peripheral structures to the proper locations within // the memory map. // // The header linker files are found in \F2806x_headers\cmd // // For BIOS applications add: F2806x_Headers_BIOS.cmd // For nonBIOS applications add: F2806x_Headers_nonBIOS.cmd ========================================================= */ /* ====================================================== // For Code Composer Studio prior to V2.2 // -------------------------------------- // 1) Use one of the following -l statements to include the // header linker command file in the project. The header linker // file is required to link the peripheral structures to the proper // locations within the memory map */ /* Uncomment this line to include file only for non-BIOS applications */ /* -l F2806x_Headers_nonBIOS.cmd */ /* Uncomment this line to include file only for BIOS applications */ /* -l F2806x_Headers_BIOS.cmd */ /* 2) In your project add the path to \F2806x_headers\cmd to the library search path under project->build options, linker tab, library search path (-i). /*========================================================= */ /* Define the memory block start/length for the F2806x PAGE 0 will be used to organize program sections PAGE 1 will be used to organize data sections Notes: Memory blocks on F28069 are uniform (ie same physical memory) in both PAGE 0 and PAGE 1. That is the same memory region should not be defined for both PAGE 0 and PAGE 1. Doing so will result in corruption of program and/or data. Contiguous SARAM memory blocks can be combined if required to create a larger memory block. */ _Cla1Prog_Start = _Cla1funcsRunStart; -heap 0x400 -stack 0x400 // Define a size for the CLA scratchpad area that will be used // by the CLA compiler for local symbols and temps // Also force references to the special symbols that mark the // scratchpad are. CLA_SCRATCHPAD_SIZE = 0x100; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x3F7FF6, length = 0x000002 //start at flash and not RAM. RAML5L8 : origin = 0x00C000, length = 0x006000 RAML8 : origin = 0x012000, length = 0x002000 FLASH_AB : origin = 0x3F0000, length = 0x007F80 /* on-chip FLASH */ /* RAML0_L2 : origin = 0x008000, length = 0x001000 */ RAML3 : origin = 0x009000, length = 0x001000 RESET : origin = 0x3FFFC0, length = 0x000002 /* FPU Tables in Boot ROM */ FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* IQ Math Tables in Boot ROM */ IQTABLES : origin = 0x3FDF00, length = 0x000B50 IQTABLES2 : origin = 0x3FEA50, length = 0x00008C IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA BOOTROM : origin = 0x3FF3B0, length = 0x000C10 //PAGE 1 : /* Part of M0, BOOT rom will use this for stack */ BOOT_RSVD : origin = 0x000002, length = 0x00004E /* on-chip RAM block M1 */ RAMM0 : origin = 0x000050, length = 0x000400 RAMM1 : origin = 0x000480, length = 0x000380 CLARAM0 : origin = 0x008800, length = 0x000400 CLARAM1 : origin = 0x008C00, length = 0x000400 CLARAM2 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L4-L8 */ RAML4 : origin = 0x00A000, length = 0x002000 /* RAML5 : origin = 0x00C000, length = 0x002000 */ /* RAML6 : origin = 0x00E000, length = 0x002000 */ /* RAML7 : origin = 0x010000, length = 0x002000 */ /* RAML8 : origin = 0x012000, length = 0x002000 */ FLASH_CD : origin = 0x3E8000, length = 0x008000 /* on-chip FLASH */ CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 } SECTIONS { /*** User Defined Sections ***/ codestart : > BEGIN, PAGE = 0 /* Used by file CodeStartBranch.asm */ wddisable : > FLASH_AB, PAGE = 0 /* Used by file CodeStartBranch.asm */ copysections : > FLASH_AB, PAGE = 0 /* Used by file SectionCopy.asm */ ramfuncs : > RAMM1, PAGE = 0 // .text : > RAML5L8, PAGE = 0 // .cinit : > RAMM0, PAGE = 0 // .pinit : > RAMM0, PAGE = 0 // .switch : > RAMM0, PAGE = 0 .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ .stack : > RAMM0, PAGE = 0 .ebss : > RAML4, PAGE = 0 // .econst : > RAML4, PAGE = 0 .esysmem : > RAML4, PAGE = 0 .sysmem : > RAML4, PAGE = 0 .cio : > RAML4, PAGE = 0 .scratchpad : > CLARAM0, PAGE = 0 .bss_cla : > CLARAM0, PAGE = 0 .const_cla : > CLARAM0, PAGE = 0 IQmath : > RAML4, PAGE = 0 IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD /* Allocate FPU math areas: */ FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD .cinit : LOAD = FLASH_AB, PAGE = 0 /* Load section to Flash */ RUN = RAML5L8 , PAGE = 0 /* Run section from RAM */ LOAD_START(_cinit_loadstart), RUN_START(_cinit_runstart), SIZE(_cinit_size) .const : LOAD = FLASH_AB, PAGE = 0 /* Load section to Flash */ RUN = RAML5L8 , PAGE = 0 /* Run section from RAM */ LOAD_START(_const_loadstart), RUN_START(_const_runstart), SIZE(_const_size) .econst : LOAD = FLASH_CD, PAGE = 0 /* Load section to Flash */ RUN = RAML4, PAGE = 0 /* Run section from RAM */ LOAD_START(_econst_loadstart), RUN_START(_econst_runstart), SIZE(_econst_size) .pinit : LOAD = FLASH_AB, PAGE = 0 /* Load section to Flash */ RUN = RAML5L8 , PAGE = 0 /* Run section from RAM */ LOAD_START(_pinit_loadstart), RUN_START(_pinit_runstart), SIZE(_pinit_size) .switch : LOAD = FLASH_AB, PAGE = 0 /* Load section to Flash */ RUN = RAML5L8 , PAGE = 0 /* Run section from RAM */ LOAD_START(_switch_loadstart), RUN_START(_switch_runstart), SIZE(_switch_size) .text : LOAD = FLASH_AB, PAGE = 0 /* Load section to Flash */ RUN = RAML5L8 , PAGE = 0 /* Run section from RAM */ LOAD_START(_text_loadstart), RUN_START(_text_runstart), SIZE(_text_size) Cla1Prog : LOAD = FLASH_CD, PAGE = 0 RUN = RAML8, PAGE = 0 LOAD_START(_Cla1funcsLoadStart), LOAD_END(_Cla1funcsLoadEnd), RUN_START(_Cla1funcsRunStart), LOAD_SIZE(_Cla1funcsLoadSize) Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 0 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 0 Cla1DataRam0 : > CLARAM0, PAGE = 0 Cla1DataRam1 : > CLARAM1, PAGE = 0 Cla1DataRam2 : > CLARAM2, PAGE = 0 CLA1mathTables : > CLARAM1, LOAD_START(_Cla1mathTablesLoadStart), LOAD_END(_Cla1mathTablesLoadEnd), LOAD_SIZE(_Cla1mathTablesLoadSize), RUN_START(_Cla1mathTablesRunStart), PAGE = 0 CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > CLARAM0, PAGE = 0 /* Uncomment the section below if calling the IQNexp() or IQexp() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD { IQmath.lib (IQmathTablesRam) } */ /* Uncomment the section below if calling the IQNasin() or IQasin() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD { IQmath.lib (IQmathTablesRam) } */ } /* //=========================================================================== // End of file. //=========================================================================== */