#include #include int num=0; void setup() { Wire.begin(); pinMode(A3, OUTPUT); digitalWrite(A3, HIGH); pinMode(3,OUTPUT); //debug to led 3 //power amp setup Wire.beginTransmission(0xE0); //write enable register if(Wire.available()) { num = 1; } Wire.write(0x02); // register address 0X02 if(Wire.available()) { num = 1; } Wire.write(0x0C); // SWS '0', HPL and HPR enabled, class D disable if(Wire.available()) { num = 1; } Wire.endTransmission(); delay(100); Wire.beginTransmission(0xE0); //write enable register if(Wire.available()) { num = 1; } Wire.write(0x03); // register address was 0X03 if(Wire.available()) { num = 1; } Wire.write(0x81); // LIM_LOCK enable, mode 001, I want this at the heaphones if(Wire.available()) { num = 1; } Wire.endTransmission(); delay(100); Wire.beginTransmission(0xE0); if(Wire.available()) { num = 1; } Wire.write(0x05); // register address was 0X05 if(Wire.available()) { num = 1; } Wire.write(0x13); // volume num = 1; } Wire.endTransmission(); delay(100); Wire.beginTransmission(0xE0); if(Wire.available()) { num = 1; } Wire.write(0x06); // register address was 0X06 if(Wire.available()) { num = 1; } Wire.write(0x13); // volume data if(Wire.available()) { num = 1; } Wire.endTransmission(); delay(100); Wire.beginTransmission(0xE0); if(Wire.available()) { num = 1; } Wire.write(0x07); // register address was 0X07 if(Wire.available()) { num = 1; } Wire.write(0x12); // HP voltage and gain if(Wire.available()) { num = 1; } Wire.endTransmission(); delay(100); } void loop() { if(num ==1){ digitalWrite(3,HIGH); } }