void TAS_Init(void) { delay_ms(50); TAS_txone(0x1B, 0x00); //Oscillator trim delay_ms(75); TAS_txone(0x07, 0x30); //Master volume @ -9dB delay_ms(50); TAS_txone(0x0E, 0x91); //Volume slew rate @ 1024 steps (85mS@48kHz) delay_ms(50); TAS_txone(0x19, 0x3A); //PWM shutdown group - PBTL setting delay_ms(50); TAS_txx(0x25, 0x01, 0x10, 0x32, 0x45); //PWM Output Mux - PBTL setting delay_ms(50); TAS_txx(0x20, 0x00, 0x81, 0x77, 0x72); //nput Mux Reg - BD mode setting delay_ms(50); //The following registers 11-14 are inter-channel delay (ICD) for PBTL TAS_txone(0x11, 0xB8); delay_ms(50); TAS_txone(0x12, 0x60); delay_ms(50); TAS_txone(0x13, 0xA0); delay_ms(50); TAS_txone(0x14, 0x48); delay_ms(50); }