static const unsigned char R3C_DATA[8] = {0x00,0x00,0x0c,0x78,0xFF,0xFF,0xFE,0xDB };//42ms static const unsigned char R46_DATA[4] = {0x00,0x02,0x06,0x23}; static const unsigned char R40_DATA[8] = {0x06,0x63,0x00,0x00,0x06,0x62,0xFF,0xFF}; static const unsigned char R3B_DATA[8] = {0x00,0x01,0x40,0x3F,0x00,0x7E,0xBF,0xC1}; static const unsigned char R20_DATA[4] = {0x00,0x01,0x77,0x72}; static const unsigned char R25_DATA[4] = {0x01,0x10,0x32,0x45}; static const unsigned char R50_DATA[4] = {0x00,0x00,0x00,0x10};//EQ ON static const unsigned char R51_DATA[8] = {0x00,0x80,0x00,0x00,0x00,0x00,0x00,0x00}; static const unsigned char R52_DATA[8] = {0x00,0x80,0x00,0x00,0x00,0x00,0x00,0x00}; ///////////////////////////////////////////////////////////////////////////////////// static const unsigned char R70_DATA_L[4] = {0x00,0x80,0x00,0x00}; static const unsigned char R74_DATA_L[4] = {0x00,0x80,0x00,0x00}; static const unsigned char R72_DATA_L[4] = {0x00,0x00,0x00,0x00}; static const unsigned char R73_DATA_L[4] = {0x00,0x80,0x00,0x00}; static const unsigned char R76_DATA_L[4] = {0x00,0x80,0x00,0x00}; static const unsigned char R77_DATA_L[4] = {0x00,0x00,0x00,0x00}; ////////////////////////////////////////////////////////////////////////////////////// static const unsigned char R70_DATA_R[4] = {0x00,0x80,0x00,0x00}; static const unsigned char R74_DATA_R[4] = {0x00,0x80,0x00,0x00}; static const unsigned char R72_DATA_R[4] = {0x00,0x80,0x00,0x00}; static const unsigned char R73_DATA_R[4] = {0x00,0x00,0x00,0x00}; static const unsigned char R76_DATA_R[4] = {0x00,0x00,0x00,0x00}; static const unsigned char R77_DATA_R[4] = {0x00,0x80,0x00,0x00}; void init(void) { TAS5715_L_Byte_Write(0x1B,0); //Enable Factory PLL trim DelayMs(80); TAS5715_L_Byte_Write(0x06,0x07); //soft mute TAS5715_L_Byte_Write(0x03,0x80); TAS5715_L_Byte_Write(0x04,0x05); TAS5715_L_Byte_Write(0x07,0xFF); TAS5715_L_Byte_Write(0x08,0x1C); TAS5715_L_Byte_Write(0x09,0x1C); TAS5715_L_Byte_Write(0x0C,0xFF); TAS5715_L_Byte_Write(0x11,0xAC); //aD mode TAS5715_L_Byte_Write(0x12,0x54); // TAS5715_L_Byte_Write(0x13,0xAC); // TAS5715_L_Byte_Write(0x14,0x54); // TAS5715_L_Byte_Write(0x1a,0x16); // TAS5715_L_Byte_Write(0x19,0x3A);//all channel ON TAS5715_L_Array_Write(0x20,4,(UINT8 *)R20_DATA); //L->ch1,L->CH2 TAS5715_L_Array_Write(0x25,4,(UINT8 *)R25_DATA); TAS5715_L_Array_Write(0x50,4,(UINT8 *)R50_DATA); TAS5715_L_Array_Write(0x51,8,(UINT8 *)R51_DATA); TAS5715_L_Array_Write(0x52,8,(UINT8 *)R52_DATA); TAS5715_L_Array_Write(0x46,4,(UINT8 *)R46_DATA); TAS5715_L_Array_Write(0x72,4,(UINT8 *)R72_DATA_L); TAS5715_L_Array_Write(0x73,4,(UINT8 *)R73_DATA_L); TAS5715_L_Array_Write(0x76,4,(UINT8 *)R76_DATA_L); TAS5715_L_Array_Write(0x77,4,(UINT8 *)R77_DATA_L); TAS5715_L_Array_Write(0x70,4,(UINT8 *)R70_DATA_L); TAS5715_L_Array_Write(0x74,4,(UINT8 *)R74_DATA_L); TAS5715_L_Array_Write(0x3B,8,(UINT8 *)R3B_DATA);//SOFT FILTER TAS5715_L_Array_Write(0x3C,8,(UINT8 *)R3C_DATA);//ATTK RELEASE TAS5715_L_Array_Write(0x40,8,(UINT8 *)R40_DATA);//threshold TAS5715_L_Byte_Write(0x05,0x00); //exit all-channel shutdown (hard unmute) }