U-Boot SPL 2011.09 (Jul 26 2012 - 17:18:20) Texas Instruments Revision detection unimplemented No daughter card present OMAP SD/MMC: 0 reading u-boot.img reading u-boot.img U-Boot 2011.09 (Jul 26 2012 - 17:13:38) I2C: ready DRAM: 256 MiB WARNING: Caches not enabled No daughter card present NAND: HW ECC Hamming Code selected No NAND device found!!! 0 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - readenv() failed, using default environment Net: cpsw Hit any key to stop autoboot: 0 SD/MMC found on device 0 reading uEnv.txt 261 bytes read Loaded environment from uEnv.txt Importing environment from mmc ... Running uenvcmd ... Booting from network... Auto Negotitation failed for port 1 link up on port 0, speed 100, full duplex BOOTP broadcast 1 DHCP client bound to address 10.5.5.93 Using cpsw device TFTP from server 10.5.5.86; our IP address is 10.5.5.93 Filename 'uImage-am335x-evm.bin'. Load address: 0x82000000 Loading: ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################# done Bytes transferred = 3163680 (304620 hex) ## Booting kernel from Legacy Image at 82000000 ... Image Name: Arago/3.2.0-psp04.06.00.08.sdk/a Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3163616 Bytes = 3 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 3.2.0 (jenkins@sdit-build01) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Thu Jul 26 17:16:27 CDT 2012 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES1.0 (sgx neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/nfs nfsroot=10.5.5.86:/home/ngrutman/ti-sdk-am335x-evm-05.05.00. 00/targetNFS,nolock rw ip=dhcp [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Memory: 256MB = 256MB total [ 0.000000] Memory: 253256k/253256k available, 8888k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc059d000 (5716 kB) [ 0.000000] .init : 0xc059d000 - 0xc05db000 ( 248 kB) [ 0.000000] .data : 0xc05dc000 - 0xc0644198 ( 417 kB) [ 0.000000] .bss : 0xc06441bc - 0xc0671024 ( 180 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000122] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144) [ 0.058532] pid_max: default: 32768 minimum: 301 [ 0.058654] Security Framework initialized [ 0.058776] Mount-cache hash table entries: 512 [ 0.059143] CPU: Testing write buffer coherency: ok [ 0.079040] omap_hwmod: pruss: failed to hardreset [ 0.080139] print_constraints: dummy: [ 0.080505] NET: Registered protocol family 16 [ 0.082580] OMAP GPIO hardware version 0.1 [ 0.085144] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.087341] omap_i2c.1: alias fck already exists [ 0.088195] omap2_mcspi.1: alias fck already exists [ 0.088409] omap2_mcspi.2: alias fck already exists [ 0.089172] edma.0: alias fck already exists [ 0.089202] edma.0: alias fck already exists [ 0.089202] edma.0: alias fck already exists [ 0.115783] bio: create slab at 0 [ 0.117950] SCSI subsystem initialized [ 0.119628] usbcore: registered new interface driver usbfs [ 0.119934] usbcore: registered new interface driver hub [ 0.120117] usbcore: registered new device driver usb [ 0.120300] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3 [ 0.120574] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1 [ 0.138610] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.140472] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.142883] print_constraints: VRTC: [ 0.144317] print_constraints: VIO: at 1500 mV [ 0.146636] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal [ 0.148925] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal [ 0.149932] print_constraints: VDD3: 5000 mV [ 0.151336] print_constraints: VDIG1: at 1800 mV [ 0.152770] print_constraints: VDIG2: at 1800 mV [ 0.154174] print_constraints: VPLL: at 1800 mV [ 0.155609] print_constraints: VDAC: at 1800 mV [ 0.157012] print_constraints: VAUX1: at 1800 mV [ 0.158447] print_constraints: VAUX2: at 3300 mV [ 0.159881] print_constraints: VAUX33: at 3300 mV [ 0.161315] print_constraints: VMMC: at 3300 mV [ 0.161804] tps65910 1-002d: No interrupt support, no core IRQ [ 0.163024] Advanced Linux Sound Architecture Driver Version 1.0.24. [ 0.164154] Switching to clocksource gp timer [ 0.179504] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.179687] musb-hdrc musb-hdrc.0: dma type: pio [ 0.179992] MUSB0 controller's USBSS revision = 4ea20800 [ 0.180541] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using PIO, IRQ 18 [ 0.180725] musb-hdrc musb-hdrc.1: dma type: pio [ 0.180999] MUSB1 controller's USBSS revision = 4ea20800 [ 0.181121] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.181182] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 0.181335] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.181335] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.181365] usb usb1: Product: MUSB HDRC host driver [ 0.181365] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd [ 0.181365] usb usb1: SerialNumber: musb-hdrc.1 [ 0.182159] hub 1-0:1.0: USB hub found [ 0.182189] hub 1-0:1.0: 1 port detected [ 0.182708] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using PIO, IRQ 19 [ 0.183105] NET: Registered protocol family 2 [ 0.183319] IP route cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.183593] TCP established hash table entries: 8192 (order: 4, 65536 bytes) [ 0.183746] TCP bind hash table entries: 8192 (order: 3, 32768 bytes) [ 0.183837] TCP: Hash tables configured (established 8192 bind 8192) [ 0.183868] TCP reno registered [ 0.183868] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.183898] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.184082] NET: Registered protocol family 1 [ 0.184417] RPC: Registered named UNIX socket transport module. [ 0.184417] RPC: Registered udp transport module. [ 0.184448] RPC: Registered tcp transport module. [ 0.184448] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.184692] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.196014] VFS: Disk quotas dquot_6.5.2 [ 0.196075] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.196624] msgmni has been set to 494 [ 0.199707] alg: No test for stdrng (krng) [ 0.200378] io scheduler noop registered [ 0.200378] io scheduler deadline registered [ 0.200469] io scheduler cfq registered (default) [ 0.201629] Could not set LED4 to fully on [ 0.203399] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 0.827301] console [ttyO0] enabled [ 0.831542] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 0.839416] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 0.847198] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 0.854980] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 0.862731] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 0.879821] brd: module loaded [ 0.887878] loop: module loaded [ 0.891326] i2c-core: driver [tsl2550] using legacy suspend method [ 0.897827] i2c-core: driver [tsl2550] using legacy resume method [ 0.904235] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.964721] No daughter card found [ 0.968322] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.983520] Board name: A335X_SK [ 0.986877] Board version: 1.2B [ 0.990173] The board is a AM335x Starter Kit. [ 0.995056] omap_hsmmc.0: alias fck already exists [ 1.000579] omap_hsmmc.1: alias fck already exists [ 1.006591] da8xx_lcdc.0: alias fck already exists [ 1.012054] da8xx_lcdc da8xx_lcdc.0: GLCD: Found NHD-4.3-ATXI#-T-1 panel [ 1.027313] Console: switching to colour frame buffer device 60x34 [ 1.040191] davinci-mcasp.1: alias fck already exists [ 1.046081] Configure Bluetooth Enable pin... [ 1.051544] registered am33xx_sr device [ 1.055816] _regulator_get: 1-0018 supply Vdd not found, using dummy regulator [ 1.063415] _regulator_get: 1-0018 supply Vdd_IO not found, using dummy regulator [ 1.091857] lis3lv02d: 8 bits 3DLH sensor found [ 1.185180] input: ST LIS3LV02DL Accelerometer as /devices/platform/lis3lv02d/input/input0 [ 1.196044] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.203216] omap2-nand driver initializing [ 1.207702] OneNAND driver initializing [ 1.212921] CAN device driver interface [ 1.216979] CAN bus driver for Bosch D_CAN controller 1.0 [ 1.264801] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 1.271240] davinci_mdio davinci_mdio.0: detected phy mask fffffffc [ 1.279479] davinci_mdio.0: probed [ 1.283050] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown [ 1.290435] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown [ 1.298126] usbcore: registered new interface driver zd1201 [ 1.304138] usbcore: registered new interface driver cdc_ether [ 1.310394] usbcore: registered new interface driver cdc_eem [ 1.316467] usbcore: registered new interface driver dm9601 [ 1.322326] cdc_ncm: 04-Aug-2011 [ 1.325866] usbcore: registered new interface driver cdc_ncm [ 1.331787] Initializing USB Mass Storage driver... [ 1.337097] usbcore: registered new interface driver usb-storage [ 1.343383] USB Mass Storage support registered. [ 1.348663] mousedev: PS/2 mouse device common for all mice [ 1.355834] input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input1 [ 1.364257] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 [ 1.370941] omap_rtc: already running [ 1.374938] i2c /dev entries driver [ 1.378997] Linux video capture interface: v2.00 [ 1.384094] usbcore: registered new interface driver uvcvideo [ 1.390106] USB Video Class driver (1.1.1) [ 1.396423] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.404968] cpuidle: using governor ladder [ 1.409729] cpuidle: using governor menu [ 1.418579] omap4_aes_mod_init: loading AM33X AES driver [ 1.424224] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02 [ 1.430786] omap4_aes_probe: probe() done [ 1.435424] omap4_sham_mod_init: loading AM33X SHA/MD5 driver [ 1.441558] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03 [ 1.453002] omap4_sham_probe: probe() done [ 1.463104] usbcore: registered new interface driver usbhid [ 1.468963] usbhid: USB HID core driver [ 1.473602] usbcore: registered new interface driver snd-usb-audio [ 1.485168] _regulator_get: 1-001b supply IOVDD not found, using dummy regulator [ 1.492950] _regulator_get: 1-001b supply DVDD not found, using dummy regulator [ 1.500640] _regulator_get: 1-001b supply AVDD not found, using dummy regulator [ 1.508300] _regulator_get: 1-001b supply DRVDD not found, using dummy regulator [ 1.518768] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok [ 1.526611] ALSA device list: [ 1.529724] #0: AM335X EVM [ 1.532714] oprofile: hardware counters not available [ 1.537994] oprofile: using timer interrupt. [ 1.542480] nf_conntrack version 0.5.0 (3957 buckets, 15828 max) [ 1.549255] ip_tables: (C) 2000-2006 Netfilter Core Team [ 1.554931] TCP cubic registered [ 1.558288] NET: Registered protocol family 17 [ 1.562927] can: controller area network core (rev 20090105 abi 8) [ 1.569488] NET: Registered protocol family 29 [ 1.574096] can: raw protocol (rev 20090105) [ 1.578582] can: broadcast manager protocol (rev 20090105 t) [ 1.584503] Registering the dns_resolver key type [ 1.589508] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 1.597503] ThumbEE CPU extension supported. [ 1.602020] mux: Failed to setup hwmod io irq -22 [ 1.607543] Power Management for AM33XX family [ 1.612365] Trying to load am335x-pm-firmware.bin (60 secs timeout) [ 1.619079] Copied the M3 firmware to UMEM [ 1.623535] smartreflex smartreflex: am33xx_sr_probe: Zero NValue read from EFUSE [ 1.631378] smartreflex: probe of smartreflex failed with error -22 [ 1.638519] sr_init: platform driver register failed [ 1.648681] clock: disabling unused clocks to save power [ 1.665679] mmc0: host does not support reading read-only switch. assuming write-enable. [ 1.676025] Detected MACID=d4:94:a1:83:f:8c [ 1.681243] mmc0: new high speed SD card at address 1234 [ 1.687408] cpsw: Detected MACID = d4:94:a1:83:0f:8d [ 1.693420] mmcblk0: mmc0:1234 SA02G 1.83 GiB [ 1.700378] input: gpio-keys as /devices/platform/gpio-keys/input/input2 [ 1.707824] mmcblk0: p1 p2 [ 1.782257] omap_rtc omap_rtc: setting system clock to 2012-07-27 10:34:38 UTC (1343385278) [ 1.795654] net eth0: CPSW phy found : id is : 0x4dd074 [ 1.805725] net eth1: CPSW phy found : id is : 0x4dd074 [ 1.829376] mmc1: card claims to support voltages below the defined range. These will be ignored. [ 1.848480] mmc1: queuing unknown CIS tuple 0x91 (3 bytes) [ 1.855133] mmc1: new SDIO card at address 0001 [ 4.796234] PHY: 0:00 - Link is Up - 100/Full [ 4.825408] Sending DHCP requests ., OK [ 4.845886] IP-Config: Got DHCP answer from 0.0.0.0, my address is 10.5.5.93 [ 4.854003] IP-Config: Complete: [ 4.857421] device=eth0, addr=10.5.5.93, mask=255.255.254.0, gw=10.5.4.254, [ 4.864868] host=10.5.5.93, domain=adsi.aitech.ent, nis-domain=(none), [ 4.872222] bootserver=0.0.0.0, rootserver=10.5.5.86, rootpath= [ 4.885742] VFS: Mounted root (nfs filesystem) on device 0:14. [ 4.892181] Freeing init memory: 248K INIT: version 2.86 booting Please wait: booting... Starting udev [ 6.034301] Disabling lock debugging due to kernel taint [ 7.109588] cfg80211: Calling CRDA to update world regulatory domain [ 7.592041] cfg80211: World regulatory domain updated: [ 7.597930] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp) [ 7.606658] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 7.614929] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm) [ 7.623199] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm) [ 7.631439] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 7.639801] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 8.248504] wl12xx: driver version: ol_R5.00.17 [ 8.253234] wl12xx: compilation time: Thu May 17 05:25:00 2012 [ 8.641998] wl12xx: loaded [ 8.783477] alignment: ignoring faults is unsafe on this CPU. Defaulting to fixup mode. Root filesystem already rw, not remounting Caching udev devnodes ALSA: Restoring mixer settings... No state is present for card EVM Found hardware: "AM335X_EVM" "" "" "" "" Hardware is initialized using a generic method No state is present for card EVM NOT configuring network interfaces: / is an NFS mount INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Hardware abstraction layer hald Starting Dropbear SSH server: dropbear. Starting telnet daemon. Starting network benchmark server: netserver. Starting syslogd/klogd: done Starting thttpd. Starting PVR Starting Lighttpd Web Server: lighttpd. 2012-07-27 10:34:48: (log.c.166) server started [ 12.648132] kjournald starting. Commit interval 5 seconds [ 12.660614] EXT3-fs (mmcblk0p2): using internal journal [ 12.666137] EXT3-fs (mmcblk0p2): recovery complete [ 12.671112] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode / Starting Matrix GUI application. [ 13.418975] gadget: Mass Storage Function, version: 2009/09/11 [ 13.426361] gadget: Number of LUNs=1 [ 13.430206] lun0: LUN: removable file: /dev/mmcblk0p1 [ 13.435607] gadget: Mass Storage Gadget, version: 2009/09/11 [ 13.441619] gadget: userspace failed to provide iSerialNumber [ 13.447723] gadget: g_mass_storage ready [ 13.451904] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 13.457519] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2 [ 13.465332] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 13.472442] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 13.479980] usb usb2: Product: MUSB HDRC host driver [ 13.485137] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd [ 13.490692] usb usb2: SerialNumber: musb-hdrc.0 [ 13.496063] hub 2-0:1.0: USB hub found [ 13.499969] hub 2-0:1.0: 1 port detected [ 13.504119] musb_g_ep0_irq 720: SetupEnd came in a wrong ep0stage setup [ 14.000183] gadget: high-speed config #1: Linux File-Backed Storage *************************************************************** *************************************************************** NOTICE: This file system contains the followin GPLv3 packages: binutils-symlinks binutils gdbserver If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm ttyO0 Arago 2011.09 am335x-evm ttyO0 am335x-evm login: