USB Host mode controller at 47401800 using PIO, IRQ 0 OMAP SD/MMC: 0 reading u-boot.img reading u-boot.img U-Boot 2013.01.01 (Jun 25 2013 - 16:42:52) I2C: ready DRAM: 256 MiB WARNING: Caches not enabled NAND: No NAND device found!!! 0 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - readenv() failed, using default environment musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Peripheral mode controller at 47401000 using PIO, IRQ 0 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Host mode controller at 47401800 using PIO, IRQ 0 Net: not set. Validating first E-fuse MAC cpsw, usb_ether Hit any key to stop autoboot: 0 mmc0 is current device SD/MMC found on device 0 reading uEnv.txt 260 bytes read in 3 ms (84 KiB/s) Loaded environment from uEnv.txt Importing environment from mmc ... Running uenvcmd ... Booting from network... cpsw Waiting for PHY auto negotiation to complete. done link up on port 0, speed 100, full duplex BOOTP broadcast 1 DHCP client bound to address 10.5.5.93 Using cpsw device TFTP from server 10.5.5.86; our IP address is 10.5.5.93 Filename 'uImage-am335x-evm.bin'. Load address: 0x80200000 Loading: ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################# 144.5 KiB/s done Bytes transferred = 3163680 (304620 hex) ## Booting kernel from Legacy Image at 80200000 ... Image Name: Arago/3.2.0-psp04.06.00.08.sdk/a Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3163616 Bytes = 3 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 3.2.0 (jenkins@sdit-build01) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Thu Jul 26 17:16:27 CDT 2012 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES1.0 (sgx neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/nfs nfsroot=10.5.5.86:/home/ngrutman/ti-sdk-am335x-evm-06.00.00.00/targetNFS,nolock rw ip=dhcp [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Memory: 256MB = 256MB total [ 0.000000] Memory: 253256k/253256k available, 8888k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc059d000 (5716 kB) [ 0.000000] .init : 0xc059d000 - 0xc05db000 ( 248 kB) [ 0.000000] .data : 0xc05dc000 - 0xc0644198 ( 417 kB) [ 0.000000] .bss : 0xc06441bc - 0xc0671024 ( 180 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144) [ 0.058532] pid_max: default: 32768 minimum: 301 [ 0.058654] Security Framework initialized [ 0.058776] Mount-cache hash table entries: 512 [ 0.059143] CPU: Testing write buffer coherency: ok [ 0.079071] omap_hwmod: pruss: failed to hardreset [ 0.080139] print_constraints: dummy: [ 0.080505] NET: Registered protocol family 16 [ 0.082611] OMAP GPIO hardware version 0.1 [ 0.085144] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.087341] omap_i2c.1: alias fck already exists [ 0.088226] omap2_mcspi.1: alias fck already exists [ 0.088439] omap2_mcspi.2: alias fck already exists [ 0.089233] edma.0: alias fck already exists [ 0.089233] edma.0: alias fck already exists [ 0.089263] edma.0: alias fck already exists [ 0.115875] bio: create slab at 0 [ 0.118041] SCSI subsystem initialized [ 0.119750] usbcore: registered new interface driver usbfs [ 0.120025] usbcore: registered new interface driver hub [ 0.120239] usbcore: registered new device driver usb [ 0.120391] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3 [ 0.120666] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1 [ 0.138610] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.140502] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.142913] print_constraints: VRTC: [ 0.144348] print_constraints: VIO: at 1500 mV [ 0.146636] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal [ 0.148956] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal [ 0.149963] print_constraints: VDD3: 5000 mV [ 0.151367] print_constraints: VDIG1: at 1800 mV [ 0.152801] print_constraints: VDIG2: at 1800 mV [ 0.154205] print_constraints: VPLL: at 1800 mV [ 0.155639] print_constraints: VDAC: at 1800 mV [ 0.157043] print_constraints: VAUX1: at 1800 mV [ 0.158477] print_constraints: VAUX2: at 3300 mV [ 0.159912] print_constraints: VAUX33: at 3300 mV [ 0.161346] print_constraints: VMMC: at 3300 mV [ 0.161834] tps65910 1-002d: No interrupt support, no core IRQ [ 0.163024] Advanced Linux Sound Architecture Driver Version 1.0.24. [ 0.164184] Switching to clocksource gp timer [ 0.179504] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.179687] musb-hdrc musb-hdrc.0: dma type: pio [ 0.179992] MUSB0 controller's USBSS revision = 4ea20800 [ 0.180541] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using PIO, IRQ 18 [ 0.180694] musb-hdrc musb-hdrc.1: dma type: pio [ 0.180999] MUSB1 controller's USBSS revision = 4ea20800 [ 0.181121] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.181182] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 0.181304] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.181335] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.181335] usb usb1: Product: MUSB HDRC host driver [ 0.181365] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd [ 0.181365] usb usb1: SerialNumber: musb-hdrc.1 [ 0.182128] hub 1-0:1.0: USB hub found [ 0.182159] hub 1-0:1.0: 1 port detected [ 0.182708] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using PIO, IRQ 19 [ 0.183105] NET: Registered protocol family 2 [ 0.183288] IP route cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.183593] TCP established hash table entries: 8192 (order: 4, 65536 bytes) [ 0.183746] TCP bind hash table entries: 8192 (order: 3, 32768 bytes) [ 0.183837] TCP: Hash tables configured (established 8192 bind 8192) [ 0.183868] TCP reno registered [ 0.183868] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.183898] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.184082] NET: Registered protocol family 1 [ 0.184417] RPC: Registered named UNIX socket transport module. [ 0.184417] RPC: Registered udp transport module. [ 0.184448] RPC: Registered tcp transport module. [ 0.184448] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.184692] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.195983] VFS: Disk quotas dquot_6.5.2 [ 0.196044] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.196594] msgmni has been set to 494 [ 0.199676] alg: No test for stdrng (krng) [ 0.200347] io scheduler noop registered [ 0.200378] io scheduler deadline registered [ 0.200439] io scheduler cfq registered (default) [ 0.201599] Could not set LED4 to fully on [ 0.203338] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 0.827239] console [ttyO0] enabled [ 0.831481] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 0.839324] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 0.847137] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 0.854919] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 0.862701] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 0.879760] brd: module loaded [ 0.887817] loop: module loaded [ 0.891265] i2c-core: driver [tsl2550] using legacy suspend method [ 0.897766] i2c-core: driver [tsl2550] using legacy resume method [ 0.904174] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.964721] No daughter card found [ 0.968322] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.983520] Board name: A335X_SK [ 0.986877] Board version: 1.2B [ 0.990142] The board is a AM335x Starter Kit. [ 0.995056] omap_hsmmc.0: alias fck already exists [ 1.000579] omap_hsmmc.1: alias fck already exists [ 1.006591] da8xx_lcdc.0: alias fck already exists [ 1.012054] da8xx_lcdc da8xx_lcdc.0: GLCD: Found NHD-4.3-ATXI#-T-1 panel [ 1.027343] Console: switching to colour frame buffer device 60x34 [ 1.040191] davinci-mcasp.1: alias fck already exists [ 1.046081] Configure Bluetooth Enable pin... [ 1.051544] registered am33xx_sr device [ 1.055816] _regulator_get: 1-0018 supply Vdd not found, using dummy regulator [ 1.063415] _regulator_get: 1-0018 supply Vdd_IO not found, using dummy regulator [ 1.091888] lis3lv02d: 8 bits 3DLH sensor found [ 1.185180] input: ST LIS3LV02DL Accelerometer as /devices/platform/lis3lv02d/input/input0 [ 1.196044] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.203186] omap2-nand driver initializing [ 1.207702] OneNAND driver initializing [ 1.212921] CAN device driver interface [ 1.216949] CAN bus driver for Bosch D_CAN controller 1.0 [ 1.264801] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 1.271240] davinci_mdio davinci_mdio.0: detected phy mask fffffffc [ 1.279510] davinci_mdio.0: probed [ 1.283081] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown [ 1.290466] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown [ 1.298156] usbcore: registered new interface driver zd1201 [ 1.304168] usbcore: registered new interface driver cdc_ether [ 1.310424] usbcore: registered new interface driver cdc_eem [ 1.316497] usbcore: registered new interface driver dm9601 [ 1.322357] cdc_ncm: 04-Aug-2011 [ 1.325897] usbcore: registered new interface driver cdc_ncm [ 1.331817] Initializing USB Mass Storage driver... [ 1.337158] usbcore: registered new interface driver usb-storage [ 1.343414] USB Mass Storage support registered. [ 1.348724] mousedev: PS/2 mouse device common for all mice [ 1.355895] input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input1 [ 1.364349] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 [ 1.371032] omap_rtc: already running [ 1.375030] i2c /dev entries driver [ 1.379089] Linux video capture interface: v2.00 [ 1.384216] usbcore: registered new interface driver uvcvideo [ 1.390228] USB Video Class driver (1.1.1) [ 1.396514] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.405090] cpuidle: using governor ladder [ 1.409851] cpuidle: using governor menu [ 1.418670] omap4_aes_mod_init: loading AM33X AES driver [ 1.424316] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02 [ 1.430877] omap4_aes_probe: probe() done [ 1.435546] omap4_sham_mod_init: loading AM33X SHA/MD5 driver [ 1.441680] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03 [ 1.453155] omap4_sham_probe: probe() done [ 1.463165] usbcore: registered new interface driver usbhid [ 1.469055] usbhid: USB HID core driver [ 1.473693] usbcore: registered new interface driver snd-usb-audio [ 1.485260] _regulator_get: 1-001b supply IOVDD not found, using dummy regulator [ 1.493011] _regulator_get: 1-001b supply DVDD not found, using dummy regulator [ 1.500701] _regulator_get: 1-001b supply AVDD not found, using dummy regulator [ 1.508392] _regulator_get: 1-001b supply DRVDD not found, using dummy regulator [ 1.518829] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok [ 1.526611] ALSA device list: [ 1.529724] #0: AM335X EVM [ 1.532714] oprofile: hardware counters not available [ 1.537994] oprofile: using timer interrupt. [ 1.542480] nf_conntrack version 0.5.0 (3957 buckets, 15828 max) [ 1.549255] ip_tables: (C) 2000-2006 Netfilter Core Team [ 1.554931] TCP cubic registered [ 1.558288] NET: Registered protocol family 17 [ 1.562927] can: controller area network core (rev 20090105 abi 8) [ 1.569488] NET: Registered protocol family 29 [ 1.574127] can: raw protocol (rev 20090105) [ 1.578582] can: broadcast manager protocol (rev 20090105 t) [ 1.584503] Registering the dns_resolver key type [ 1.589508] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 1.597503] ThumbEE CPU extension supported. [ 1.602020] mux: Failed to setup hwmod io irq -22 [ 1.607543] Power Management for AM33XX family [ 1.612396] Trying to load am335x-pm-firmware.bin (60 secs timeout) [ 1.619079] Copied the M3 firmware to UMEM [ 1.623565] smartreflex smartreflex: am33xx_sr_probe: Zero NValue read from EFUSE [ 1.631408] smartreflex: probe of smartreflex failed with error -22 [ 1.638519] sr_init: platform driver register failed [ 1.648651] clock: disabling unused clocks to save power [ 1.667205] mmc0: host does not support reading read-only switch. assuming write-enable. [ 1.676086] Detected MACID=d4:94:a1:83:f:8c [ 1.681488] cpsw: Detected MACID = d4:94:a1:83:0f:8d [ 1.687225] mmc0: new high speed SDHC card at address 15bd [ 1.694671] input: gpio-keys as /devices/platform/gpio-keys/input/input2 [ 1.702301] mmcblk0: mmc0:15bd SD04G 3.69 GiB [ 1.708221] omap_rtc omap_rtc: setting system clock to 2013-06-25 23:09:46 UTC (1372201786) [ 1.717468] mmcblk0: p1 p2 [ 1.725341] net eth0: CPSW phy found : id is : 0x4dd074 [ 1.735412] net eth1: CPSW phy found : id is : 0x4dd074 [ 1.849426] mmc1: card claims to support voltages below the defined range. These will be ignored. [ 1.868560] mmc1: queuing unknown CIS tuple 0x91 (3 bytes) [ 1.875183] mmc1: new SDIO card at address 0001 [ 3.726318] PHY: 0:00 - Link is Up - 100/Full [ 3.765380] Sending DHCP requests ., OK [ 3.785858] IP-Config: Got DHCP answer from 0.0.0.0, my address is 10.5.5.93 [ 3.793945] IP-Config: Complete: [ 3.797363] device=eth0, addr=10.5.5.93, mask=255.255.254.0, gw=10.5.4.254, [ 3.804840] host=10.5.5.93, domain=adsi.aitech.ent, nis-domain=(none), [ 3.812103] bootserver=0.0.0.0, rootserver=10.5.5.86, rootpath= [ 3.826049] VFS: Mounted root (nfs filesystem) on device 0:14. [ 3.832519] Freeing init memory: 248K INIT: version 2.88 booting Starting udev [ 6.630432] wl12xx_sdio: disagrees about version of symbol module_layout [ 6.637573] wl12xx_sdio: disagrees about version of symbol module_layout [ 7.410217] wl12xx_sdio: disagrees about version of symbol module_layout [ 7.439331] wl12xx_sdio: disagrees about version of symbol module_layout [ 8.431396] kjournald starting. Commit interval 5 seconds [ 8.689575] EXT3-fs (mmcblk0p2): using internal journal [ 8.695037] EXT3-fs (mmcblk0p2): recovery complete [ 8.700073] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory bootlogd. ALSA: Restoring mixer settings... No state is present for card EVM Found hardware: "AM335X_EVM" "" "" "" "" Hardware is initialized using a generic method No state is present for card EVM NOT configuring network interfaces: / is an NFS mount INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Dropbear SSH server: dropbear. Starting telnet daemon. Performing wifi calibration... rm: can't remove '/lib/firmware/ti-connectivity/wl1271-nvs.bin': No such file or directory Error: Module wl12xx_sdio is not currently loaded nl80211 not found. [ 10.250244] wl12xx_sdio: disagrees about version of symbol module_layout ERROR: could not insert 'wl12xx_sdio': Exec format error Starting network benchmark server: netserver. Starting syslogd/klogd: done Starting thttpd. Starting PVR [ 10.961273] pvrsrvkm: disagrees about version of symbol module_layout Error: could not insert module /lib/modules/3.2.0/kernel/drivers/gpu/pvr/pvrsrvkm.ko: Invalid module format Could not find pvrsrvkm driver Starting Lighttpd Web Server: lighttpd. 2013-06-25 23:09:54: (log.c.166) server started / Starting Matrix GUI application. [ 11.920501] g_mass_storage: disagrees about version of symbol module_layout ERROR: could not insert 'g_mass_storage': Exec format error *************************************************************** *************************************************************** NOTICE: This file system contains the followin GPLv3 packages: binutils-symlinks binutils gdbserver If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** Stopping Bootlog daemon: bootlogd. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm ttyO0 Arago 2013.05 am335x-evm ttyO0 am335x-evm login: