U-Boot SPL 2021.01-00002-g27f28e9f8f-dirty (Oct 04 2023 - 05:16:39 -0700) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') SPL initial stack usage: 13424 bytes Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Loading Environment from MMC... *** Warning - No MMC card found, using default environment Starting ATF on ARM64 core... NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty NOTICE: BL31: Built : 05:06:58, Feb 24 2023 U-Boot SPL 2021.01-00002-g27f28e9f8f-dirty (Oct 04 2023 - 05:16:21 -0700) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') Trying to boot from MMC2 U-Boot 2021.01-00002-g27f28e9f8f-dirty (Oct 04 2023 - 05:16:21 -0700) SoC: AM62X SR1.0 GP Model: Coda Octopus Dive - Voice Processor 29/09/2023 12:45PM EEPROM not available at 0x50, trying to read at 0x51 Reading on-board EEPROM at 0x51 failed 1 DRAM: 2 GiB MMC: mmc@fa10000: 0, mmc@fa00000: 1, mmc@fa20000: 2 Loading Environment from MMC... *** Warning - bad CRC, using default environment In: serial@2800000 Out: serial@2800000 Err: serial@2800000 EEPROM not available at 0x50, trying to read at 0x51 Reading on-board EEPROM at 0x51 failed 1 Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 2  1  0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 1490 bytes read in 2 ms (727.5 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... 1 bytes read in 3 ms (0 Bytes/s) Already setup. 19147264 bytes read in 786 ms (23.2 MiB/s) 45070 bytes read in 5 ms (8.6 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 000000008fef1000, end 000000008fffffff ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.10.168-g2c23e6c538 (root@ubuntu) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #18 SMP PREEMPT Wed Oct 4 07:04:23 PDT 2023 [ 0.000000] Machine model: Coda Octopus Dive - Voice Processor 03/10/2023 10:30 AM [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB [ 0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB [ 0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009c7fffff] [ 0.000000] node 0: [mem 0x000000009c800000-0x000000009e6fffff] [ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e77ffff] [ 0.000000] node 0: [mem 0x000000009e780000-0x000000009fffffff] [ 0.000000] node 0: [mem 0x00000000a0000000-0x00000000ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] cma: Reserved 512 MiB at 0x00000000dd000000 [ 0.000000] psci: PSCI -> Starting [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: set_conduit -> SMCCC_CONDUIT_SMC [ 0.000000] psci: PSCI -> smc method property [ 0.000000] psci: psci_probe -> Reading PSCI Version... [ 0.000000] psci: psci_get_version -> reading version from 0x84000000 [ 0.000000] psci: PSCI -> ARM SMC