# This uEnv.txt file can contain additional environment settings that you # want to set in U-Boot at boot time. This can be simple variables such # as the serverip or custom variables. The format of this file is: # variable=value # NOTE: This file will be evaluated after the bootcmd is run and the # bootcmd must be set to load this file if it exists (this is the # default on all newer U-Boot images. This also means that some # variables such as bootdelay cannot be changed by this file since # it is not evaluated until the bootcmd is run. # Update the Linux hostname based on board_name # The SK also requires an additional dtbo to boot. Prepend it to name_overlays depending on board_name uenvcmd=if test "$board_name" = "am67-sk"; then ; setenv args_all $args_all systemd.hostname=am67a-sk ; setenv name_overlays k3-am67-sk-som-ddr-mem-carveout.dtbo $name_overlays; fi # Setting the right U-Boot environment variables dorprocboot=1 name_overlays=k3-j722s-vision-apps.dtbo