U-Boot SPL 2019.01-gc14892445a-dirty (May 06 2021 - 09:25:37 +0200) Trying to boot from MMC1 U-Boot 2019.01-gc14892445a-dirty (May 06 2021 - 09:25:37 +0200) CPU : AM335X-GP rev 2.1 Model: TI AM335x Gateway4 DRAM: 512 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Loading Environment from FAT... *** Warning - bad CRC, using default environment not set. Validating first E-fuse MAC Net: eth0: ethernet@4a100000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 ** Unable to read file boot.scr ** ** Unable to read file uEnv.txt ** switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 4280832 bytes read in 363 ms (11.2 MiB/s) 34436 bytes read in 4 ms (8.2 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 87ff4000, end 87fff683 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.19.94-gbe5389fd85 (oe-user@oe-host) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 PREEMPT Sun Apr 19 03:43:09 UTC 2020 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: TI AM335x GATEWAY4 [ 0.000000] Memory policy: Data cache writeback [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 48 MiB at 0x9d000000 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (neon) [ 0.000000] random: get_random_bytes called from start_kernel+0xa4/0x434 with crng_init=0 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129920 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=998f0e4d-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 455964K/524288K available (9216K kernel code, 307K rwdata, 2720K rodata, 1024K init, 252K bss, 19172K reserved, 49152K cma-reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (10208 kB) [ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (1024 kB) [ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 308 kB) [ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) ( 253 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] Tasks RCU enabled. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000021] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns [ 0.000048] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns [ 0.000064] OMAP clocksource: timer1 at 24000000 Hz [ 0.000288] timer_probe: no matching timers found [ 0.000531] Console: colour dummy device 80x30 [ 0.000568] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0' [ 0.000577] This ensures that you still see kernel messages. Please [ 0.000585] update your kernel commandline. [ 0.000656] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032) [ 0.118727] pid_max: default: 32768 minimum: 301 [ 0.119009] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.119029] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.120137] CPU: Testing write buffer coherency: ok [ 0.120224] CPU0: Spectre v2: using BPIALL workaround [ 0.121398] Setting up static identity map for 0x80100000 - 0x80100060 [ 0.121608] rcu: Hierarchical SRCU implementation. [ 0.122083] EFI services will not be available. [ 0.124048] devtmpfs: initialized [ 0.135019] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.135555] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.135589] futex hash table entries: 256 (order: -1, 3072 bytes) [ 0.140596] pinctrl core: initialized pinctrl subsystem [ 0.141605] DMI not present or invalid. [ 0.142166] NET: Registered protocol family 16 [ 0.145389] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.175735] l4_wkup_cm:clk:0010:0: failed to disable [ 0.231093] cpuidle: using governor ladder [ 0.231147] cpuidle: using governor menu [ 0.238247] OMAP GPIO hardware version 0.1 [ 0.250486] No ATAGs? [ 0.250503] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.270620] edma 49000000.edma: TI EDMA DMA engine driver [ 0.274754] SCSI subsystem initialized [ 0.275381] media: Linux media interface: v0.10 [ 0.275448] videodev: Linux video capture interface: v2.00 [ 0.275589] pps_core: LinuxPPS API ver. 1 registered [ 0.275602] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.275636] PTP clock support registered [ 0.275686] EDAC MC: Ver: 3.0.0 [ 0.277153] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.277923] Advanced Linux Sound Architecture Driver Initialized. [ 0.279843] clocksource: Switched to clocksource timer1 [ 0.291900] NET: Registered protocol family 2 [ 0.293022] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes) [ 0.293074] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 0.293139] TCP bind hash table entries: 4096 (order: 2, 16384 bytes) [ 0.293201] TCP: Hash tables configured (established 4096 bind 4096) [ 0.293343] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.293373] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.293582] NET: Registered protocol family 1 [ 0.294370] RPC: Registered named UNIX socket transport module. [ 0.294390] RPC: Registered udp transport module. [ 0.294399] RPC: Registered tcp transport module. [ 0.294409] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.295638] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 0.297355] Initialise system trusted keyrings [ 0.297784] workingset: timestamp_bits=14 max_order=17 bucket_order=3 [ 0.304867] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.305903] NFS: Registering the id_resolver key type [ 0.305962] Key type id_resolver registered [ 0.305974] Key type id_legacy registered [ 0.306035] ntfs: driver 2.1.32 [Flags: R/O]. [ 0.309261] Key type asymmetric registered [ 0.309285] Asymmetric key parser 'x509' registered [ 0.309381] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.309400] io scheduler noop registered [ 0.309411] io scheduler deadline registered [ 0.309754] io scheduler cfq registered (default) [ 0.309771] io scheduler mq-deadline registered [ 0.309783] io scheduler kyber registered [ 0.312373] pinctrl-single 44e10800.pinmux: 142 pins, size 568 [ 0.385664] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.391314] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250 [ 1.009457] console [ttyS0] enabled [ 1.015643] omap_rng 48310000.rng: Random Number Generator ver. 20 [ 1.022082] random: fast init done [ 1.025765] random: crng init done [ 1.047086] brd: module loaded [ 1.059681] loop: module loaded [ 1.068173] libphy: Fixed MDIO Bus: probed [ 1.149934] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000 [ 1.157645] davinci_mdio 4a101000.mdio: detected phy mask fffffffd [ 1.165158] libphy: 4a101000.mdio: probed [ 1.169216] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver unknown [ 1.178592] cpsw 4a100000.ethernet: Detected MACID = 14:42:fc:bb:02:83 [ 1.185522] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4 [ 1.192041] cpsw 4a100000.ethernet: ALE Table size 1024 [ 1.197341] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies) [ 1.206532] i2c /dev entries driver [ 1.212824] cpuidle: enable-method property 'ti,am3352' found operations [ 1.220335] sdhci: Secure Digital Host Controller Interface driver [ 1.226557] sdhci: Copyright(c) Pierre Ossman [ 1.232036] omap_gpio 481ae000.gpio: Could not set line 14 debounce to 200000 microseconds (-22) [ 1.240986] omap_hsmmc 48060000.mmc: Got CD GPIO [ 1.246315] omap_hsmmc 48060000.mmc: Linked as a consumer to regulator.1 [ 1.280575] omap_hsmmc 481d8000.mmc: Linked as a consumer to regulator.1 [ 1.313209] sdhci-pltfm: SDHCI platform and OF driver helper [ 1.321749] ledtrig-cpu: registered to indicate activity on CPUs [ 1.327908] mmc0: host does not support reading read-only switch, assuming write-enable [ 1.342410] NET: Registered protocol family 10 [ 1.348992] mmc0: new high speed SDHC card at address 1234 [ 1.354870] Segment Routing with IPv6 [ 1.358674] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 1.366213] mmcblk0: mmc0:1234 SA16G 14.5 GiB [ 1.372351] NET: Registered protocol family 17 [ 1.377222] Key type dns_resolver registered [ 1.383090] omap_voltage_late_init: Voltage driver support not added [ 1.389743] mmcblk0: p1 p2 [ 1.395451] Loading compiled-in X.509 certificates [ 1.406332] mmc1: new high speed MMC card at address 0001 [ 1.421744] mmcblk1: mmc1:0001 004GA0 3.69 GiB [ 1.426979] mmcblk1boot0: mmc1:0001 004GA0 partition 1 2.00 MiB [ 1.435406] mmcblk1boot1: mmc1:0001 004GA0 partition 2 2.00 MiB [ 1.441779] mmcblk1rpmb: mmc1:0001 004GA0 partition 3 512 KiB, chardev (244:0) [ 1.450828] mmcblk1: p1 p2 [ 1.469810] tps65217 0-0024: TPS65217 ID 0xe version 1.2 [ 1.475868] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 1.482335] cpu cpu0: Linked as a consumer to regulator.3 [ 1.487866] cpu cpu0: Dropping the link to regulator.3 [ 1.493544] cpu cpu0: Linked as a consumer to regulator.3 [ 1.500831] hctosys: unable to open rtc device (rtc0) [ 1.506627] ALSA device list: [ 1.509618] No soundcards found. [ 8.992650] EXT4-fs (mmcblk0p2): recovery complete [ 9.000526] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 9.009439] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 9.025619] devtmpfs: mounted [ 9.030041] Freeing unused kernel memory: 1024K [ 9.035024] Run /sbin/init as init process [ 9.400614] systemd[1]: System time before build time, advancing clock. [ 9.453059] systemd[1]: systemd 239 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 9.475344] systemd[1]: Detected architecture arm. Welcome to Arago 2019.11! [ 9.534216] systemd[1]: Set hostname to . [ 9.859632] systemd[1]: File /lib/systemd/system/systemd-journald.service:36 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling. [ 9.877077] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.) [ 10.278876] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ 10.324400] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ 10.360578] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. [ 10.390941] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password Requests to Console Directory Watch. [ 10.431582] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password Requests to Wall Directory Watch. [ OK ] Reached target Paths. [ OK ] Listening on Process Core Dump Socket. [ OK ] Listening on Journal Socket. [ OK ] Started Hardware RNG Entropy Gatherer Daemon. Mounting Kernel Debug File System... Starting Load Kernel Modules... Mounting POSIX Message Queue File System... [ OK ] Listening on udev Kernel Socket. [ 10.784437] cryptodev: loading out-of-tree module taints kernel. [ 10.794066] cryptodev: driver 1.9 loaded. [ OK ] Created slice User and Session Slice. [ OK ] Reached target Slices. [ 10.843923] usbcore: registered new interface driver usbfs [ 10.849533] usbcore: registered new interface driver hub [ 10.855590] usbcore: registered new device driver usb [ OK ] Listening on udev Control Socket. [ 10.886858] usbcore: registered new interface driver ftdi_sio [ 10.900501] usbserial: USB Serial support registered for FTDI USB Serial Device Starting udev Coldplug all Devices... [ OK ] Listening on Network Service Netlink Socket. [ OK ] Listening on Journal Socket (/dev/log). Starting Journal Service... Starting Remount Root and Kernel File Systems... [ OK ] Created slice system-getty.slice. [ OK ] Reached target Swap. [ 11.166150] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) Mounting Temporary Directory (/tmp)... [ OK ] Mounted Kernel Debug File System. [ OK ] Started Load Kernel Modules. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Started Remount Root and Kernel File Systems. [ OK ] Started Journal Service. [ OK ] Mounted Temporary Directory (/tmp). Starting Flush Journal to Persistent Storage... Starting Create Static Device Nodes in /dev... Starting Apply Kernel Variables... Mounting Kernel Configuration File System... [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Started Apply Kernel Variables. [ OK ] Mounted Kernel Configuration File System. [ 11.830925] systemd-journald[76]: Received request to flush runtime journal from PID 1 [ OK ] Reached target Local File Systems (Pre). Mounting /media/ram... [ OK ] Reached target Containers. Mounting /var/volatile... Starting udev Kernel Device Manager... [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Mounted /media/ram. [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started udev Kernel Device Manager. [ OK ] Started Load/Save Random Seed. [ OK ] Started Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Network Service... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started Update UTMP about System Boot/Shutdown. [ OK ] Started Network Service. Starting Network Name Resolution... [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Time Synchronized. [ OK ] Started udev Coldplug all Devices. [ OK ] Reached target System Initialization. [ OK ] Listening on D-Bus System Message Bus Socket. Starting Reboot and dump vmcore via kexec... [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on RPCbind Server Activation Socket. [ OK ] Started Daily rotation of log files. [ OK ] Listening on dropbear.socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ 14.406909] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ OK ] Started D-Bus System Message Bus. [ 14.545545] omap_rtc 44e3e000.rtc: registered as rtc0 [ 14.782263] at24 0-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write [ OK ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf. Starting Print notice about GPLv3 packages... [ OK ] Started Job spooling tools. [ OK ] Started Periodic Command Scheduler. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Timers. Starting RPC Bind Service... Starting Login Service... [ OK ] Started Network Name Resolution. [ OK ] Started Reboot and dump vmcore via kexec. [ OK ] Found device /dev/ttyS0. [ OK ] Reached target Network. Starting Lightning Fast Webserver With Light System Requirements... [ 15.899143] omap-sham 53100000.sham: hw accel on OMAP rev 4.3 [ 15.962099] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2 Starting Simple Network Management Protocol (SNMP) Daemon.... [ 16.037178] remoteproc remoteproc0: wkup_m3 is available [ OK ] Started Redis In-Memory Data Store. [ 16.190280] omap-aes 53500000.aes: will run requests pump with realtime priority Starting Permit User Sessions... [ 16.335732] omap_hwmod: gfx: failed to hardreset Starting Avahi mDNS/DNS-SD Stack... [ OK ] Reached target Host and Network Name Lookups. [ OK ] Started RPC Bind Service. [ 16.761596] pvrsrvkm 56000000.sgx: Unable to reset SGX! [ OK ] Started Lightning Fast Webserver With Light System Requirements. [ 16.802843] remoteproc remoteproc0: powering up wkup_m3 [ 16.824054] PM: Cannot get wkup_m3_ipc handle [ 16.948615] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.sgx on minor 0 [ 16.966877] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 242888 [ OK ] Started Permit User Sessions. [ 17.109391] PM: Cannot get wkup_m3_ipc handle [ 17.126151] remoteproc remoteproc0: remote processor wkup_m3 is now up [ 17.126176] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192 [ OK ] Started Serial Getty on ttyS0. [ 17.311536] NET: Registered protocol family 15 [ OK ] Started Getty on tty1. [ OK ] Started NFS status monitor for NFSv2/3 locking.. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ 18.597658] net eth0: initializing cpsw version 1.12 (0) [ 18.652851] PM: bootloader does not support rtc-only! [ 18.709983] Generic PHY 4a101000.mdio:01: attached PHY driver [Generic PHY] (mii_bus:phy_addr=4a101000.mdio:01, irq=POLL) [ OK ] Found device /dev/ttyS3. [ 19.016359] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ 19.234537] Initializing XFRM netlink socket _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org Gateway4 ttyS0 Arago 2019.11 Gateway4 ttyS0 Gateway4 login: root *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: autoconf bash-dev bash bc binutils cifs-utils cpio cpp-symlinks cpp dosfstools elfutils findutils g++-symlinks g++ gawk gcc-symlinks gcc gdb gdbserver gettext glmark2 gstreamer1.0-libav gzip hidapi libbfd libcairo-perf-utils libdw1 libelf1 libgdbm-compat4 libgdbm-dev libgdbm6 libgettextlib libgettextsrc libgmp10 libidn2-0 libmavconn libmpc3 libmpfr6 libreadline-dev libreadline7 libunistring2 m4-dev m4 make mavlink mavros-extras mavros-msgs mavros nettle pdm-anomaly-detection socketcan-interface swig-dev swig which If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** [ 35.293419] EXT4-fs (mmcblk1p2): mounting ext3 file system using the ext4 subsystem [ 35.368195] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null) root@Gateway4:~# rtcwake -m standby -s 5 rtcwake: assuming RTC uses UTC ... rtcwake: wakeup from "standby" using /dev/rtc0 at Sat Jan 1 00:00:06 2000 [ 45.393436] PM: suspend entry (shallow) [ 45.397359] PM: Syncing filesystems ... done. [ 45.420537] Freezing user space processes ... (elapsed 0.002 seconds) done. [ 45.430558] OOM killer disabled. [ 45.433863] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done. [ 45.443351] Suspending console(s) (use no_console_suspend to debug) [ 45.473969] pm33xx pm33xx: PM: Successfully put all powerdomains to target state [ 45.473969] PM: Wakeup source UART [ 45.496450] net eth0: initializing cpsw version 1.12 (0) [ 45.500234] Generic PHY 4a101000.mdio:01: attached PHY driver [Generic PHY] (mii_bus:phy_addr=4a101000.mdio:01, irq=POLL) [ 45.539894] OOM killer enabled. [ 45.543058] Restarting tasks ... done. [ 45.589085] PM: suspend exit root@Gateway4:~#