ti-i2c initialized....board detected..............>>>>>>>>>>>>>>>>>>>>>> Timed out in wait_for_event: status=0000 �!�������������������������������ɑ�detected..............>>>>>>>>>>>>>>>>************>>>>>>>>>>>>>>>>>>>>>> U-Boot SPL 2018.01-gc14892445a-dirty (Jun 03 2024 - 20:53:45) Trying to boot from NAND U-Boot 2018.01-gc14892445a-dirty (Jun 03 2024 - 20:53:45 +0530) CPU : AM335X-GP rev 2.1 Model: TI AM3359 ICE-V2 DRAM: 512 MiB NAND: 512 MiB MMC: Net: ********************UBOOT MSCC.C vsc8531_config function************************* >>>>>>>>>>>>>>>>>>>>>> init_b <<<<<<<<<<<<<<<<<<< u-boot <<<<<<<<<<<<<<<<<< mscc.c <<<<<<<<<<<<<<<<<< ********************UBOOT MSCC.C vsc8531_MAC_config function************************* *****U-BOOT MSCC.C vsc8531_config_init function***** 31 cpsw, usb_ether Hit any key to stop autoboot: 0 Booting from nand ... NAND read: device 0 offset 0x80000, size 0x40000 262144 bytes read: OK NAND read: device 0 offset 0x200000, size 0x1000000 16777216 bytes read: OK ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8fff3000, end 8ffff49e ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.19.94 (root@rd07) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))4 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: TI AM3359 ICE-V2 [ 0.000000] Memory policy: Data cache writeback [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 48 MiB at 0x9d000000 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (sgx neon) [ 0.000000] random: get_random_bytes called from start_kernel+0xa4/0x434 with crng_init=0 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129920 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048 rootfstype=ubifs rootwait=1 [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 452876K/524288K available (9216K kernel code, 308K rwdata, 2724K rodata, 4096K init, 252K bss, 22260K reserved, 49152K) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (10208 kB) [ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (4096 kB) [ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 309 kB) [ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) ( 253 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] Tasks RCU enabled. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts [ 0.000000] OMAP clockevent source: timer2 at 25000000 Hz [ 0.000018] sched_clock: 32 bits at 25MHz, resolution 40ns, wraps every 85899345900ns [ 0.000041] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 76450417870 ns [ 0.000054] OMAP clocksource: timer1 at 25000000 Hz [ 0.000240] timer_probe: no matching timers found [ 0.000441] Console: colour dummy device 80x30 [ 0.000472] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0' [ 0.000479] This ensures that you still see kernel messages. Please [ 0.000486] update your kernel commandline. [ 0.000546] Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216) [ 0.089030] pid_max: default: 32768 minimum: 301 [ 0.089252] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.089267] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.090164] CPU: Testing write buffer coherency: ok [ 0.090236] CPU0: Spectre v2: using BPIALL workaround [ 0.091188] Setting up static identity map for 0x80100000 - 0x80100060 [ 0.091352] rcu: Hierarchical SRCU implementation. [ 0.091728] EFI services will not be available. [ 0.093250] devtmpfs: initialized [ 0.101961] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.102394] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.102420] futex hash table entries: 256 (order: -1, 3072 bytes) [ 0.106550] pinctrl core: initialized pinctrl subsystem [ 0.107423] DMI not present or invalid. [ 0.107903] NET: Registered protocol family 16 [ 0.110610] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.136522] l4_wkup_cm:clk:0010:0: failed to disable [ 0.189546] cpuidle: using governor ladder [ 0.189588] cpuidle: using governor menu [ 0.195211] OMAP GPIO hardware version 0.1 [ 0.204444] No ATAGs? [ 0.204457] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.219985] edma 49000000.edma: TI EDMA DMA engine driver [ 0.223325] SCSI subsystem initialized [ 0.223838] media: Linux media interface: v0.10 [ 0.223897] videodev: Linux video capture interface: v2.00 [ 0.224000] pps_core: LinuxPPS API ver. 1 registered [ 0.224010] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.224036] PTP clock support registered [ 0.224074] EDAC MC: Ver: 3.0.0 [ 0.225288] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.225927] Advanced Linux Sound Architecture Driver Initialized. [ 0.227252] clocksource: Switched to clocksource timer1 [ 0.236563] NET: Registered protocol family 2 [ 0.237575] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes) [ 0.237615] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 0.237664] TCP bind hash table entries: 4096 (order: 2, 16384 bytes) [ 0.237711] TCP: Hash tables configured (established 4096 bind 4096) [ 0.237827] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.237850] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.238015] NET: Registered protocol family 1 [ 0.238679] RPC: Registered named UNIX socket transport module. [ 0.238694] RPC: Registered udp transport module. [ 0.238702] RPC: Registered tcp transport module. [ 0.238709] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.502954] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 0.504471] Initialise system trusted keyrings [ 0.504809] workingset: timestamp_bits=14 max_order=17 bucket_order=3 [ 0.510224] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.511045] NFS: Registering the id_resolver key type [ 0.511094] Key type id_resolver registered [ 0.511104] Key type id_legacy registered [ 0.511159] ntfs: driver 2.1.32 [Flags: R/O]. [ 0.513684] Key type asymmetric registered [ 0.513705] Asymmetric key parser 'x509' registered [ 0.513785] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.513800] io scheduler noop registered [ 0.513809] io scheduler deadline registered [ 0.514069] io scheduler cfq registered (default) [ 0.514082] io scheduler mq-deadline registered [ 0.514091] io scheduler kyber registered [ 0.515978] pinctrl-single 44e10800.pinmux: 142 pins, size 568 [ 0.515999] pinctrl-single 44e10800.pinmux: <<<<<<<<<<<<<<<<<<<<<<<< Added VSC8531 RESET >>>>>>>>>>>>>>>>>>>>>>>>> [ 0.682097] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.686387] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250 [ 1.315486] console [ttyS0] enabled [ 1.320326] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 31, base_baud = 3000000) is a 8250 [ 1.330367] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 32, base_baud = 3000000) is a 8250 [ 1.341283] omap_rng 48310000.rng: Random Number Generator ver. 20 [ 1.347736] random: fast init done [ 1.351388] random: crng init done [ 1.369031] brd: module loaded [ 1.379689] loop: module loaded [ 1.384431] <<<<<<<<<<<<<<<<<<<<***************SPI Slave Intialized>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>> [ 1.399777] <<<<<<<<<<<<<<<<<<<<***************SPI Slave Intialized>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>> [ 1.414709] libphy: Fixed MDIO Bus: probed [ 1.487342] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000 [ 1.495054] libphy: 4a101000.mdio: probed [ 1.509421] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver Microsemi VSC8531 [ 1.518510] davinci_mdio 4a101000.mdio: phy[3]: device 4a101000.mdio:03, driver Microsemi VSC8531 [ 1.528685] cpsw 4a100000.ethernet: Detected MACID = 14:7f:0f:e5:26:ec [ 1.535395] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4 [ 1.541927] cpsw 4a100000.ethernet: ALE Table size 1024 [ 1.547220] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies) [ 1.555402] cpsw 4a100000.ethernet: cpsw: Detected MACID = 14:7f:0f:e5:26:ee [ 1.563866] >>>>>>>>>>>>>>>>>>>>>Entered into spi_nor_read_id function_1<<<<<<<<<<<<<<<<<<<<<<< [ 1.564136] >>>>>>>>>>>>>>>>>>>>>Entered into spi_nor_read_id function_5<<<<<<<<<<<<<<<<<<<<<<< [ 1.572927] >>>>>>>>>>>>>>>>>>>Temp Value is >>>>>>>>>>>>>>>>>>>. 0 [ 1.587979] >>>>>>>>>>>>>>>>>>>Info Value is >>>>>>>>>>>>>>>>>>>. 5 [ 1.594271] >>>>>>>>>>>>>>>>>>>>>Entered into spi_nor_read_id function_3<<<<<<<<<<<<<<<<<<<<<<< [ 1.594287] m25p80_SBR-GCM spi1.0: unrecognized JEDEC id bytes: ff, ff, ff, ff, ff, ff, 0 [ 1.611545] m25p80_SBR-GCM spi1.0: n25q256a (32768 Kbytes) [ 1.617091] 1 fixed-partitions partitions found on MTD device spi1.0 [ 1.623499] Creating 1 MTD partitions on "spi1.0": [ 1.628336] 0x000000000000-0x000002000000 : "spi1_partition_SBR-GCM" [ 1.637694] i2c /dev entries driver [ 1.643708] cpuidle: enable-method property 'ti,am3352' found operations [ 1.651023] sdhci: Secure Digital Host Controller Interface driver [ 1.657366] sdhci: Copyright(c) Pierre Ossman [ 1.662238] sdhci-pltfm: SDHCI platform and OF driver helper [ 1.668566] ledtrig-cpu: registered to indicate activity on CPUs [ 1.679303] NET: Registered protocol family 10 [ 1.685336] Segment Routing with IPv6 [ 1.689312] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 1.696043] NET: Registered protocol family 17 [ 1.700952] Key type dns_resolver registered [ 1.705523] omap_voltage_late_init: Voltage driver support not added [ 1.713036] Loading compiled-in X.509 certificates [ 1.729868] omap-gpmc 50000000.gpmc: GPMC revision 6.0 [ 1.735051] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000 [ 1.742966] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xdc [ 1.749498] nand: Micron MT29F4G08ABADAWP [ 1.753529] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64 [ 1.761245] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme [ 1.766747] 10 fixed-partitions partitions found on MTD device omap2-nand.0 [ 1.773776] Creating 10 MTD partitions on "omap2-nand.0": [ 1.779230] 0x000000000000-0x000000020000 : "NAND.SPL" [ 1.785618] 0x000000020000-0x000000040000 : "NAND.SPL.backup1" [ 1.792559] 0x000000040000-0x000000060000 : "NAND.SPL.backup2" [ 1.799440] 0x000000060000-0x000000080000 : "NAND.SPL.backup3" [ 1.806245] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os" [ 1.813386] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot" [ 1.820220] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env" [ 1.826897] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1" [ 1.834398] 0x000000200000-0x000001200000 : "NAND.kernel" [ 1.848273] 0x000000e00000-0x000002000000 : "NAND.file-system" [ 1.863657] gpmc_read_settings_dt: page/burst-length set but not used! [ 2.887319] omap_i2c 44e0b000.i2c: timeout waiting for bus ready [ 2.893675] tps65910 0-002d: No interrupt support, no core IRQ [ 3.917310] omap_i2c 44e0b000.i2c: timeout waiting for bus ready [ 3.923470] tps65910-pmic: probe of tps65910-pmic failed with error -16 [ 3.931362] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 3.939201] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 500 kHz [ 3.945311] ubi0: attaching mtd10 [ 4.004448] ubi0: scanning is finished [ 4.008342] ubi0 error: ubi_read_volume_table: the layout volume was not found [ 4.015812] ubi0 error: ubi_attach_mtd_dev: failed to attach mtd10, error -22 [ 4.023068] UBI error: cannot attach mtd10 [ 4.027690] hctosys: unable to open rtc device (rtc0) [ 4.033372] ALSA device list: [ 4.036360] No soundcards found. [ 4.039931] Warning: unable to open an initial console. [ 4.050814] Freeing unused kernel memory: 4096K [ 4.055910] Run /init as init process [ 5.827464] net eth0: initializing cpsw version 1.12 (0) [ 5.927297] [ 5.927297] ****************** *KERNEL MSCC.C vsc85xx_config_init function************************* [ 5.938689] [ 5.938689] *****KERNEL MSCC.C vsc85xx_default_config function_Before*****=31 [ 5.947837] [ 5.947837] *****KERNEL MSCC.C vsc85xx_default_config function*****=31 [ 6.049877] Microsemi VSC8531 4a101000.mdio:00: attached PHY driver [Microsemi VSC8531] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL) [ 6.067359] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm /dev/ttyS0 Arago 2020.09 am335x-evm /dev/ttyS0 am335x-evm login: _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm /dev/ttyS0 Arago 2020.09 am335x-evm /dev/ttyS0 am335x-evm login: _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm /dev/ttyS0 Arago 2020.09 am335x-evm /dev/ttyS0 am335x-evm login: root root@am335x-evm:~# root@am335x-evm:~# root@am335x-evm:~# root@am335x-evm:~# root@am335x-evm:~# root@am335x-evm:~# [ 34.407353] vbat: disabling root@am335x-evm:~# root@am335x-evm:~# root@am335x-evm:~# root@am335x-evm:~# ^C root@am335x-evm:~# CTRL-A Z for help | 115200 8N1 | NOR | Minicom 2.8 | VT102 | Offline | ttyUSB0