U-Boot SPL 2023.04-gc1c2bdf272 (Nov 30 2023 - 18:17:44 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') Reading on-board EEPROM at 0x50 failed -1 SPL initial stack usage: 1424 bytes Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Starting ATF on ARM64 core... NOTICE: BL31: v2.9(release):v2.9.0-614-gd7a7135d32-dirty NOTICE: BL31: Built : 09:34:15, Aug 24 2023 I/TC: I/TC: OP-TEE version: 4.0.0 (gcc version 11.4.0 (GCC)) #1 Fri Oct 20 18:29:31 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Fixing SA2UL firewall owner for GP device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2023.04-gc1c2bdf272 (Nov 30 2023 - 18:17:44 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') i2c_omap i2c@42120000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19 Reading on-board EEPROM at 0x50 failed -1 Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted U-Boot 2023.04-gc1c2bdf272 (Nov 30 2023 - 18:17:44 +0000) SoC: AM65X SR2.0 GP Model: Texas Instruments AM654 Base Board i2c_omap i2c@42120000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19 Reading on-board EEPROM at 0x50 failed -1 Board: AM6-COMPROCEVM rev E3 DRAM: 4 GiB Core: 119 devices, 31 uclasses, devicetree: separate MMC: mmc@4f80000: 0, mmc@4fa0000: 1 Loading Environment from nowhere... OK In: serial Out: serial Err: serial am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00102 cpsw_ver: 0x6BA80102 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000 Reading on-board EEPROM at 0x50 failed -1 i2c_write: error waiting for data ACK (status=0x116) pca953x gpio@38: Error reading output register i2c_write: error waiting for data ACK (status=0x116) pca953x gpio@39: Error reading output register i2c_write: error waiting for data ACK (status=0x116) pca953x gpio@21: Error reading output register Net: eth0: ethernet@46000000port@1 Hit any key to stop autoboot: 0 i2c_write: error waiting for data ACK (status=0x116) pca953x gpio@39: Error reading output register switch to partitions #0, OK mmc1 is current device i2c_write: error waiting for data ACK (status=0x116) pca953x gpio@39: Error reading output register SD/MMC found on device 1 Failed to load 'boot.scr' 1223 bytes read in 30 ms (39.1 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... 1 bytes read in 29 ms (0 Bytes/s) Already setup. ## Error: "main_cpsw0_qsgmii_phyinit" not defined 19241472 bytes read in 829 ms (22.1 MiB/s) 67088 bytes read in 33 ms (1.9 MiB/s) Working FDT set to 88000000 ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000 Loading Device Tree to 000000008feec000, end 000000008fffffff ... OK Working FDT set to 8feec000 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 6.1.46-rt13-gb4f1767f9e (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT_RT Thu Nov 30 22:21:00 UTC 2023 [ 0.000000] Machine model: Texas Instruments AM654 Base Board [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff] [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a20fffff] [ 0.000000] node 0: [mem 0x00000000a2100000-0x00000000ffffffff] [ 0.000000] node 0: [mem 0x0000000880000000-0x00000008ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff] [ 0.000000] cma: Reserved 32 MiB at 0x00000000fe000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.4 [ 0.000000] percpu: Embedded 19 pages/cpu s37696 r8192 d31936 u77824 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] alternatives: applying boot alternatives [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1032192 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=59d14097-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear) [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] software IO TLB: area num 4. [ 0.000000] software IO TLB: mapped [mem 0x00000000fa000000-0x00000000fe000000] (64MB) [ 0.000000] Memory: 3945128K/4194304K available (11584K kernel code, 1254K rwdata, 3944K rodata, 1856K init, 461K bss, 216408K reserved, 32768K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4. [ 0.000000] rcu: RCU priority boosting: priority 1 delay 500 ms. [ 0.000000] rcu: RCU_SOFTIRQ processing moved to rcuc kthreads. [ 0.000000] No expedited grace period (rcu_normal_after_boot). [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 100 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 960 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] Root IRQ handler: gic_handle_irq [ 0.000000] GICv3: GICv3 features: 16 PPIs [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x0000000880040000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880050000 [ 0.000000] rcu: Offload RCU callbacks from CPUs: 0-3. [ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention. [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.000461] Console: colour dummy device 80x25 [ 0.457580] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=200000) [ 0.457594] pid_max: default: 32768 minimum: 301 [ 0.457690] LSM: Security Framework initializing [ 0.457857] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.457889] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.460319] cblist_init_generic: Setting adjustable number of callback queues. [ 0.503531] cblist_init_generic: Setting shift to 2 and lim to 1. [ 0.509880] cblist_init_generic: Setting adjustable number of callback queues. [ 0.517299] cblist_init_generic: Setting shift to 2 and lim to 1. [ 0.524012] rcu: Hierarchical SRCU implementation. [ 0.524017] rcu: Max phase no-delay instances is 400. [ 0.524118] printk: bootconsole [ns16550a0] printing thread started [ 0.541561] Platform MSI: msi-controller@1820000 domain created [ 0.541821] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.542185] EFI services will not be available. [ 0.542604] smp: Bringing up secondary CPUs ... I/TC: Secondary CPU 1 initializing I/TC: Secondary CPU 1 switching to normal world boot [ 0.576921] Detected VIPT I-cache on CPU1 [ 0.577064] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [ 0.577085] GICv3: CPU1: using allocated LPI pending table @0x0000000880060000 [ 0.577143] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] I/TC: Secondary CPU 2 initializing I/TC: Secondary CPU 2 switching to normal world boot [ 0.612473] Detected VIPT I-cache on CPU2 [ 0.612703] GICv3: CPU2: found redistributor 100 region 0:0x00000000018c0000 [ 0.612723] GICv3: CPU2: using allocated LPI pending table @0x0000000880070000 [ 0.612783] CPU2: Booted secondary processor 0x0000000100 [0x410fd034] I/TC: Secondary CPU 3 initializing I/TC: Secondary CPU 3 switching to normal world boot [ 0.648046] Detected VIPT I-cache on CPU3 [ 0.648148] GICv3: CPU3: found redistributor 101 region 0:0x00000000018e0000 [ 0.648163] GICv3: CPU3: using allocated LPI pending table @0x0000000880080000 [ 0.648197] CPU3: Booted secondary processor 0x0000000101 [0x410fd034] [ 0.648366] smp: Brought up 1 node, 4 CPUs [ 0.678020] SMP: Total of 4 processors activated. [ 0.678028] CPU features: detected: 32-bit EL0 Support [ 0.678035] CPU features: detected: CRC32 instructions [ 0.678113] CPU: All CPU(s) started at EL2 [ 0.678117] alternatives: applying system-wide alternatives [ 0.680506] devtmpfs: initialized [ 0.699092] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 1911260446275000 ns [ 0.699118] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) [ 0.700563] pinctrl core: initialized pinctrl subsystem [ 0.701312] DMI not present or invalid. [ 0.702166] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.716285] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations [ 0.716838] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.717185] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.717320] audit: initializing netlink subsys (disabled) [ 0.717568] audit: type=2000 audit(0.712:1): state=initialized audit_enabled=0 res=1 [ 0.718257] thermal_sys: Registered thermal governor 'step_wise' [ 0.718511] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.751882] ASID allocator initialised with 65536 entries [ 0.775177] KASLR disabled due to lack of seed [ 0.789238] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages [ 0.789248] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page [ 0.789255] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages [ 0.789259] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page [ 0.789265] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages [ 0.789269] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page [ 0.789276] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages [ 0.789280] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page [ 0.793330] k3-chipinfo 43000014.chipid: Family:AM65X rev:SR2.0 JTAGID[0x1bb5a02f] Detected [ 0.794886] iommu: Default domain type: Translated [ 0.794893] iommu: DMA domain TLB invalidation policy: strict mode [ 0.795398] SCSI subsystem initialized [ 0.795891] usbcore: registered new interface driver usbfs [ 0.795952] usbcore: registered new interface driver hub [ 0.795995] usbcore: registered new device driver usb [ 0.796590] pps_core: LinuxPPS API ver. 1 registered [ 0.796594] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.796619] PTP clock support registered [ 0.796820] EDAC MC: Ver: 3.0.0 [ 0.797966] FPGA manager framework [ 0.798103] Advanced Linux Sound Architecture Driver Initialized. [ 0.799481] clocksource: Switched to clocksource arch_sys_counter [ 0.799799] VFS: Disk quotas dquot_6.6.0 e 0.799852] VFS: Dquot-cache hash It/aTbC:le R eensterriveeds: s 5ha12r e(do rmedemror 0y ,i s4 0e9n6a bbleytd I/) T T[C : D y0.n8a1m1i2c7 2s]h aNreEdT :m Reemgoirsyt eisre ed naPFb_lIeNdE orpIr/otTCoc: olNo frmamaill Wy l[ d v ir0.tu8a11li7z1a5t]i oInP isudeppntosr th aiss h ditasabblel eden trieI/sT: C:6 5A5s36yn c(horrdonerou:s 7,n o5tif2i42ca8t8 iobnytse asr, e ldiniseaarb)le [ 0.816197] tcp_listen_portaddr_hash hash table entries: 2048 (order: 4, 81920 bytes, linear) [ 0.816349] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.816373] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 0.817012] TCP bind hash table entries: 32768 (order: 9, 2621440 bytes, linear) [ 0.820177] TCP: Hash tables configured (established 32768 bind 32768) [ 0.820435] UDP hash table entries: 2048 (order: 5, 196608 bytes, linear) [ 0.820729] UDP-Lite hash table entries: 2048 (order: 5, 196608 bytes, linear) [ 0.821206] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 0.821958] RPC: Registered named UNIX socket transport module. [ 0.821967] RPC: Registered udp transport module. [ 0.821971] RPC: Registered tcp transport module. [ 0.821974] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.821984] NET: Registered PF_XDP protocol family [ 0.822007] PCI: CLS 0 bytes, default 64 [ 0.823619] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available [ 0.825912] Initialise system trusted keyrings [ 0.826188] workingset: timestamp_bits=46 max_order=20 bucket_order=0 [ 1.0[85890] printk: console [ttyS2] printing thread started 0.836476] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 1.085913] printk: console [ttyS2] enabled [ 1.085923] printk: bootconsole [ns16550a0] disabled [ 1.097495] printk: bootconsole [ns16550a0] printing thread stopped [ 1.104138] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode [ 1.138514] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.144105] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83869 [ 1.144164] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 quirks:00000000 [ 1.144319] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4 [ 1.144328] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 1.145601] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0 [ 1.149954] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0 [ 1.152654] mmc0: CQHCI version 5.10 [ 1.166931] pca953x 0-0020: supply vcc not found, using dummy regulator [ 1.167132] pca953x 0-0020: using no AI [ 1.180201] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100 [ 1.180723] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100 [ 1.183020] ti-udma 285c0000.dma-controller: Channels: 28 (tchan: 14, rchan: 14, gp-rflow: 16) [ 1.191985] ti-udma 31150000.dma-controller: Channels: 119 (tchan: 53, rchan: 66, gp-rflow: 64) [ 1.194786] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit [ 1.208557] spi-nor spi0.0: unrecognized JEDEC id bytes: ff ff ff ff ff ff [ 1.214702] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode [ 1.248525] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.253935] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83869 [ 1.254000] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 quirks:00000000 [ 1.254161] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4 [ 1.254170] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 1.255166] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0 [ 1.279840] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48 [ 1.283436] fixedregulator-sd GPIO handle specifies active low - ignored [ 1.286016] debugfs: Directory 'pd:121' with parent 'pm_genpd' already present! [ 1.286082] debugfs: Directory 'pd:120' with parent 'pm_genpd' already present! [ 1.286210] mmc1: CQHCI version 5.10 [ 1.289646] input: gpio-keys as /devices/platform/gpio-keys/input/input0 [ 1.292715] mmc0: Command Queue Engine enabled [ 1.292734] mmc0: new HS200 MMC card at address 0001 [ 1.293679] mmcblk0: mmc0:0001 G1M15L 29.6 GiB [ 1.296243] mmcblk0boot0: mmc0:0001 G1M15L 31.5 MiB [ 1.298154] mmcblk0boot1: mmc0:0001 G1M15L 31.5 MiB [ 1.299895] mmcblk0rpmb: mmc0:0001 G1M15L 4.00 MiB, chardev (240:0) [ 1.306333] ALSA device list: [ 1.306345] No soundcards found. [ 1.328141] mmc1: SDHCI controller on 4fa0000.mmc [4fa0000.mmc] using ADMA 64-bit [ 1.328352] Waiting for root device PARTUUID=59d14097-02... [ 1.576959] mmc1: new ultra high speed SDR104 SDHC card at address aaaa [ 1.577949] mmcblk1: mmc1:aaaa SC16G 14.8 GiB [ 1.582002] mmcblk1: p1 p2 [ 1.603092] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none. [ 1.603175] VFS: Mounted root (ext4 filesystem) on device 179:98. [ 1.606528] devtmpfs: mounted [ 1.607936] Freeing unused kernel memory: 1856K [ 1.608087] Run /sbin/init as init process [ 1.799400] systemd[1]: System time before build time, advancing clock. [ 1.853112] NET: Registered PF_INET6 protocol family [ 1.854873] Segment Routing with IPv6 [ 1.854921] In-situ OAM (IOAM) with IPv6 [ 1.890705] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid) [ 1.891555] systemd[1]: Detected architecture arm64. Welcome to Arago 2023.10! [ 1.978606] systemd[1]: Hostname set to . [ 2.099580] systemd-sysv-generator[200]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust. [ 2.444826] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether. [ 2.531216] systemd[1]: Queued start job for default target Multi-User System. [ OK ] Created slice Slice /system/getty 2.701641] systemd[1]: Created slice Slice /system/getty. 0m. [ 2.720227] systemd[1]: Created slice Slice /system/modprobe. [ OK ] Created slice Slice /system/modprobe. [ OK ] Created slice Slice /system/serial-[ 2.738799] systemd[1]: Created slice Slice /system/serial-getty. getty. [ OK ] Created slice User and Session Slic[ 2.757117] systemd[1]: Created slice User and Session Slice. e. [ OK ] Started Dispatch Password …ts to [ 2.772072] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. Console Directory Watch. [ OK ] Started Forward Password R…uests [ 2.789015] systemd[1]: Started Forward Password Requests to Wall Directory Watch. to Wall Directory Watch. [ OK ] Reached target Path Units. [ 2.808095] systemd[1]: Reached target Path Units. [ OK ] Reached target Remote File Systems systemd[1]: Reached target Remote File Systems. [0m. [ OK ] Reached target Slice Units. [ 2.832715] systemd[1]: Reached target Slice Units. [ OK ] Reached target Swaps. [ 2.843564] systemd[1]: Reached target Swaps. [ OK ] Listening on RPCbind Server Activat[ 2.920577] systemd[1]: Listening on RPCbind Server Activation Socket. ion Socket. [ OK ] Reached target RPC Port Mapper.[ 2.935837] systemd[1]: Reached target RPC Port Mapper. [ OK ] Listening on Process Core Dump Sock[ 2.961952] systemd[1]: Listening on Process Core Dump Socket. et. [ OK ] Listening on initctl Compatibility [ 2.977079] systemd[1]: Listening on initctl Compatibility Named Pipe. Named Pipe. [ OK ] Listening on Journal Audit Socket 2.992942] systemd[1]: Listening on Journal Audit Socket. 0m. [ 3.007351] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 3.022441] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ OK ] Listening on Network Service Netlin[ 3.034726] systemd[1]: Listening on Network Service Netlink Socket. k Socket. [ OK ] Listening on udev Control Socket 3.050653] systemd[1]: Listening on udev Control Socket. m. [ OK ] Listening on udev Kernel Socket[ 3.065178] systemd[1]: Listening on udev Kernel Socket. . [ 3.079376] systemd[1]: Listening on User Database Manager Socket. [ OK ] Listening on User Database Manager Socket. [ 3.119288] systemd[1]: Mounting Huge Pages File System... Mounting Huge Pages File System... Mounting POSIX Message Queue File System..[ 3.137905] systemd[1]: Mounting POSIX Message Queue File System... . Mounting Kernel Debug File System... [ 3.160015] systemd[1]: Mounting Kernel Debug File System... [ 3.172181] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing). Mounting Temporary Directory /tmp...[ 3.185909] systemd[1]: Mounting Temporary Directory /tmp... [ 3.208325] systemd[1]: Starting Create List of Static Device Nodes... Starting Create List of Static Device Nodes... [ 3.230287] systemd[1]: Starting Load Kernel Module configfs... Starting Load Kernel Module configfs... [ 3.249325] systemd[1]: Starting Load Kernel Module drm... Starting Load Kernel Module drm... [ 3.267419] systemd[1]: Starting Load Kernel Module fuse... Starting Load Kernel Module fuse... [ 3.290432] fuse: init (API version 7.37) Starting Start psplash boot splash screen.[ 3.294809] systemd[1]: Starting Start psplash boot splash screen... .. [ 3.319313] systemd[1]: Starting RPC Bind... Starting RPC Bind... [ 3.329891] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/). Starting Journal Service... [ 3.341361] systemd[1]: Starting Journal Service... Starting Load Kernel Modules... [ 3.363563] systemd[1]: Starting Load Kernel Modules... Starting Generate network …ts from Kernel co[ 3.382883] systemd[1]: Starting Generate network units from Kernel command line... mmand line... [ 3.395684] cryptodev: loading out-of-tree module taints kernel. [ 3.397919] cryptodev: driver 1.12 loaded. Starting Remount Root and Kernel File Systems systemd[1]: Starting Remount Root and Kernel File Systems... [0m... Starting Coldplug All udev Devices... [ 3.438505] systemd[1]: Starting Coldplug All udev Devices... [ 3.445533] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none. [ OK ] Started RPC Bind. [ 3.466893] systemd[1]: Started RPC Bind. [ OK ] Mounted Huge Pages File System.[ 3.477060] systemd[1]: Mounted Huge Pages File System. [ 3.489268] systemd[1]: Mounted POSIX Message Queue File System. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Kernel Debug File System 3.504588] systemd[1]: Mounted Kernel Debug File System. m. [ 3.519424] systemd[1]: Mounted Temporary Directory /tmp. [ OK ] Mounted Temporary Directory /tmp. [ 3.537428] systemd[1]: Finished Create List of Static Device Nodes. [ OK ] Finished Create List of Static Device Nodes. [ 3.555400] systemd[1]: modprobe@configfs.service: Deactivated successfully. [ OK ] Finished Load Kernel Module configf[ 3.556958] systemd[1]: Finished Load Kernel Module configfs. s. [ OK ] Started Journal Service. [ 3.578579] systemd[1]: Started Journal Service. [ OK ] Finished Load Kernel Module drm. [ OK ] Finished Load Kernel Module fuse. [FAILED] Failed to start Start psplash boot splash screen. See 'systemctl status psplash-start.service' for details. [DEPEND] Dependency failed for Star…progress communication helper. [ OK ] Finished Load Kernel Modules. [ OK ] Finished Generate network units from Kernel command line. [ OK ] Finished Remount Root and Kernel File Systems. Mounting FUSE Control File System... Mounting Kernel Configuration File System... Starting Flush Journal to Persistent Storage... [ 3.833690] systemd-journald[216]: Received client request to flush runtime journal. Starting Apply Kernel Variables... Starting Create Static Device Nodes in /dev... [ OK ] Mounted FUSE Control File System. [ OK ] Mounted Kernel Configuration File System. [ OK ] Finished Flush Journal to Persistent Storage. [ OK ] Finished Apply Kernel Variables. [ OK ] Finished Create Static Device Nodes in /dev. [ OK ] Reached target Preparation for Local File Systems. Mounting /media/ram... Mounting /var/volatile... [ 4.049418] audit: type=1334 audit(1651167747.250:2): prog-id=5 op=LOAD Starting Rule-based Manage…for Device Events[ 4.052867] audit: type=1334 audit(1651167747.251:3): prog-id=6 op=LOAD and Files... [ OK ] Mounted /media/ram. [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Finished Coldplug All udev Devices. [ OK ] Finished Create Volatile Files and Directories. [ OK ] Started Rule-based Manager for Device Events and Files. Starting Network Time Synchronization... Starting Record System Boot/Shutdown in UTMP... [ OK ] Finished Record System Boot/Shutdown in UTMP. [ 4.393518] random: crng init done [ OK ] Finished Load/Save Random Seed. [ OK ] Found device /dev/ttyS2. [ 4.866906] spi-nor spi2.0: unrecognized JEDEC id bytes: 00 00 00 00 00 00 [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Initialization. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target System Time Set. [ OK ] Reached target Timer Units. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on D-Bus System Message Bus Socket. Starting Docker Socket for the API... [ OK ] Listening on dropbear.socket. Starting D-Bus System Message Bus... [ OK ] Listening on Docker Socket for the API. [ OK ] Reached target Socket Units. [ 5.096412] davinci_mdio b232400.mdio: Configuring MDIO in manual mode [ 5.129768] platform 41000000.r5f: configured R5F for remoteproc mode [ 5.145862] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000 [ 5.146305] remoteproc remoteproc0: 41000000.r5f is available [ 5.154804] remoteproc remoteproc0: Direct firmware load for am65x-mcu-r5f0_0-fw failed with error -2 [ 5.154838] remoteproc remoteproc0: powering up 41000000.r5f [ 5.154892] remoteproc remoteproc0: Direct firmware load for am65x-mcu-r5f0_0-fw failed with error -2 [ 5.154904] remoteproc remoteproc0: request_firmware failed: -2 [ 5.169224] davinci_mdio b232400.mdio: davinci mdio revision 1.7, bus freq 1000000 [ 5.197899] davinci_mdio b232400.mdio: phy[0]: device b232400.mdio:00, driver unknown [ 5.197920] davinci_mdio b232400.mdio: phy[3]: device b232400.mdio:03, driver unknown [ 5.369246] remoteproc remoteproc1: b00a000.txpru is available [ 5.370138] remoteproc remoteproc2: b00c000.txpru is available [ 5.370893] remoteproc remoteproc3: b10a000.txpru is available [ 5.371406] remoteproc remoteproc4: b10c000.txpru is available [ 5.372014] remoteproc remoteproc5: b20a000.txpru is available [ 5.372547] remoteproc remoteproc6: b20c000.txpru is available [ OK ] Started D-Bus System Message Bus. [ OK ] Reached target Basic System. Starting Print notice about GPLv3 packages... Starting IPv6 Packet Filtering Framework... Starting IPv4 Packet Filtering Framework... [ 5.589699] audit: type=1334 audit(1651175251.682:4): prog-id=7 op=LOAD [ 5.590259] audit: type=1334 audit(1651175251.684:5): prog-id=8 op=LOAD Starting User Login Management... [ OK ] Started TEE Supplicant. Starting Telnet Server... [FAILED] Failed to start Print notice about GPLv3 packages. See 'systemctl status gplv3-notice.service' for details. [ OK ] Finished IPv6 Packet Filtering Framework. [ OK ] Finished IPv4 Packet Filtering Framework. [ OK ] Finished Telnet Server. [ OK ] Reached target Preparation for Network. Starting Network Configuration... [ OK ] Started User Login Management. [ 6.288323] remoteproc remoteproc7: b006000.rtu is available [ 6.295689] remoteproc remoteproc8: b034000.pru is available [ 6.354950] remoteproc remoteproc9: b004000.rtu is available [ 6.371897] remoteproc remoteproc10: b038000.pru is available [ 6.383888] remoteproc remoteproc11: b134000.pru is available [ 6.387176] remoteproc remoteproc12: b104000.rtu is available [ 6.400548] remoteproc remoteproc13: b138000.pru is available [ 6.402136] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 6.403635] remoteproc remoteproc14: b106000.rtu is available [ 6.405147] remoteproc remoteproc15: b234000.pru is available [ 6.408458] remoteproc remoteproc16: b204000.rtu is available [ 6.411257] remoteproc remoteproc17: b238000.pru is available [ 6.414420] remoteproc remoteproc18: b206000.rtu is available [ 6.421984] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 6.422331] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 [ 6.422356] cfg80211: failed to load regulatory.db [ OK ] Started Network Configuration. Starting Network Name Resolution... [ 6.606310] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:00] driver [TI DP83869] (irq=POLL) [ 6.606345] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode [ OK ] Reached target Hardware activated USB gadget. [ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch. [ OK ] Created slice Slice /system/systemd-fsck. [ OK ] Found device /dev/mmcblk1p1. [ OK ] Started Network Name Resolution. [ OK ] Reached target Network. [ OK ] Reached target Host and Network Name Lookups. Starting Avahi mDNS/DNS-SD Stack... Starting containerd container runtime... [ OK ] Started Netperf Benchmark Server. [ OK ] Started NFS status monitor for NFSv2/3 locking.. Starting File System Check on /dev/mmcblk1p1... Starting Permit User Sessions... [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Finished Permit User Sessions. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttyS2. [ OK ] Reached target Login Prompts. Starting Synchronize System and HW clocks... [FAILED] Failed to start Synchronize System and HW clocks. See 'systemctl status sync-clocks.service' for details. [ OK ] Finished File System Check on /dev/mmcblk1p1. Mounting /run/media/boot-mmcblk1p1... [ OK ] Mounted /run/media/boot-mmcblk1p1. [ OK ] Started containerd container runtime. [ OK ] Reached target Multi-User System. Starting Record Runlevel Change in UTMP... [ OK ] Finished Record Runlevel Change in UTMP. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project am65xx-evm - Arago 2023.10 am65xx-evm - am65xx-evm login: root [ 11.765146] audit: type=1334 audit(1651175257.859:6): prog-id=9 op=LOAD [ 11.765355] audit: type=1334 audit(1651175257.859:7): prog-id=10 op=LOAD [ 12.291544] audit: type=1006 audit(1651175258.385:8): pid=545 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1 [ 12.291579] audit: type=1300 audit(1651175258.385:8): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=fffff6c7c058 a2=1 a3=ffffb010a020 items=0 ppid=1 pid=545 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null) [ 12.291599] audit: type=1327 audit(1651175258.385:8): proctitle="(systemd)" [ 12.348675] audit: type=1334 audit(1651175258.442:9): prog-id=11 op=LOAD [ 12.348717] audit: type=1300 audit(1651175258.442:9): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffd6b8eb00 a2=78 a3=0 items=0 ppid=1 pid=545 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="systemd" exe="/lib/systemd/systemd" key=(null) [ 12.348737] audit: type=1327 audit(1651175258.442:9): proctitle="(systemd)" [ 12.348765] audit: type=1334 audit(1651175258.443:10): prog-id=11 op=UNLOAD [ 12.348933] audit: type=1334 audit(1651175258.443:11): prog-id=12 op=LOAD root@am65xx-evm:~# ls root@am65xx-evm:~# [ 16.875237] icssg-prueth icssg2-eth: port 1: using random MAC addr: de:03:b9:b1:73:28 [ 16.877655] icssg-prueth icssg2-eth: port 2: using random MAC addr: 4e:61:ca:e9:63:68 [ 16.883625] Generic PHY b232400.mdio:00: attached PHY driver (mii_bus:phy_addr=b232400.mdio:00, irq=POLL) [ 16.891446] Generic PHY b232400.mdio:03: attached PHY driver (mii_bus:phy_addr=b232400.mdio:03, irq=POLL) [ 16.892953] icssg-prueth icssg2-eth: TI PRU ethernet driver initialized: dual EMAC mode [ 17.044590] remoteproc remoteproc15: powering up b234000.pru [ 17.049705] remoteproc remoteproc15: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 40936 [ 17.049743] remoteproc remoteproc15: unsupported resource 5 [ 17.049778] remoteproc remoteproc15: remote processor b234000.pru is now up [ 17.049817] remoteproc remoteproc16: powering up b204000.rtu [ 17.050818] remoteproc remoteproc16: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 30884 [ 17.050870] remoteproc remoteproc16: remote processor b204000.rtu is now up [ 17.050910] remoteproc remoteproc5: powering up b20a000.txpru [ 17.052084] remoteproc remoteproc5: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 36672 [ 17.052129] remoteproc remoteproc5: remote processor b20a000.txpru is now up [ 17.052597] remoteproc remoteproc17: powering up b238000.pru [ 17.053781] remoteproc remoteproc17: Booting fw image ti-pruss/am65x-sr2-pru1-prueth-fw.elf, size 41208 [ 17.053808] remoteproc remoteproc17: unsupported resource 5 [ 17.053837] remoteproc remoteproc17: remote processor b238000.pru is now up [ 17.053867] remoteproc remoteproc18: powering up b206000.rtu [ 17.054817] remoteproc remoteproc18: Booting fw image ti-pruss/am65x-sr2-rtu1-prueth-fw.elf, size 30124 [ 17.054856] remoteproc remoteproc18: remote processor b206000.rtu is now up [ 17.054888] remoteproc remoteproc6: powering up b20c000.txpru [ 17.055930] remoteproc remoteproc6: Booting fw image ti-pruss/am65x-sr2-txpru1-prueth-fw.elf, size 35184 [ 17.055970] remoteproc remoteproc6: remote processor b20c000.txpru is now up [ 17.057587] pps pps0: new PPS source ptp2 [ 17.062168] icssg-prueth icssg2-eth eth2: Link is Up - 100Mbps/Full - flow control off [ 17.115510] IPv6: ADDRCONF(NETDEV_CHANGE): eth2: link becomes ready [ 17.117204] icssg-prueth icssg2-eth eth1: Link is Up - 100Mbps/Full - flow control off [ 17.117295] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready ls root@am65xx-evm:~# root@am65xx-evm:~# ls root@am65xx-evm:~#