U-Boot SPL 2013.01.01 (Feb 27 2015 - 17:38:21) musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Peripheral mode controller at 47401000 using PIO, IRQ 0 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Host mode controller at 47401800 using PIO, IRQ 0 OMAP SD/MMC: 0 reading u-boot.img reading u-boot.img U-Boot 2013.01.01 (Feb 27 2015 - 17:38:21) I2C: ready DRAM: 512 MiB WARNING: Caches not enabled Incorrect magic number (0xffffffff) in EEPROM Could not get board ID. NAND: ####01---NAND device: Manufacturer ID: 0x2c, Chip ID: 0x38 (Toshiba ) ####02---NAND device: Manufacturer ID: 0x2c, Chip ID: 0x38 (Micron NAND 1GiB 3,3V Micron 8-bit) 1024 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - bad CRC, using default environment musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Peripheral mode controller at 47401000 using PIO, IRQ 0 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Host mode controller at 47401800 using PIO, IRQ 0 Net: not set. Validating first E-fuse MAC PHY reset timed out cpsw, usb_ether Hit any key to stop autoboot: 0 mmc0 is current device SD/MMC found on device 0 reading uEnv.txt 297 bytes read in 3 ms (96.7 KiB/s) Loaded environment from uEnv.txt Importing environment from mmc ... reading uImage 3215968 bytes read in 334 ms (9.2 MiB/s) Booting from mmc ... ## Booting kernel from Legacy Image at 80007fc0 ... Image Name: Linux-3.2.0 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3215904 Bytes = 3.1 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK XIP Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 3.2.0 (root@ubuntu) (gcc version 4.6.3 (Ubuntu/Linaro 4.6.3-1ubuntu5) ) #197 Tue Mar 17 18:57:18 IST 2015 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES1.0 (sgx neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext3 rootwait ip=none [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 512MB = 512MB total [ 0.000000] Memory: 512836k/512836k available, 11452k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc05a0000 (5728 kB) [ 0.000000] .init : 0xc05a0000 - 0xc0638000 ( 608 kB) [ 0.000000] .data : 0xc0638000 - 0xc0694318 ( 369 kB) [ 0.000000] .bss : 0xc069433c - 0xc06c0854 ( 178 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000122] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736) [ 0.089233] pid_max: default: 32768 minimum: 301 [ 0.089355] Security Framework initialized [ 0.089416] Mount-cache hash table entries: 512 [ 0.089752] CPU: Testing write buffer coherency: ok [ 0.090423] devtmpfs: initialized [ 0.108886] omap_hwmod: gfx: failed to hardreset [ 0.124664] omap_hwmod: pruss: failed to hardreset [ 0.125762] print_constraints: dummy: [ 0.126068] NET: Registered protocol family 16 [ 0.127777] OMAP GPIO hardware version 0.1 [ 0.129791] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.131591] omap_i2c.1: alias fck already exists [ 0.132324] omap2_mcspi.1: alias fck already exists [ 0.132507] omap2_mcspi.2: alias fck already exists [ 0.132720] edma.0: alias fck already exists [ 0.132720] edma.0: alias fck already exists [ 0.132751] edma.0: alias fck already exists [ 0.151672] bio: create slab at 0 [ 0.153442] SCSI subsystem initialized [ 0.154724] usbcore: registered new interface driver usbfs [ 0.154968] usbcore: registered new interface driver hub [ 0.155120] usbcore: registered new device driver usb [ 0.155242] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3 [ 0.155487] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1 [ 0.169250] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.170806] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.173065] print_constraints: VRTC: [ 0.174438] print_constraints: VIO: at 1800 mV [ 0.176666] print_constraints: VDD1: 600 <--> 1500 mV at 1325 mV normal [ 0.178863] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal [ 0.179779] print_constraints: VDD3: 5000 mV [ 0.181121] print_constraints: VDIG1: at 1800 mV [ 0.182495] print_constraints: VDIG2: at 1800 mV [ 0.183837] print_constraints: VPLL: at 1800 mV [ 0.185180] print_constraints: VDAC: at 1800 mV [ 0.186523] print_constraints: VAUX1: at 1800 mV [ 0.187896] print_constraints: VAUX2: at 3300 mV [ 0.189239] print_constraints: VAUX33: at 3300 mV [ 0.190582] print_constraints: VMMC: at 3300 mV [ 0.190948] tps65910 1-002d: No interrupt support, no core IRQ [ 0.191925] Advanced Linux Sound Architecture Driver Version 1.0.24. [ 0.192932] Switching to clocksource gp timer [ 0.206604] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.206756] musb-hdrc musb-hdrc.0: dma type: pio [ 0.207458] musb-hdrc musb-hdrc.0: USB OTG mode controller at e081c000 using PIO, IRQ 18 [ 0.207580] musb-hdrc musb-hdrc.1: dma type: pio [ 0.207916] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.207977] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 0.208099] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.208099] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.208129] usb usb1: Product: MUSB HDRC host driver [ 0.208129] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd [ 0.208129] usb usb1: SerialNumber: musb-hdrc.1 [ 0.208862] hub 1-0:1.0: USB hub found [ 0.208892] hub 1-0:1.0: 1 port detected [ 0.209381] musb-hdrc musb-hdrc.1: USB Host mode controller at e081e800 using PIO, IRQ 19 [ 0.209747] NET: Registered protocol family 2 [ 0.209899] IP route cache hash table entries: 4096 (order: 2, 16384 bytes) [ 0.210174] TCP established hash table entries: 16384 (order: 5, 131072 bytes) [ 0.210388] TCP bind hash table entries: 16384 (order: 4, 65536 bytes) [ 0.210510] TCP: Hash tables configured (established 16384 bind 16384) [ 0.210540] TCP reno registered [ 0.210540] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.210540] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.210693] NET: Registered protocol family 1 [ 0.210937] RPC: Registered named UNIX socket transport module. [ 0.210937] RPC: Registered udp transport module. [ 0.210937] RPC: Registered tcp transport module. [ 0.210968] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.211151] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.230743] VFS: Disk quotas dquot_6.5.2 [ 0.230804] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.231231] msgmni has been set to 1001 [ 0.231903] io scheduler noop registered [ 0.231933] io scheduler deadline registered [ 0.231964] io scheduler cfq registered (default) [ 0.233154] usbcore: registered new interface driver udlfb [ 0.233917] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 0.870361] console [ttyO0] enabled [ 0.874603] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 0.882385] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 0.890136] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 0.897918] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 0.905670] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 0.920898] brd: module loaded [ 0.928222] loop: module loaded [ 0.931671] i2c-core: driver [tsl2550] using legacy suspend method [ 0.938171] i2c-core: driver [tsl2550] using legacy resume method [ 0.944732] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 1.043609] No daughter card found [ 1.047210] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 1.056579] Board name: A33515BB [ 1.059967] Board version: 1.4A [ 1.063232] SKU: SKU#01 [ 1.083526] The board is general purpose EVM in profile 0 [ 1.089172] Found invalid GP EVM revision, falling back to Rev1.1A [ 1.141387] da8xx_lcdc.0: alias fck already exists [ 1.146697] usb 1-1: new high-speed USB device number 2 using musb-hdrc [ 1.154022] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel [ 1.175048] Console: switching to colour frame buffer device 100x30 [ 1.194091] omap-gpmc omap-gpmc: GPMC revision 6.0 [ 1.199096] Registering NAND on CS0 [ 1.203399] omap_i2c.2: alias fck already exists [ 1.223602] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz [ 1.230072] tsl2550 2-0039: standard operating mode [ 1.235351] tsl2550: probe of 2-0039 failed with error -121 [ 1.249389] omap_hsmmc.0: alias fck already exists [ 1.254791] omap_hsmmc.2: alias fck already exists [ 1.274566] Configure Bluetooth Enable pin... [ 1.294158] _regulator_get: 2-0018 supply Vdd not found, using dummy regulator [ 1.301788] _regulator_get: 2-0018 supply Vdd_IO not found, using dummy regulator [ 1.334838] usb 1-1: New USB device found, idVendor=04b4, idProduct=6572 [ 1.341827] usb 1-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0 [ 1.349304] usb 1-1: Product: USB2.0 Hub [ 1.353485] lis3lv02d: unknown sensor type 0x87 [ 1.358306] lis3lv02d_i2c: probe of 2-0018 failed with error -22 [ 1.365295] adc#01 : 4 [ 1.368652] adc#02 : 8 [ 1.373077] hub 1-1:1.0: USB hub found [ 1.377624] hub 1-1:1.0: 4 ports detected [ 1.382873] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.390228] omap2-nand driver initializing [ 1.394866] ONFI flash detected [ 1.398254] ONFI param page 0 valid [ 1.401916] NAND device: Manufacturer ID: 0x2c, Chip ID: 0x38 (Micron MT29F8G08ABABAWP) [ 1.410522] Creating 8 MTD partitions on "omap2-nand.0": [ 1.416107] 0x000000000000-0x000000080000 : "SPL" [ 1.422912] 0x000000080000-0x000000100000 : "SPL.backup1" [ 1.429748] 0x000000100000-0x000000180000 : "SPL.backup2" [ 1.436492] 0x000000180000-0x000000200000 : "SPL.backup3" [ 1.443237] 0x000000200000-0x000000380000 : "U-Boot" [ 1.449707] 0x000000380000-0x000000400000 : "U-Boot Env" [ 1.456390] 0x000000400000-0x000001000000 : "Kernel" [ 1.463928] 0x000001000000-0x000040000000 : "File System" [ 1.574371] OneNAND driver initializing [ 1.623565] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 1.630035] davinci_mdio davinci_mdio.0: no live phy, scanning all [ 1.636810] davinci_mdio: probe of davinci_mdio.0 failed with error -5 [ 1.643798] PPP generic driver version 2.4.2 [ 1.648620] PPP BSD Compression module registered [ 1.653564] PPP Deflate Compression module registered [ 1.659240] PPP MPPE Compression module registered [ 1.664520] usbcore: registered new interface driver zd1201 [ 1.670532] usbcore: registered new interface driver cdc_ether [ 1.676910] usbcore: registered new interface driver cdc_eem [ 1.683013] usbcore: registered new interface driver dm9601 [ 1.688903] cdc_ncm: 04-Aug-2011 [ 1.692504] usbcore: registered new interface driver cdc_ncm [ 1.698455] Initializing USB Mass Storage driver... [ 1.703796] usbcore: registered new interface driver usb-storage [ 1.710052] USB Mass Storage support registered. [ 1.715209] usbcore: registered new interface driver usbserial [ 1.721313] usbserial: USB Serial Driver core [ 1.726013] USB Serial support registered for cp210x [ 1.731384] usbcore: registered new interface driver cp210x [ 1.737243] cp210x: v0.09:Silicon Labs CP210x RS232 serial adaptor driver [ 1.744445] USB Serial support registered for pl2303 [ 1.749755] usbcore: registered new interface driver pl2303 [ 1.755615] pl2303: Prolific PL2303 USB to serial adaptor driver [ 1.762329] mousedev: PS/2 mouse device common for all mice [ 1.769134] input: adp5588-keys as /devices/platform/omap/omap_i2c.1/i2c-1/1-0034/input/input0 [ 1.783843] usb 1-1.2: new full-speed USB device number 3 using musb-hdrc [ 1.791320] adp5588_keys 1-0034: Rev.4 keypad, irq 216 [ 1.797729] input: ti-tsc as /devices/platform/omap/ti_tscadc/tsc/input/input1 [ 1.806488] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 [ 1.813293] i2c /dev entries driver [ 1.817687] Linux video capture interface: v2.00 [ 1.822845] lm75: probe of 2-0048 failed with error -121 [ 1.894989] usb 1-1.2: New USB device found, idVendor=10c4, idProduct=ea60 [ 1.902191] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [ 1.909820] usb 1-1.2: Product: CP2102 USB to UART Bridge Controller [ 1.916473] usb 1-1.2: Manufacturer: Silicon Labs [ 1.921386] usb 1-1.2: SerialNumber: 0001 [ 1.926971] cp210x 1-1.2:1.0: cp210x converter detected [ 1.964416] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.975402] cpuidle: using governor ladder [ 1.980163] cpuidle: using governor menu [ 1.984436] sdhci: Secure Digital Host Controller Interface driver [ 1.990905] sdhci: Copyright(c) Pierre Ossman [ 2.001037] usbcore: registered new interface driver usbhid [ 2.006927] usbhid: USB HID core driver [ 2.011657] tiadc tiadc: attached adc driver [ 2.016479] usb 1-1.2: reset full-speed USB device number 3 using musb-hdrc [ 2.024139] i2c-core: driver [hmc5843] using legacy suspend method [ 2.030578] i2c-core: driver [hmc5843] using legacy resume method [ 2.037872] usbcore: registered new interface driver snd-usb-audio [ 2.044372] ALSA device list: [ 2.047454] No soundcards found. [ 2.051025] oprofile: hardware counters not available [ 2.056304] oprofile: using timer interrupt. [ 2.060791] nf_conntrack version 0.5.0 (8013 buckets, 32052 max) [ 2.067626] ip_tables: (C) 2000-2006 Netfilter Core Team [ 2.073303] TCP cubic registered [ 2.076690] NET: Registered protocol family 17 [ 2.081451] Bridge firewalling registered [ 2.085693] lib80211: common routines for IEEE802.11 drivers [ 2.091644] Registering the dns_resolver key type [ 2.096588] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 2.104614] ThumbEE CPU extension supported. [ 2.109100] mux: Failed to setup hwmod io irq -22 [ 2.114685] Power Management for AM33XX family [ 2.119537] Trying to load am335x-pm-firmware.bin (60 secs timeout) [ 2.126190] Copied the M3 firmware to UMEM [ 2.130493] omap_hwmod: wkup_m3: wkup_m3: hwmod data error: OMAP4 does not support st_shift [ 2.145812] clock: disabling unused clocks to save power [ 2.153564] Detected MACID=d0:ff:50:55:5d:df [ 2.159576] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800) [ 2.215087] usb 1-1.2: cp210x converter now attached to ttyUSB0 [ 2.222290] Waiting for root device /dev/mmcblk0p2... [ 2.247314] mmc0: new SDHC card at address aaaa [ 2.252685] mmcblk0: mmc0:aaaa SU04G 3.69 GiB [ 2.259735] mmcblk0: p1 p2 [ 2.344757] usb 1-1.3: new full-speed USB device number 4 using musb-hdrc [ 2.354003] EXT3-fs (mmcblk0p2): recovery required on readonly filesystem [ 2.361083] EXT3-fs (mmcblk0p2): write access will be enabled during recovery [ 2.388977] mmc1: card claims to support voltages below the defined range. These will be ignored. [ 2.408050] mmc1: queuing unknown CIS tuple 0x91 (3 bytes) [ 2.414703] mmc1: new SDIO card at address 0001 [ 2.445220] usb 1-1.3: New USB device found, idVendor=10c4, idProduct=ea60 [ 2.452423] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [ 2.460083] usb 1-1.3: Product: CP2102 USB to UART Bridge Controller [ 2.466735] usb 1-1.3: Manufacturer: Silicon Labs [ 2.471618] usb 1-1.3: SerialNumber: 0001 [ 2.476806] kjournald starting. Commit interval 5 seconds [ 2.482635] EXT3-fs (mmcblk0p2): recovery complete [ 2.488250] cp210x 1-1.3:1.0: cp210x converter detected [ 2.498382] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode [ 2.505615] VFS: Mounted root (ext3 filesystem) readonly on device 179:2. [ 2.513580] Freeing init memory: 608K [ 2.574127] usb 1-1.3: reset full-speed USB device number 4 using musb-hdrc INIT: [ 2.675537] usb 1-1.3: cp210x converter now attached to ttyUSB1 version 2.88 booting [ 2.754455] usb 1-1.4: new full-speed USB device number 5 using musb-hdrc [ 2.855499] usb 1-1.4: New USB device found, idVendor=10c4, idProduct=ea60 [ 2.862701] usb 1-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [ 2.870361] usb 1-1.4: Product: CP2102 USB to UART Bridge Controller [ 2.876983] usb 1-1.4: Manufacturer: Silicon Labs [ 2.881896] usb 1-1.4: SerialNumber: 0001 [ 2.888885] cp210x 1-1.4:1.0: cp210x converter detected [ 2.974334] usb 1-1.4: reset full-speed USB device number 5 using musb-hdrc [ 3.090576] usb 1-1.4: cp210x converter now attached to ttyUSB2 Starting udev [ 4.348999] Disabling lock debugging due to kernel taint [ 6.709930] cfg80211: Calling CRDA to update world regulatory domain [ 6.830139] wl12xx: driver version: ol_R5.SP4.01-2-g1aa2c8e [ 6.835998] wl12xx: compilation time: Sat Jan 10 12:45:07 2015 [ 7.177429] cfg80211: World regulatory domain updated: [ 7.182861] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp) [ 7.191619] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 7.199890] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm) [ 7.208160] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm) [ 7.216430] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 7.224670] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 7.290100] wl12xx: loaded Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory bootlogd. [ 14.587982] EXT3-fs (mmcblk0p2): using internal journal ALSA: Restoring mixer settings... Configuring network interfaces... /usr/sbin/alsactl: load_state:1686: No soundcards found... [ 15.233001] PHY 0:00 not found [ 15.236297] PHY 0:01 not found udhcpc (v1.20.2) started Sending discover... Sending discover... Sending discover... No lease, failing done. INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Dropbear SSH server: dropbear. Starting telnet daemon. Performing wifi calibration... [ 25.628326] wl12xx: loaded Starting network benchmark server: netserver. Starting syslogd/klogd: done Starting thttpd. Launching Applications Desktop.. /etc/rc5.d/S40app.sh: line 3: cd: /home/pda/app/launcher: No such file or directory ....Launched.... Starting Lighttpd Web Server: 2015-03-18 14:26:22: (log.c.166) server started lighttpd. / Starting Matrix GUI application. [ 26.802917] gadget: Mass Storage Function, version: 2009/09/11 [ 26.809234] gadget: Number of LUNs=1 [ 26.813049] lun0: LUN: removable file: /dev/mmcblk0p1 [ 26.818450] gadget: Mass Storage Gadget, version: 2009/09/11 [ 26.824462] gadget: userspace failed to provide iSerialNumber [ 26.830566] gadget: g_mass_storage ready [ 26.834777] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 26.840362] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2 [ 26.848205] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 26.855285] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 26.862823] usb usb2: Product: MUSB HDRC host driver [ 26.868011] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd [ 26.873535] usb usb2: SerialNumber: musb-hdrc.0 [ 26.880187] hub 2-0:1.0: USB hub found [ 26.884124] hub 2-0:1.0: 1 port detected [ 27.205963] usb 2-1: new high-speed USB device number 2 using musb-hdrc [ 27.414855] usb 2-1: device v04f2 pb355 is not supported [ 27.420501] usb 2-1: New USB device found, idVendor=04f2, idProduct=b355 [ 27.427490] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0 [ 27.434936] usb 2-1: Product: 5M Web Camera [ 27.584655] uvcvideo: Found UVC 1.00 device 5M Web Camera (04f2:b355) [ 27.617645] input: 5M Web Camera as /devices/platform/omap/musb-ti81xx/musb-hdrc.0/usb2/2-1/2-1:1.0/input/input2 [ 27.635131] usbcore: registered new interface driver uvcvideo [ 27.641235] USB Video Class driver (1.1.1) *************************************************************** *************************************************************** NOTICE: This file system contains the followin GPLv3 packages: binutils-symlinks binutils gdbserver If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** Stopping Bootlog daemon: bootlogd. Error _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm ttyO0 Arago 2013.05 am335x-evm ttyO0 am335x-evm login: