# # Sample configuration file for ISC dhcpd for Debian # # Attention: If /etc/ltsp/dhcpd.conf exists, that will be used as # configuration file instead of this file. # # # The ddns-updates-style parameter controls whether or not the server will # attempt to do a DNS update when a lease is confirmed. We default to the # behavior of the version 2 packages ('none', since DHCP v2 didn't # have support for DDNS.) ddns-update-style none; # option definitions common to all supported networks... #option domain-name "example.org"; #option domain-name-servers ns1.example.org, ns2.example.org; #default-lease-time 600; #max-lease-time 7200; # If this DHCP server is the official DHCP server for the local # network, the authoritative directive should be uncommented. #authoritative; # Use this to send dhcp log messages to a different log file (you also # have to hack syslog.conf to complete the redirection). log-facility local7; # No service will be given on this subnet, but declaring it helps the # DHCP server to understand the network topology. #subnet 10.152.187.0 netmask 255.255.255.0 { #} # This is a very basic subnet declaration. #subnet 10.254.239.0 netmask 255.255.255.224 { # range 10.254.239.10 10.254.239.20; # option routers rtr-239-0-1.example.org, rtr-239-0-2.example.org; #} # This declaration allows BOOTP clients to get dynamic addresses, # which we don't really recommend. #subnet 10.254.239.32 netmask 255.255.255.224 { # range dynamic-bootp 10.254.239.40 10.254.239.60; # option broadcast-address 10.254.239.31; # option routers rtr-239-32-1.example.org; #} # A slightly different configuration for an internal subnet. #subnet 10.5.5.0 netmask 255.255.255.224 { # range 10.5.5.26 10.5.5.30; # option domain-name-servers ns1.internal.example.org; # option domain-name "internal.example.org"; # option routers 10.5.5.1; # option broadcast-address 10.5.5.31; # default-lease-time 600; # max-lease-time 7200; #} # Hosts which require special configuration options can be listed in # host statements. If no address is specified, the address will be # allocated dynamically (if possible), but the host-specific information # will still come from the host declaration. #host passacaglia { # hardware ethernet 0:0:c0:5d:bd:95; # filename "vmunix.passacaglia"; # server-name "toccata.fugue.com"; #} # Fixed IP addresses can also be specified for hosts. These addresses # should not also be listed as being available for dynamic assignment. # Hosts for which fixed IP addresses have been specified can boot using # BOOTP or DHCP. Hosts for which no fixed address is specified can only # be booted with DHCP, unless there is an address range on the subnet # to which a BOOTP client is connected which has the dynamic-bootp flag # set. #host fantasia { # hardware ethernet 08:00:07:26:c0:a5; # fixed-address fantasia.fugue.com; #} # You can declare a class of clients and then do address allocation # based on that. The example below shows a case where all clients # in a certain class get addresses on the 10.17.224/24 subnet, and all # other clients get addresses on the 10.0.29/24 subnet. #class "foo" { # match if substring (option vendor-class-identifier, 0, 4) = "SUNW"; #} #shared-network 224-29 { # subnet 10.17.224.0 netmask 255.255.255.0 { # option routers rtr-224.example.org; # } # subnet 10.0.29.0 netmask 255.255.255.0 { # option routers rtr-29.example.org; # } # pool { # allow members of "foo"; # range 10.17.224.10 10.17.224.250; # } # pool { # deny members of "foo"; # range 10.0.29.10 10.0.29.230; # } #} default-lease-time 600; max-lease-time 7200; option subnet-mask 255.255.255.0; option broadcast-address 192.168.1.255; option routers 192.168.1.254; option domain-name-servers 192.168.1.1, 192.168.1.2; option domain-name "mugunthan.com"; subnet 192.168.1.0 netmask 255.255.255.0 { #range dynamic-bootp 192.168.1.40 192.168.1.60; range 192.168.1.10 192.168.1.100; range 192.168.1.150 192.168.1.200; } host am43xxx_evm { hardware ethernet 34:b1:f7:3d:bb:40; fixed-address 192.168.1.5; if substring (option vendor-class-identifier, 0, 10) = "AM43xx ROM" { filename "u-boot-spl-restore.bin"; } elsif substring (option vendor-class-identifier, 0, 17) = "AM43xx U-Boot SPL" { filename "u-boot-restore.img"; } else { filename "zImage"; } } host am43xxx_evm_sk { hardware ethernet 34:b1:f7:3d:c1:3d; fixed-address 192.168.1.6; if substring (option vendor-class-identifier, 0, 10) = "AM43xx ROM" { filename "u-boot-spl-restore.bin"; } elsif substring (option vendor-class-identifier, 0, 17) = "AM43xx U-Boot SPL" { filename "u-boot-restore.img"; } else { filename "zImage"; } } host am437x_evm { #hardware ethernet 34:b1:f7:3d:b5:e5; #hardware ethernet 68:9e:19:ba:b0:de; #hardware ethernet 68:9e:19:ba:6d:b2; hardware ethernet c4:be:84:cc:80:e9; fixed-address 192.168.1.7; if substring (option vendor-class-identifier, 0, 10) = "AM43xx ROM" { filename "u-boot-spl-restore.bin"; } elsif substring (option vendor-class-identifier, 0, 17) = "AM43xx U-Boot SPL" { filename "u-boot-restore.img"; } else { filename "zImage"; } } host am437x_evm_1 { hardware ethernet 34:b1:f7:31:09:e8; fixed-address 192.168.1.9; if substring (option vendor-class-identifier, 0, 10) = "AM43xx ROM" { filename "u-boot-spl-restore.bin"; } elsif substring (option vendor-class-identifier, 0, 17) = "AM43xx U-Boot SPL" { filename "u-boot-restore.img"; } else { filename "zImage"; } } host am335x_evm { hardware ethernet 40:5f:c2:76:43:6d; fixed-address 192.168.1.8; if substring (option vendor-class-identifier, 0, 10) = "DM814x ROM" { filename "u-boot-spl-restore.bin"; } elsif substring (option vendor-class-identifier, 0, 17) = "AM335x U-Boot SPL" { filename "u-boot-restore.img"; } else { filename "zImage"; } } host am335x_evm_pg2 { hardware ethernet bc:6a:29:61:57:c2; fixed-address 192.168.1.8; if substring (option vendor-class-identifier, 0, 10) = "AM335x ROM" { filename "u-boot-spl-restore.bin"; } elsif substring (option vendor-class-identifier, 0, 17) = "AM335x U-Boot SPL" { filename "u-boot-restore.img"; } else { filename "zImage"; } }