i got errors ERROR: arago-base-tisdk-image-1.0-r0 do_image_complete: Error executing a python function in exec_python_func() autogenerated: The stack trace of python calls that resulted in this exception/failure was: File: 'exec_python_func() autogenerated', lineno: 2, function: 0001: *** 0002:sstate_task_postfunc(d) 0003: File: '/home/sridhar/tisdk_04_01/sources/oe-core/meta/classes/sstate.bbclass', lineno: 672, function: sstate_task_postfunc 0668: 0669:python sstate_task_postfunc () { 0670: shared_state = sstate_state_fromvars(d) 0671: *** 0672: sstate_install(shared_state, d) 0673: for intercept in shared_state['interceptfuncs']: 0674: bb.build.exec_func(intercept, d, (d.getVar("WORKDIR", True),)) 0675: omask = os.umask(0o002) 0676: if omask != 0o002: File: '/home/sridhar/tisdk_04_01/sources/oe-core/meta/classes/sstate.bbclass', lineno: 276, function: sstate_install 0272: 0273: # Run the actual file install 0274: for state in ss['dirs']: 0275: if os.path.exists(state[1]): *** 0276: oe.path.copyhardlinktree(state[1], state[2]) 0277: 0278: for postinst in (d.getVar('SSTATEPOSTINSTFUNCS', True) or '').split(): 0279: # All hooks should run in the SSTATE_INSTDIR 0280: bb.build.exec_func(postinst, d, (sstateinst,)) File: '/home/sridhar/tisdk_04_01/sources/oe-core/meta/lib/oe/path.py', lineno: 81, function: copyhardlinktree 0077: if (os.stat(src).st_dev == os.stat(dst).st_dev): 0078: # Need to copy directories only with tar first since cp will error if two 0079: # writers try and create a directory at the same time 0080: cmd = "cd %s; find . -type d -print | tar --xattrs --xattrs-include='*' -cf - -C %s -p --no-recursion --files-from - | tar --xattrs --xattrs-include='*' -xf - -C %s" % (src, src, dst) *** 0081: subprocess.check_output(cmd, shell=True, stderr=subprocess.STDOUT) 0082: source = '' 0083: if os.path.isdir(src): 0084: import glob 0085: if len(glob.glob('%s/.??*' % src)) > 0: File: '/usr/lib/python3.4/subprocess.py', lineno: 620, function: check_output 0616: process.wait() 0617: raise 0618: retcode = process.poll() 0619: if retcode: *** 0620: raise CalledProcessError(retcode, process.args, output=output) 0621: return output 0622: 0623: 0624:def list2cmdline(seq): Exception: subprocess.CalledProcessError: Command 'cd /home/sridhar/tisdk_04_01/build/arago-tmp-external-linaro-toolchain/work/am335x_evm-linux-gnueabi/arago-base-tisdk-image/1.0-r0/deploy-arago-base-tisdk-image-image-complete; find . -type d -print | tar --xattrs --xattrs-include='*' -cf - -C /home/sridhar/tisdk_04_01/build/arago-tmp-external-linaro-toolchain/work/am335x_evm-linux-gnueabi/arago-base-tisdk-image/1.0-r0/deploy-arago-base-tisdk-image-image-complete -p --no-recursion --files-from - | tar --xattrs --xattrs-include='*' -xf - -C /home/sridhar/tisdk_04_01/build/arago-tmp-external-linaro-toolchain/deploy/images/am335x-evm' returned non-zero exit status 2 Subprocess output: tar: .: Cannot utime: Operation not permitted tar: Exiting with failure status due to previous errors ERROR: arago-base-tisdk-image-1.0-r0 do_image_complete: Function failed: sstate_task_postfunc ERROR: Logfile of failure stored in: /home/sridhar/tisdk_04_01/build/arago-tmp-external-linaro-toolchain/work/am335x_evm-linux-gnueabi/arago-base-tisdk-image/1.0-r0/temp/log.do_image_complete.17846 ERROR: Task (/home/sridhar/tisdk_04_01/sources/meta-arago/meta-arago-distro/recipes-core/images/arago-base-tisdk-image.bb:do_image_complete) failed with exit code '1' NOTE: Tasks Summary: Attempted 4480 tasks of which 4479 didn't need to be rerun and 1 failed.