/etc/rcS.d/S04udev: line 119: syntax error near unexpected token `fi' /etc/rcS.d/S04udev: line 119: ` fi' [ 3.306747] random: dd urandom read with 73 bits of entropy available rm: can't remove '/tmp': Permission denied Sat Jan 9 00:07:04 UTC 2016 INIT: Entering runlevel: 5 NOT configuring network interfaces: / is an NFS mount udhcpc (v1.23.1) started Sending discover... Sending select for 172.17.2.177... Lease of 172.17.2.177 obtained, lease time 7200 /etc/udhcpc.d/50default: Adding DNS 172.17.0.1 /etc/udhcpc.d/50default: Adding DNS 8.8.8.8 /etc/udhcpc.d/50default: Adding DNS 8.8.4.4 /etc/udhcpc.d/50default: Adding DNS 202.251.202.3 [ 6.086239] random: nonblocking pool is initialized Starting system message bus: dbus. Starting Dropbear SSH server: [ 6.417142] ipv6: disagrees about version of symbol module_layout [ 6.435810] ipv6: disagrees about version of symbol module_layout dropbear. Starting softhsm daemon. Starting telnet daemon. [ 6.703180] ipv6: disagrees about version of symbol module_layout Starting rpcbind daemon...[ 6.822739] ipv6: disagrees about version of symbol module_layout rpcbind: cannot create socket for udp6 [ 6.842114] ipv6: disagrees about version of symbol module_layout rpcbind: cannot create socket for tcp6 done. starting statd: [ 6.894674] ipv6: disagrees about version of symbol module_layout done Starting thttpd[ 7.625897] ipv6: disagrees about version of symbol module_layout . [ 7.654838] ipv6: disagrees about version of symbol module_layout * starting FTP Server: vsftpd... done. *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: autoconf binutils-dev binutils bison-dev bison cpp-symlinks cpp g++-symlinks g++ gawk-dev gawk gcc-symlinks gcc gdb gdbc6x gdbserver libgmp10 libmpc3 libmpfr4 make If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org k2hk-evm /dev/ttyS0 Arago 2015.12 k2hk-evm /dev/ttyS0 k2hk-evm login: root Login incorrect k2hk-evm login: